![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
This structure stores the Sensor's context parameters. More...
#include <mma8491q_drv.h>

Data Fields | |
| uint64_t | adjustedODR |
| void * | pGpioEN |
| uint8_t | sensorMode |
| volatile bool | inTransition |
This structure stores the Sensor's context parameters.
Definition at line 46 of file mma8491q_drv.h.
| uint64_t adjustedODR |
Definition at line 48 of file mma8491q_drv.h.
| volatile bool inTransition |
The current operating Mode of the Sensor.
Definition at line 51 of file mma8491q_drv.h.
| void* pGpioEN |
The actual ODR calculated considering T_On and T_Rst.
Definition at line 49 of file mma8491q_drv.h.
| uint8_t sensorMode |
The GPIO handle for the EN Pin.
Definition at line 50 of file mma8491q_drv.h.