ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_STATUS_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xdr: 1
 
   uint8_t   ydr: 1
 
   uint8_t   zdr: 1
 
   uint8_t   zyxdr: 1
 
   uint8_t   xow: 1
 
   uint8_t   yow: 1
 
   uint8_t   zow: 1
 
   uint8_t   zyxow: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 76 of file mma865x.h.

Field Documentation

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 95 of file mma865x.h.

◆ xdr

uint8_t xdr

Definition at line 78 of file mma865x.h.

◆ xow

uint8_t xow

Definition at line 86 of file mma865x.h.

◆ ydr

uint8_t ydr

Definition at line 80 of file mma865x.h.

◆ yow

uint8_t yow

Definition at line 88 of file mma865x.h.

◆ zdr

uint8_t zdr

Definition at line 82 of file mma865x.h.

◆ zow

uint8_t zow

Definition at line 90 of file mma865x.h.

◆ zyxdr

uint8_t zyxdr

Definition at line 84 of file mma865x.h.

◆ zyxow

uint8_t zyxow

Definition at line 92 of file mma865x.h.


The documentation for this union was generated from the following file: