ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_F_SETUP_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_F_SETUP_t:
Collaboration graph

Data Fields

struct {
   uint8_t   f_wmrk: 6
 
   uint8_t   f_mode: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 276 of file mma865x.h.

Field Documentation

◆ b

struct { ... } b

◆ f_mode

uint8_t f_mode

Definition at line 280 of file mma865x.h.

◆ f_wmrk

uint8_t f_wmrk

Definition at line 278 of file mma865x.h.

◆ w

uint8_t w

Definition at line 283 of file mma865x.h.


The documentation for this union was generated from the following file: