ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_PL_STATUS_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_PL_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   bafro: 1
 
   uint8_t   lapo: 2
 
   uint8_t   _reserved_: 3
 
   uint8_t   lo: 1
 
   uint8_t   newlp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 606 of file mma865x.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 612 of file mma865x.h.

◆ b

struct { ... } b

◆ bafro

uint8_t bafro

Definition at line 608 of file mma865x.h.

◆ lapo

uint8_t lapo

Definition at line 610 of file mma865x.h.

◆ lo

uint8_t lo

Definition at line 613 of file mma865x.h.

◆ newlp

uint8_t newlp

Definition at line 615 of file mma865x.h.

◆ w

uint8_t w

Definition at line 618 of file mma865x.h.


The documentation for this union was generated from the following file: