ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_P_L_THS_REG_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_P_L_THS_REG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   hys: 3
 
   uint8_t   p_l_ths: 5
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 775 of file mma865x.h.

Field Documentation

◆ b

struct { ... } b

◆ hys

uint8_t hys

Definition at line 777 of file mma865x.h.

◆ p_l_ths

uint8_t p_l_ths

Definition at line 781 of file mma865x.h.

◆ w

uint8_t w

Definition at line 784 of file mma865x.h.


The documentation for this union was generated from the following file: