ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_TRANSIENT_THS_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_TRANSIENT_THS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   ths: 7
 
   uint8_t   dbcntm: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1165 of file mma865x.h.

Field Documentation

◆ b

struct { ... } b

◆ dbcntm

uint8_t dbcntm

Definition at line 1170 of file mma865x.h.

◆ ths

uint8_t ths

Definition at line 1167 of file mma865x.h.

◆ w

uint8_t w

Definition at line 1173 of file mma865x.h.


The documentation for this union was generated from the following file: