ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_PULSE_SRC_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_PULSE_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pol_x: 1
 
   uint8_t   pol_y: 1
 
   uint8_t   pol_z: 1
 
   uint8_t   dpe: 1
 
   uint8_t   axx: 1
 
   uint8_t   axy: 1
 
   uint8_t   axz: 1
 
   uint8_t   ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1302 of file mma865x.h.

Field Documentation

◆ axx

uint8_t axx

Definition at line 1312 of file mma865x.h.

◆ axy

uint8_t axy

Definition at line 1314 of file mma865x.h.

◆ axz

uint8_t axz

Definition at line 1316 of file mma865x.h.

◆ b

struct { ... } b

◆ dpe

uint8_t dpe

Definition at line 1310 of file mma865x.h.

◆ ea

uint8_t ea

Definition at line 1318 of file mma865x.h.

◆ pol_x

uint8_t pol_x

Definition at line 1304 of file mma865x.h.

◆ pol_y

uint8_t pol_y

Definition at line 1306 of file mma865x.h.

◆ pol_z

uint8_t pol_z

Definition at line 1308 of file mma865x.h.

◆ w

uint8_t w

Definition at line 1321 of file mma865x.h.


The documentation for this union was generated from the following file: