ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_CTRL_REG1_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_CTRL_REG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   active: 1
 
   uint8_t   f_read: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   dr: 3
 
   uint8_t   aslp_rate: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1508 of file mma865x.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1514 of file mma865x.h.

◆ active

uint8_t active

Definition at line 1510 of file mma865x.h.

◆ aslp_rate

uint8_t aslp_rate

Definition at line 1517 of file mma865x.h.

◆ b

struct { ... } b

◆ dr

uint8_t dr

Definition at line 1515 of file mma865x.h.

◆ f_read

uint8_t f_read

Definition at line 1512 of file mma865x.h.

◆ w

uint8_t w

Definition at line 1521 of file mma865x.h.


The documentation for this union was generated from the following file: