ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_CTRL_REG3_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_CTRL_REG3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pp_od: 1
 
   uint8_t   ipol: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   wake_ff_mt: 1
 
   uint8_t   wake_pulse: 1
 
   uint8_t   wake_lndprt: 1
 
   uint8_t   wake_trans: 1
 
   uint8_t   fifo_gate: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1636 of file mma865x.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1642 of file mma865x.h.

◆ b

struct { ... } b

◆ fifo_gate

uint8_t fifo_gate

Definition at line 1651 of file mma865x.h.

◆ ipol

uint8_t ipol

Definition at line 1640 of file mma865x.h.

◆ pp_od

uint8_t pp_od

Definition at line 1638 of file mma865x.h.

◆ w

uint8_t w

Definition at line 1654 of file mma865x.h.

◆ wake_ff_mt

uint8_t wake_ff_mt

Definition at line 1643 of file mma865x.h.

◆ wake_lndprt

uint8_t wake_lndprt

Definition at line 1647 of file mma865x.h.

◆ wake_pulse

uint8_t wake_pulse

Definition at line 1645 of file mma865x.h.

◆ wake_trans

uint8_t wake_trans

Definition at line 1649 of file mma865x.h.


The documentation for this union was generated from the following file: