ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MMA865x_CTRL_REG4_t Union Reference

#include <mma865x.h>

Collaboration diagram for MMA865x_CTRL_REG4_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_en_drdy: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   int_en_ff_mt: 1
 
   uint8_t   int_en_pulse: 1
 
   uint8_t   int_en_lndprt: 1
 
   uint8_t   int_en_trans: 1
 
   uint8_t   int_en_fifo: 1
 
   uint8_t   int_en_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1715 of file mma865x.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 1719 of file mma865x.h.

◆ b

struct { ... } b

◆ int_en_aslp

uint8_t int_en_aslp

Definition at line 1730 of file mma865x.h.

◆ int_en_drdy

uint8_t int_en_drdy

Definition at line 1717 of file mma865x.h.

◆ int_en_ff_mt

uint8_t int_en_ff_mt

Definition at line 1720 of file mma865x.h.

◆ int_en_fifo

uint8_t int_en_fifo

Definition at line 1728 of file mma865x.h.

◆ int_en_lndprt

uint8_t int_en_lndprt

Definition at line 1724 of file mma865x.h.

◆ int_en_pulse

uint8_t int_en_pulse

Definition at line 1722 of file mma865x.h.

◆ int_en_trans

uint8_t int_en_trans

Definition at line 1726 of file mma865x.h.

◆ w

uint8_t w

Definition at line 1733 of file mma865x.h.


The documentation for this union was generated from the following file: