ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MPL3115_DR_STATUS_t Union Reference

#include <mpl3115.h>

Collaboration diagram for MPL3115_DR_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 1
 
   uint8_t   tdr: 1
 
   uint8_t   pdr: 1
 
   uint8_t   ptdr: 1
 
   uint8_t   _reserved_1: 1
 
   uint8_t   tow: 1
 
   uint8_t   pow: 1
 
   uint8_t   ptow: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 165 of file mpl3115.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 167 of file mpl3115.h.

◆ _reserved_1

uint8_t _reserved_1

Definition at line 174 of file mpl3115.h.

◆ b

struct { ... } b

◆ pdr

uint8_t pdr

Definition at line 170 of file mpl3115.h.

◆ pow

uint8_t pow

Definition at line 177 of file mpl3115.h.

◆ ptdr

uint8_t ptdr

Definition at line 172 of file mpl3115.h.

◆ ptow

uint8_t ptow

Definition at line 179 of file mpl3115.h.

◆ tdr

uint8_t tdr

Definition at line 168 of file mpl3115.h.

◆ tow

uint8_t tow

Definition at line 175 of file mpl3115.h.

◆ w

uint8_t w

Definition at line 182 of file mpl3115.h.


The documentation for this union was generated from the following file: