ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MPL3115_CTRL_REG3_t Union Reference

#include <mpl3115.h>

Collaboration diagram for MPL3115_CTRL_REG3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pp_od2: 1
 
   uint8_t   ipol2: 1
 
   uint8_t   _reserved_: 2
 
   uint8_t   pp_od1: 1
 
   uint8_t   ipol1: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 946 of file mpl3115.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 953 of file mpl3115.h.

◆ b

struct { ... } b

◆ ipol1

uint8_t ipol1

Definition at line 957 of file mpl3115.h.

◆ ipol2

uint8_t ipol2

Definition at line 951 of file mpl3115.h.

◆ pp_od1

uint8_t pp_od1

Definition at line 954 of file mpl3115.h.

◆ pp_od2

uint8_t pp_od2

Definition at line 948 of file mpl3115.h.

◆ w

uint8_t w

Definition at line 960 of file mpl3115.h.


The documentation for this union was generated from the following file: