ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
MPL3115_CTRL_REG4_t Union Reference

#include <mpl3115.h>

Collaboration diagram for MPL3115_CTRL_REG4_t:
Collaboration graph

Data Fields

struct {
   uint8_t   int_en_tchg: 1
 
   uint8_t   int_en_pchg: 1
 
   uint8_t   int_en_tth: 1
 
   uint8_t   int_en_pth: 1
 
   uint8_t   int_en_tw: 1
 
   uint8_t   int_en_pw: 1
 
   uint8_t   int_en_fifo: 1
 
   uint8_t   int_en_drdy: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1001 of file mpl3115.h.

Field Documentation

◆ b

struct { ... } b

◆ int_en_drdy

uint8_t int_en_drdy

Definition at line 1017 of file mpl3115.h.

◆ int_en_fifo

uint8_t int_en_fifo

Definition at line 1015 of file mpl3115.h.

◆ int_en_pchg

uint8_t int_en_pchg

Definition at line 1005 of file mpl3115.h.

◆ int_en_pth

uint8_t int_en_pth

Definition at line 1009 of file mpl3115.h.

◆ int_en_pw

uint8_t int_en_pw

Definition at line 1013 of file mpl3115.h.

◆ int_en_tchg

uint8_t int_en_tchg

Definition at line 1003 of file mpl3115.h.

◆ int_en_tth

uint8_t int_en_tth

Definition at line 1007 of file mpl3115.h.

◆ int_en_tw

uint8_t int_en_tw

Definition at line 1011 of file mpl3115.h.

◆ w

uint8_t w

Definition at line 1020 of file mpl3115.h.


The documentation for this union was generated from the following file: