![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
This structure defines the fxos8700 all registers metadata. More...

Data Fields | |
| uint8_t | offset |
| uint8_t | value |
| uint8_t | trigger |
| uint8_t | read_offset |
| uint8_t | read_value |
| uint8_t | read_trigger |
| uint8_t | readall_value [FXOS8700_NUM_REGISTERS] |
| uint8_t | readall_size |
| uint8_t | readall_trigger |
| uint8_t | toggle |
| uint8_t | trigger_accel_offnoise |
| uint8_t | trigger_mag_offnoise |
| uint8_t | fs_value |
| uint8_t | mods_value |
| uint16_t | freefall_cntr |
| uint16_t | tapdetect_cntr |
| uint16_t | orient_cntr |
| uint16_t | vecmchange_cntr |
| uint8_t | reg_addr [FXOS8700_NUM_REGISTERS] |
| uint8_t | dataready_cntr |
| float | accel [3] |
| float | mag [3] |
This structure defines the fxos8700 all registers metadata.
Definition at line 158 of file fxos8700_freemaster_demo.c.
| float accel[3] |
Definition at line 180 of file fxos8700_freemaster_demo.c.
| uint8_t dataready_cntr |
Definition at line 179 of file fxos8700_freemaster_demo.c.
| uint16_t freefall_cntr |
Definition at line 174 of file fxos8700_freemaster_demo.c.
| uint8_t fs_value |
Definition at line 172 of file fxos8700_freemaster_demo.c.
Referenced by update_dropdown_selection().
| float mag[3] |
Definition at line 181 of file fxos8700_freemaster_demo.c.
| uint8_t mods_value |
Definition at line 173 of file fxos8700_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint8_t offset |
Definition at line 160 of file fxos8700_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint16_t orient_cntr |
Definition at line 176 of file fxos8700_freemaster_demo.c.
| uint8_t read_offset |
Definition at line 163 of file fxos8700_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint8_t read_trigger |
Definition at line 165 of file fxos8700_freemaster_demo.c.
| uint8_t read_value |
Definition at line 164 of file fxos8700_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint8_t readall_size |
Definition at line 167 of file fxos8700_freemaster_demo.c.
| uint8_t readall_trigger |
Definition at line 168 of file fxos8700_freemaster_demo.c.
| uint8_t readall_value[FXOS8700_NUM_REGISTERS] |
Definition at line 166 of file fxos8700_freemaster_demo.c.
Referenced by apply_register_readall().
| uint8_t reg_addr[FXOS8700_NUM_REGISTERS] |
Definition at line 178 of file fxos8700_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint16_t tapdetect_cntr |
Definition at line 175 of file fxos8700_freemaster_demo.c.
| uint8_t toggle |
Definition at line 169 of file fxos8700_freemaster_demo.c.
| uint8_t trigger |
Definition at line 162 of file fxos8700_freemaster_demo.c.
| uint8_t trigger_accel_offnoise |
Definition at line 170 of file fxos8700_freemaster_demo.c.
| uint8_t trigger_mag_offnoise |
Definition at line 171 of file fxos8700_freemaster_demo.c.
| uint8_t value |
Definition at line 161 of file fxos8700_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint16_t vecmchange_cntr |
Definition at line 177 of file fxos8700_freemaster_demo.c.