![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
This structure defines the mma865x all registers metadata. More...

Data Fields | |
| uint8_t | offset |
| uint8_t | value |
| uint8_t | trigger |
| uint8_t | read_offset |
| uint8_t | read_value |
| uint8_t | read_trigger |
| uint8_t | readall_value [MMA865x_NUM_REGISTERS] |
| uint8_t | readall_size |
| uint8_t | readall_trigger |
| uint8_t | toggle |
| uint8_t | trigger_accel_offnoise |
| uint8_t | fs_value |
| uint8_t | mods_value |
| uint16_t | freefall_cntr |
| uint16_t | tapdetect_cntr |
| uint16_t | orient_cntr |
| uint16_t | vecmchange_cntr |
| uint8_t | reg_addr [MMA865x_NUM_REGISTERS] |
| uint8_t | dataready_cntr |
| float | accel [3] |
| float | mag [3] |
This structure defines the mma865x all registers metadata.
Definition at line 120 of file mma865x_freemaster_demo.c.
| float accel[3] |
Definition at line 141 of file mma865x_freemaster_demo.c.
| uint8_t dataready_cntr |
Definition at line 140 of file mma865x_freemaster_demo.c.
| uint16_t freefall_cntr |
Definition at line 135 of file mma865x_freemaster_demo.c.
| uint8_t fs_value |
Definition at line 133 of file mma865x_freemaster_demo.c.
Referenced by update_dropdown_selection().
| float mag[3] |
Definition at line 142 of file mma865x_freemaster_demo.c.
| uint8_t mods_value |
Definition at line 134 of file mma865x_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint8_t offset |
Definition at line 122 of file mma865x_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint16_t orient_cntr |
Definition at line 137 of file mma865x_freemaster_demo.c.
| uint8_t read_offset |
Definition at line 125 of file mma865x_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint8_t read_trigger |
Definition at line 127 of file mma865x_freemaster_demo.c.
| uint8_t read_value |
Definition at line 126 of file mma865x_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint8_t readall_size |
Definition at line 129 of file mma865x_freemaster_demo.c.
| uint8_t readall_trigger |
Definition at line 130 of file mma865x_freemaster_demo.c.
| uint8_t readall_value[MMA865x_NUM_REGISTERS] |
Definition at line 128 of file mma865x_freemaster_demo.c.
Referenced by apply_register_readall().
| uint8_t reg_addr[MMA865x_NUM_REGISTERS] |
Definition at line 139 of file mma865x_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint16_t tapdetect_cntr |
Definition at line 136 of file mma865x_freemaster_demo.c.
| uint8_t toggle |
Definition at line 131 of file mma865x_freemaster_demo.c.
| uint8_t trigger |
Definition at line 124 of file mma865x_freemaster_demo.c.
| uint8_t trigger_accel_offnoise |
Definition at line 132 of file mma865x_freemaster_demo.c.
| uint8_t value |
Definition at line 123 of file mma865x_freemaster_demo.c.
Referenced by update_dropdown_selection().
| uint16_t vecmchange_cntr |
Definition at line 138 of file mma865x_freemaster_demo.c.