![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
This structure defines the fxls8962 raw data buffer. More...

Data Fields | |
| uint32_t | timestamp |
| int16_t | accel [3] |
| uint8_t | sdcd |
| int8_t | temp |
| int16_t | selftest [3] |
This structure defines the fxls8962 raw data buffer.
Definition at line 52 of file fxls8962_demo.c.
| int16_t accel[3] |
The time, this sample was recorded. The accel data
Definition at line 55 of file fxls8962_demo.c.
Referenced by main().
| uint8_t sdcd |
Definition at line 56 of file fxls8962_demo.c.
Referenced by main().
| int16_t selftest[3] |
Definition at line 58 of file fxls8962_demo.c.
Referenced by main(), and process_host_command().
| int8_t temp |
Definition at line 57 of file fxls8962_demo.c.
Referenced by main().
| uint32_t timestamp |
Definition at line 54 of file fxls8962_demo.c.
Referenced by main().