ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
pedometer_t::pedometer_status_tag Struct Reference

#include <pedometer.h>

Collaboration diagram for pedometer_t::pedometer_status_tag:
Collaboration graph

Data Fields

union {
   struct {
      activitylevel_t   activity: 3
 
      bool   suspend: 1
 
      bool   activitychange: 1
 
      bool   stepchange: 1
 
      bool   suspendchange: 1
 
      bool   mergedflags: 1
 
   }   bits
 
   uint8_t   byte
 
} status
 
uint8_t version
 
uint16_t stepcount
 
uint16_t distance
 
uint16_t speed
 
uint16_t calories
 
debounce_count_t sleepcount
 

Detailed Description

Definition at line 75 of file pedometer.h.

Field Documentation

◆ activity

activitylevel_t activity

Definition at line 81 of file pedometer.h.

◆ activitychange

bool activitychange

Definition at line 83 of file pedometer.h.

◆ bits

struct { ... } bits

Referenced by main().

◆ byte

uint8_t byte

Definition at line 88 of file pedometer.h.

◆ calories

uint16_t calories

Definition at line 94 of file pedometer.h.

Referenced by main().

◆ distance

uint16_t distance

Definition at line 92 of file pedometer.h.

Referenced by main().

◆ mergedflags

bool mergedflags

Definition at line 86 of file pedometer.h.

◆ sleepcount

debounce_count_t sleepcount

Definition at line 95 of file pedometer.h.

◆ speed

uint16_t speed

Definition at line 93 of file pedometer.h.

Referenced by main().

◆ status

union { ... } status

Referenced by main().

◆ stepchange

bool stepchange

Definition at line 84 of file pedometer.h.

◆ stepcount

uint16_t stepcount

Definition at line 91 of file pedometer.h.

Referenced by main().

◆ suspend

bool suspend

Definition at line 82 of file pedometer.h.

◆ suspendchange

bool suspendchange

Definition at line 85 of file pedometer.h.

◆ version

uint8_t version

Definition at line 90 of file pedometer.h.


The documentation for this struct was generated from the following file: