20 #define BOARD_NAME "FRDM-K64F" 23 #define BOARD_DEBUG_UART_TYPE DEBUG_CONSOLE_DEVICE_TYPE_UART 24 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) UART0 25 #define BOARD_DEBUG_UART_CLKSRC SYS_CLK 26 #define BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetCoreSysClkFreq() 27 #define BOARD_UART_IRQ UART0_RX_TX_IRQn 28 #define BOARD_UART_IRQ_HANDLER UART0_RX_TX_IRQHandler 30 #ifndef BOARD_DEBUG_UART_BAUDRATE 31 #define BOARD_DEBUG_UART_BAUDRATE 115200 35 #define BOARD_SW2_GPIO GPIOC 36 #define BOARD_SW2_PORT PORTC 37 #define BOARD_SW2_GPIO_PIN 6U 38 #define BOARD_SW2_IRQ PORTC_IRQn 39 #define BOARD_SW2_IRQ_HANDLER PORTC_IRQHandler 40 #define BOARD_SW2_NAME "SW2" 42 #define BOARD_SW3_GPIO GPIOA 43 #define BOARD_SW3_PORT PORTA 44 #define BOARD_SW3_GPIO_PIN 4U 45 #define BOARD_SW3_IRQ PORTA_IRQn 46 #define BOARD_SW3_IRQ_HANDLER PORTA_IRQHandler 47 #define BOARD_SW3_NAME "SW3" 49 #define LLWU_SW_GPIO BOARD_SW2_GPIO 50 #define LLWU_SW_PORT BOARD_SW2_PORT 51 #define LLWU_SW_GPIO_PIN BOARD_SW2_GPIO_PIN 52 #define LLWU_SW_IRQ BOARD_SW2_IRQ 53 #define LLWU_SW_IRQ_HANDLER BOARD_SW2_IRQ_HANDLER 54 #define LLWU_SW_NAME BOARD_SW2_NAME 57 #define LOGIC_LED_ON 0U 58 #define LOGIC_LED_OFF 1U 59 #define BOARD_LED_RED_GPIO GPIOB 60 #define BOARD_LED_RED_GPIO_PORT PORTB 61 #define BOARD_LED_RED_GPIO_PIN 22U 62 #define BOARD_LED_GREEN_GPIO GPIOE 63 #define BOARD_LED_GREEN_GPIO_PORT PORTE 64 #define BOARD_LED_GREEN_GPIO_PIN 26U 65 #define BOARD_LED_BLUE_GPIO GPIOB 66 #define BOARD_LED_BLUE_GPIO_PORT PORTB 67 #define BOARD_LED_BLUE_GPIO_PIN 21U 69 #define LED_RED_INIT(output) \ 70 GPIO_WritePinOutput(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PIN, output); \ 71 BOARD_LED_RED_GPIO->PDDR |= (1U << BOARD_LED_RED_GPIO_PIN) 72 #define LED_RED_ON() \ 73 GPIO_ClearPinsOutput(BOARD_LED_RED_GPIO, 1U << BOARD_LED_RED_GPIO_PIN) 74 #define LED_RED_OFF() \ 75 GPIO_SetPinsOutput(BOARD_LED_RED_GPIO, 1U << BOARD_LED_RED_GPIO_PIN) 76 #define LED_RED_TOGGLE() \ 77 GPIO_TogglePinsOutput(BOARD_LED_RED_GPIO, 1U << BOARD_LED_RED_GPIO_PIN) 79 #define LED_GREEN_INIT(output) \ 80 GPIO_WritePinOutput(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PIN, output); \ 81 BOARD_LED_GREEN_GPIO->PDDR |= (1U << BOARD_LED_GREEN_GPIO_PIN) 82 #define LED_GREEN_ON() \ 83 GPIO_ClearPinsOutput(BOARD_LED_GREEN_GPIO, 1U << BOARD_LED_GREEN_GPIO_PIN) 84 #define LED_GREEN_OFF() \ 85 GPIO_SetPinsOutput(BOARD_LED_GREEN_GPIO, 1U << BOARD_LED_GREEN_GPIO_PIN) 86 #define LED_GREEN_TOGGLE() \ 87 GPIO_TogglePinsOutput(BOARD_LED_GREEN_GPIO, 1U << BOARD_LED_GREEN_GPIO_PIN) 89 #define LED_BLUE_INIT(output) \ 90 GPIO_WritePinOutput(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PIN, output); \ 91 BOARD_LED_BLUE_GPIO->PDDR |= (1U << BOARD_LED_BLUE_GPIO_PIN) 92 #define LED_BLUE_ON() \ 93 GPIO_ClearPinsOutput(BOARD_LED_BLUE_GPIO, 1U << BOARD_LED_BLUE_GPIO_PIN) 94 #define LED_BLUE_OFF() \ 95 GPIO_SetPinsOutput(BOARD_LED_BLUE_GPIO, 1U << BOARD_LED_BLUE_GPIO_PIN) 96 #define LED_BLUE_TOGGLE() \ 97 GPIO_TogglePinsOutput(BOARD_LED_BLUE_GPIO, 1U << BOARD_LED_BLUE_GPIO_PIN) 100 #define BOARD_SDHC_CD_GPIO_IRQ_HANDLER PORTB_IRQHandler 103 #define BOARD_SDHC_BASEADDR SDHC 104 #define BOARD_SDHC_CLKSRC kCLOCK_CoreSysClk 105 #define BOARD_SDHC_CLK_FREQ CLOCK_GetFreq(kCLOCK_CoreSysClk) 106 #define BOARD_SDHC_IRQ SDHC_IRQn 107 #define BOARD_SDHC_CD_GPIO_BASE GPIOE 108 #define BOARD_SDHC_CD_GPIO_PIN 6U 109 #define BOARD_SDHC_CD_PORT_BASE PORTE 110 #define BOARD_SDHC_CD_PORT_IRQ PORTE_IRQn 111 #define BOARD_SDHC_CD_PORT_IRQ_HANDLER PORTE_IRQHandler 112 #define BOARD_SDHC_CD_LOGIC_RISING 114 #define BOARD_ACCEL_I2C_BASEADDR I2C0 117 #define ERPC_BOARD_DSPI_BASEADDR SPI0 118 #define ERPC_BOARD_DSPI_BAUDRATE 500000U 119 #define ERPC_BOARD_DSPI_CLKSRC DSPI0_CLK_SRC 120 #define ERPC_BOARD_DSPI_CLK_FREQ CLOCK_GetFreq(DSPI0_CLK_SRC) 121 #define ERPC_BOARD_DSPI_INT_GPIO GPIOB 122 #define ERPC_BOARD_DSPI_INT_PORT PORTB 123 #define ERPC_BOARD_DSPI_INT_PIN 2U 124 #define ERPC_BOARD_DSPI_INT_PIN_IRQ PORTB_IRQn 125 #define ERPC_BOARD_DSPI_INT_PIN_IRQ_HANDLER PORTB_IRQHandler 128 #define BOARD_DAC_BASEADDR DAC0 131 #define BOARD_ACCEL_FXOS 133 #if defined(__cplusplus) 142 #if defined(__cplusplus) void BOARD_InitDebugConsole(void)