ISSDK  1.8
IoT Sensing Software Development Kit
board.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Freescale Semiconductor, Inc.
3  * Copyright 2016-2017 NXP
4  * All rights reserved.
5  *
6  * SPDX-License-Identifier: BSD-3-Clause
7  */
8 
9 #ifndef _BOARD_H_
10 #define _BOARD_H_
11 
12 #include "clock_config.h"
13 #include "fsl_gpio.h"
14 
15 /*******************************************************************************
16  * Definitions
17  ******************************************************************************/
18 /*! @brief The board name */
19 #define BOARD_NAME "FRDM-K22F"
20 
21 /*! @brief The UART to use for debug messages. */
22 #define BOARD_USE_UART
23 #define BOARD_DEBUG_UART_TYPE DEBUG_CONSOLE_DEVICE_TYPE_UART
24 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) UART1
25 #define BOARD_DEBUG_UART_CLKSRC SYS_CLK
26 #define BOARD_DEBUG_UART_CLK_FREQ CLOCK_GetCoreSysClkFreq()
27 #define BOARD_UART_IRQ UART1_RX_TX_IRQn
28 #define BOARD_UART_IRQ_HANDLER UART1_RX_TX_IRQHandler
29 
30 #ifndef BOARD_DEBUG_UART_BAUDRATE
31 #define BOARD_DEBUG_UART_BAUDRATE 115200
32 #endif /* BOARD_DEBUG_UART_BAUDRATE */
33 
34 /*! @brief The bubble level demo information */
35 #define BOARD_FXOS8700_ADDR 0x1C
36 #define BOARD_ACCEL_ADDR BOARD_FXOS8700_ADDR
37 #define BOARD_ACCEL_BAUDRATE 100
38 #define BOARD_ACCEL_I2C_BASEADDR I2C0
39 
40 /*! @brief The i2c instance used for i2c connection by default */
41 #define BOARD_I2C_BASEADDR I2C0
42 
43 /*! @brief The CMP instance/channel used for board. */
44 #define BOARD_CMP_BASEADDR CMP0
45 #define BOARD_CMP_CHANNEL 0U
46 
47 /*! @brief The rtc instance used for board. */
48 #define BOARD_RTC_FUNC_BASEADDR RTC
49 
50 /*! @brief Define the port interrupt number for the board switches */
51 #define BOARD_SW3_GPIO GPIOB
52 #define BOARD_SW3_PORT PORTB
53 #define BOARD_SW3_GPIO_PIN 17
54 #define BOARD_SW3_IRQ PORTB_IRQn
55 #define BOARD_SW3_IRQ_HANDLER PORTB_IRQHandler
56 #define BOARD_SW3_NAME "SW3"
57 
58 #define BOARD_SW2_GPIO GPIOC
59 #define BOARD_SW2_PORT PORTC
60 #define BOARD_SW2_GPIO_PIN 1
61 #define BOARD_SW2_IRQ PORTC_IRQn
62 #define BOARD_SW2_IRQ_HANDLER PORTC_IRQHandler
63 #define BOARD_SW2_NAME "SW2"
64 
65 /* Board led color mapping */
66 #define LOGIC_LED_ON 0U
67 #define LOGIC_LED_OFF 1U
68 #define BOARD_LED_RED_GPIO GPIOA
69 #define BOARD_LED_RED_GPIO_PORT PORTA
70 #define BOARD_LED_RED_GPIO_PIN 1U
71 #define BOARD_LED_GREEN_GPIO GPIOA
72 #define BOARD_LED_GREEN_GPIO_PORT PORTA
73 #define BOARD_LED_GREEN_GPIO_PIN 2U
74 #define BOARD_LED_BLUE_GPIO GPIOD
75 #define BOARD_LED_BLUE_GPIO_PORT PORTD
76 #define BOARD_LED_BLUE_GPIO_PIN 5U
77 
78 #define LED_RED_INIT(output) \
79  GPIO_WritePinOutput(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PIN, output); \
80  BOARD_LED_RED_GPIO->PDDR |= (1U << BOARD_LED_RED_GPIO_PIN) /*!< Enable target LED_RED */
81 #define LED_RED_ON() \
82  GPIO_ClearPinsOutput(BOARD_LED_RED_GPIO, 1U << BOARD_LED_RED_GPIO_PIN) /*!< Turn on target LED_RED */
83 #define LED_RED_OFF() \
84  GPIO_SetPinsOutput(BOARD_LED_RED_GPIO, 1U << BOARD_LED_RED_GPIO_PIN) /*!< Turn off target LED_RED */
85 #define LED_RED_TOGGLE() \
86  GPIO_TogglePinsOutput(BOARD_LED_RED_GPIO, 1U << BOARD_LED_RED_GPIO_PIN) /*!< Toggle on target LED_RED */
87 
88 #define LED_GREEN_INIT(output) \
89  GPIO_WritePinOutput(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PIN, output); \
90  BOARD_LED_GREEN_GPIO->PDDR |= (1U << BOARD_LED_GREEN_GPIO_PIN) /*!< Enable target LED_GREEN */
91 #define LED_GREEN_ON() \
92  GPIO_ClearPinsOutput(BOARD_LED_GREEN_GPIO, 1U << BOARD_LED_GREEN_GPIO_PIN) /*!< Turn on target LED_GREEN */
93 #define LED_GREEN_OFF() \
94  GPIO_SetPinsOutput(BOARD_LED_GREEN_GPIO, 1U << BOARD_LED_GREEN_GPIO_PIN) /*!< Turn off target LED_GREEN */
95 #define LED_GREEN_TOGGLE() \
96  GPIO_TogglePinsOutput(BOARD_LED_GREEN_GPIO, 1U << BOARD_LED_GREEN_GPIO_PIN) /*!< Toggle on target LED_GREEN */
97 
98 #define LED_BLUE_INIT(output) \
99  GPIO_WritePinOutput(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PIN, output); \
100  BOARD_LED_BLUE_GPIO->PDDR |= (1U << BOARD_LED_BLUE_GPIO_PIN) /*!< Enable target LED_BLUE */
101 #define LED_BLUE_ON() \
102  GPIO_ClearPinsOutput(BOARD_LED_BLUE_GPIO, 1U << BOARD_LED_BLUE_GPIO_PIN) /*!< Turn on target LED_BLUE */
103 #define LED_BLUE_OFF() \
104  GPIO_SetPinsOutput(BOARD_LED_BLUE_GPIO, 1U << BOARD_LED_BLUE_GPIO_PIN) /*!< Turn off target LED_BLUE */
105 #define LED_BLUE_TOGGLE() \
106  GPIO_TogglePinsOutput(BOARD_LED_BLUE_GPIO, 1U << BOARD_LED_BLUE_GPIO_PIN) /*!< Toggle on target LED_BLUE */
107 
108 /* ERPC DSPI configuration */
109 #define ERPC_BOARD_DSPI_BASEADDR SPI0
110 #define ERPC_BOARD_DSPI_BAUDRATE 500000U
111 #define ERPC_BOARD_DSPI_CLKSRC DSPI0_CLK_SRC
112 #define ERPC_BOARD_DSPI_CLK_FREQ CLOCK_GetFreq(DSPI0_CLK_SRC)
113 #define ERPC_BOARD_DSPI_INT_GPIO GPIOB
114 #define ERPC_BOARD_DSPI_INT_PORT PORTB
115 #define ERPC_BOARD_DSPI_INT_PIN 2U
116 #define ERPC_BOARD_DSPI_INT_PIN_IRQ PORTB_IRQn
117 #define ERPC_BOARD_DSPI_INT_PIN_IRQ_HANDLER PORTB_IRQHandler
118 
119 /* @brief The SDSPI disk PHY configuration. */
120 #define BOARD_SDSPI_SPI_BASE SPI0_BASE /*!< SPI base address for SDSPI */
121 #define BOARD_SDSPI_CD_GPIO_BASE GPIOB /*!< Port related to card detect pin for SDSPI */
122 #define BOARD_SDSPI_CD_PIN 16U /*!< Card detect pin for SDSPI */
123 #define BOARD_SDSPI_CD_LOGIC_RISING /*!< Logic of card detect pin for SDSPI */
125 /* DAC base address */
126 #define BOARD_DAC_BASEADDR DAC0
128 /* Board accelerometer driver */
129 #define BOARD_ACCEL_FXOS
131 #if defined(__cplusplus)
132 extern "C" {
133 #endif /* __cplusplus */
134 
135 /*******************************************************************************
136  * API
137  ******************************************************************************/
139 void BOARD_InitDebugConsole(void);
140 
141 #if defined(__cplusplus)
142 }
143 #endif /* __cplusplus */
145 #endif /* _BOARD_H_ */
void BOARD_InitDebugConsole(void)
Definition: board.c:15