12 #include "fsl_common.h"    13 #include "fsl_reset.h"    20 #define BOARD_NAME "LPCXpresso5500"    24 #define BOARD_DEBUG_UART_TYPE kSerialPort_Uart    25 #define BOARD_DEBUG_UART_BASEADDR (uint32_t) USART0    26 #define BOARD_DEBUG_UART_INSTANCE 0U    27 #define BOARD_DEBUG_UART_CLK_FREQ 12000000U    28 #define BOARD_DEBUG_UART_CLK_ATTACH kFRO12M_to_FLEXCOMM0    29 #define BOARD_DEBUG_UART_RST kFC0_RST_SHIFT_RSTn    30 #define BOARD_DEBUG_UART_CLKSRC kCLOCK_Flexcomm0    31 #define BOARD_UART_IRQ_HANDLER FLEXCOMM0_IRQHandler    32 #define BOARD_UART_IRQ FLEXCOMM0_IRQn    34 #define BOARD_ACCEL_I2C_BASEADDR I2C4     35 #define BOARD_ACCEL_I2C_CLOCK_FREQ 12000000    37 #define BOARD_DEBUG_UART_TYPE_CORE1 kSerialPort_Uart    38 #define BOARD_DEBUG_UART_BASEADDR_CORE1 (uint32_t) USART1    39 #define BOARD_DEBUG_UART_INSTANCE_CORE1 1U    40 #define BOARD_DEBUG_UART_CLK_FREQ_CORE1 12000000U    41 #define BOARD_DEBUG_UART_CLK_ATTACH_CORE1 kFRO12M_to_FLEXCOMM1    42 #define BOARD_DEBUG_UART_RST_CORE1 kFC1_RST_SHIFT_RSTn    43 #define BOARD_DEBUG_UART_CLKSRC_CORE1 kCLOCK_Flexcomm1    44 #define BOARD_UART_IRQ_HANDLER_CORE1 FLEXCOMM1_IRQHandler    45 #define BOARD_UART_IRQ_CORE1 FLEXCOMM1_IRQn    47 #ifndef BOARD_DEBUG_UART_BAUDRATE    48 #define BOARD_DEBUG_UART_BAUDRATE 115200U    51 #ifndef BOARD_DEBUG_UART_BAUDRATE_CORE1    52 #define BOARD_DEBUG_UART_BAUDRATE_CORE1 115200U    55 #define BOARD_CODEC_I2C_BASEADDR I2C4    56 #define BOARD_CODEC_I2C_CLOCK_FREQ 12000000    58 #ifndef BOARD_LED_RED_GPIO    59 #define BOARD_LED_RED_GPIO GPIO    61 #define BOARD_LED_RED_GPIO_PORT 1U    62 #ifndef BOARD_LED_RED_GPIO_PIN    63 #define BOARD_LED_RED_GPIO_PIN 6U    66 #ifndef BOARD_LED_BLUE_GPIO    67 #define BOARD_LED_BLUE_GPIO GPIO    69 #define BOARD_LED_BLUE_GPIO_PORT 1U    70 #ifndef BOARD_LED_BLUE_GPIO_PIN    71 #define BOARD_LED_BLUE_GPIO_PIN 4U    74 #ifndef BOARD_LED_GREEN_GPIO    75 #define BOARD_LED_GREEN_GPIO GPIO    77 #define BOARD_LED_GREEN_GPIO_PORT 1U    78 #ifndef BOARD_LED_GREEN_GPIO_PIN    79 #define BOARD_LED_GREEN_GPIO_PIN 7U    82 #ifndef BOARD_SW1_GPIO    83 #define BOARD_SW1_GPIO GPIO    85 #define BOARD_SW1_GPIO_PORT 0U    86 #ifndef BOARD_SW1_GPIO_PIN    87 #define BOARD_SW1_GPIO_PIN 5U    89 #define BOARD_SW1_NAME "SW1"    90 #define BOARD_SW1_IRQ PIN_INT0_IRQn    91 #define BOARD_SW1_IRQ_HANDLER PIN_INT0_IRQHandler    93 #ifndef BOARD_SW2_GPIO    94 #define BOARD_SW2_GPIO GPIO    96 #define BOARD_SW2_GPIO_PORT 1U    97 #ifndef BOARD_SW2_GPIO_PIN    98 #define BOARD_SW2_GPIO_PIN 18U   100 #define BOARD_SW2_NAME "SW2"   101 #define BOARD_SW2_IRQ PIN_INT1_IRQn   102 #define BOARD_SW2_IRQ_HANDLER PIN_INT1_IRQHandler   103 #define BOARD_SW2_GPIO_PININT_INDEX 1   105 #ifndef BOARD_SW3_GPIO   106 #define BOARD_SW3_GPIO GPIO   108 #define BOARD_SW3_GPIO_PORT 1U   109 #ifndef BOARD_SW3_GPIO_PIN   110 #define BOARD_SW3_GPIO_PIN 9U   112 #define BOARD_SW3_NAME "SW3"   113 #define BOARD_SW3_IRQ PIN_INT1_IRQn   114 #define BOARD_SW3_IRQ_HANDLER PIN_INT1_IRQHandler   115 #define BOARD_SW3_GPIO_PININT_INDEX 1   117 #define BOARD_SDIF_BASEADDR SDIF   118 #define BOARD_SDIF_CLKSRC kCLOCK_SDio   119 #define BOARD_SDIF_CLK_FREQ CLOCK_GetFreq(kCLOCK_SDio)   120 #define BOARD_SDIF_CLK_ATTACH kMAIN_CLK_to_SDIO_CLK   121 #define BOARD_SDIF_IRQ SDIO_IRQn   122 #define BOARD_MMC_VCC_SUPPLY kMMC_VoltageWindows270to360   123 #define BOARD_SD_CARD_DETECT_PIN 17   124 #define BOARD_SD_CARD_DETECT_PORT 0   125 #define BOARD_SD_CARD_DETECT_GPIO GPIO   126 #define BOARD_SD_DETECT_TYPE kSDMMCHOST_DetectCardByHostCD   128 #define BOARD_SDIF_CD_GPIO_INIT()                                                                    \   130         CLOCK_EnableClock(kCLOCK_Gpio2);                                                             \   131         GPIO_PinInit(BOARD_SD_CARD_DETECT_GPIO, BOARD_SD_CARD_DETECT_PORT, BOARD_SD_CARD_DETECT_PIN, \   132                      &(gpio_pin_config_t){kGPIO_DigitalInput, 0U});                                  \   134 #define BOARD_SDIF_CD_STATUS() \   135     GPIO_PinRead(BOARD_SD_CARD_DETECT_GPIO, BOARD_SD_CARD_DETECT_PORT, BOARD_SD_CARD_DETECT_PIN)   138 #define LOGIC_LED_ON 0U   139 #define LOGIC_LED_OFF 1U   141 #define BOARD_SDIF_CLK_ATTACH kMAIN_CLK_to_SDIO_CLK   143 #define LED_RED_INIT(output)                                                          \   144     GPIO_PinInit(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT, BOARD_LED_RED_GPIO_PIN, \   145                  &(gpio_pin_config_t){kGPIO_DigitalOutput, (output)})    146 #define LED_RED_ON()                                            \   147     GPIO_PortClear(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT, \   148                    1U << BOARD_LED_RED_GPIO_PIN)    149 #define LED_RED_OFF()                                                                \   150     GPIO_PortSet(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT,                        \   151                  1U << BOARD_LED_RED_GPIO_PIN)    153 #define LED_RED_TOGGLE()                                         \   154     GPIO_PortToggle(BOARD_LED_RED_GPIO, BOARD_LED_RED_GPIO_PORT, \   155                     1U << BOARD_LED_RED_GPIO_PIN)    157 #define LED_BLUE_INIT(output)                                                            \   158     GPIO_PinInit(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, BOARD_LED_BLUE_GPIO_PIN, \   159                  &(gpio_pin_config_t){kGPIO_DigitalOutput, (output)})    160 #define LED_BLUE_ON()                                             \   161     GPIO_PortClear(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, \   162                    1U << BOARD_LED_BLUE_GPIO_PIN)    163 #define LED_BLUE_OFF()                                          \   164     GPIO_PortSet(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, \   165                  1U << BOARD_LED_BLUE_GPIO_PIN)    166 #define LED_BLUE_TOGGLE()                                          \   167     GPIO_PortToggle(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PORT, \   168                     1U << BOARD_LED_BLUE_GPIO_PIN)    170 #define LED_GREEN_INIT(output)                                                              \   171     GPIO_PinInit(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, BOARD_LED_GREEN_GPIO_PIN, \   172                  &(gpio_pin_config_t){kGPIO_DigitalOutput, (output)})    173 #define LED_GREEN_ON()                                              \   174     GPIO_PortClear(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, \   175                    1U << BOARD_LED_GREEN_GPIO_PIN)    176 #define LED_GREEN_OFF()                                           \   177     GPIO_PortSet(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, \   178                  1U << BOARD_LED_GREEN_GPIO_PIN)    179 #define LED_GREEN_TOGGLE()                                           \   180     GPIO_PortToggle(BOARD_LED_GREEN_GPIO, BOARD_LED_GREEN_GPIO_PORT, \   181                     1U << BOARD_LED_GREEN_GPIO_PIN)    184 #define BOARD_INITGT202SHIELD_PWRON_GPIO GPIO   185 #define BOARD_INITGT202SHIELD_PWRON_PORT 1U   186 #define BOARD_INITGT202SHIELD_PWRON_PIN 8U   188 #define BOARD_INITGT202SHIELD_IRQ_GPIO GPIO   189 #define BOARD_INITGT202SHIELD_IRQ_PORT 1U   190 #define BOARD_INITGT202SHIELD_IRQ_PIN 9U   194 #define BOARD_INITSILEX2401SHIELD_PWRON_GPIO GPIO   195 #define BOARD_INITSILEX2401SHIELD_PWRON_PORT 1U   196 #define BOARD_INITSILEX2401SHIELD_PWRON_PIN 7U   198 #define BOARD_INITSILEX2401SHIELD_IRQ_GPIO GPIO   199 #define BOARD_INITSILEX2401SHIELD_IRQ_PORT 0U   200 #define BOARD_INITSILEX2401SHIELD_IRQ_GPIO_PIN 15U   202 #if defined(__cplusplus)   212 #if defined(SDK_I2C_BASED_COMPONENT_USED) && SDK_I2C_BASED_COMPONENT_USED   213 void BOARD_I2C_Init(
I2C_Type *base, uint32_t clkSrc_Hz);
   215                         uint8_t deviceAddress,
   217                         uint8_t subaddressSize,
   221                            uint8_t deviceAddress,
   223                            uint8_t subaddressSize,
   226 void BOARD_Accel_I2C_Init(
void);
   227 status_t BOARD_Accel_I2C_Send(uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint32_t txBuff);
   228 status_t BOARD_Accel_I2C_Receive(
   229     uint8_t deviceAddress, uint32_t subAddress, uint8_t subaddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
   230 void BOARD_Codec_I2C_Init(
void);
   231 status_t BOARD_Codec_I2C_Send(
   232     uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, 
const uint8_t *txBuff, uint8_t txBuffSize);
   233 status_t BOARD_Codec_I2C_Receive(
   234     uint8_t deviceAddress, uint32_t subAddress, uint8_t subAddressSize, uint8_t *rxBuff, uint8_t rxBuffSize);
   237 #if defined(__cplusplus) void BOARD_InitDebugConsole_Core1(void)
 
void BOARD_InitDebugConsole(void)