![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
Go to the source code of this file.
Macros | |
#define | SHIELD_NAME "FRDM-STBC-AGM01" |
#define | FXOS8700_I2C_ADDR 0x1E |
#define | FXOS8700_INT1 D2 |
#define | FXOS8700_INT2 D4 |
#define | FXOS8700_CS A2 |
#define | FXAS21002_I2C_ADDR 0x20 |
#define | FXAS21002_INT1 D5 |
#define | FXAS21002_CS D10 |
#define | RESET_GPIO A3 |
#define FXAS21002_CS D10 |
Definition at line 29 of file frdm_stbc_agm01_shield.h.
#define FXAS21002_I2C_ADDR 0x20 |
Definition at line 27 of file frdm_stbc_agm01_shield.h.
#define FXAS21002_INT1 D5 |
Definition at line 28 of file frdm_stbc_agm01_shield.h.
#define FXOS8700_CS A2 |
Definition at line 24 of file frdm_stbc_agm01_shield.h.
#define FXOS8700_I2C_ADDR 0x1E |
Definition at line 21 of file frdm_stbc_agm01_shield.h.
#define FXOS8700_INT1 D2 |
Definition at line 22 of file frdm_stbc_agm01_shield.h.
#define FXOS8700_INT2 D4 |
Definition at line 23 of file frdm_stbc_agm01_shield.h.
#define RESET_GPIO A3 |
Definition at line 32 of file frdm_stbc_agm01_shield.h.
#define SHIELD_NAME "FRDM-STBC-AGM01" |
Definition at line 18 of file frdm_stbc_agm01_shield.h.