![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
Go to the source code of this file.
#define RTE_I2C1 1 |
Definition at line 13 of file RTE_Device.h.
#define RTE_I2C1_DMA_EN 0 |
Definition at line 14 of file RTE_Device.h.
#define RTE_I2C1_DMA_RX_CH 1 |
Definition at line 53 of file RTE_Device.h.
#define RTE_I2C1_DMA_RX_DMA_BASE DMA0 |
Definition at line 56 of file RTE_Device.h.
#define RTE_I2C1_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 55 of file RTE_Device.h.
#define RTE_I2C1_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C1 |
Definition at line 54 of file RTE_Device.h.
#define RTE_I2C1_DMA_TX_CH 0 |
Definition at line 49 of file RTE_Device.h.
#define RTE_I2C1_DMA_TX_DMA_BASE DMA0 |
Definition at line 52 of file RTE_Device.h.
#define RTE_I2C1_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 51 of file RTE_Device.h.
#define RTE_I2C1_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C1 |
Definition at line 50 of file RTE_Device.h.
#define RTE_I2C2 0 |
Definition at line 15 of file RTE_Device.h.
#define RTE_I2C2_DMA_EN 0 |
Definition at line 16 of file RTE_Device.h.
#define RTE_I2C2_DMA_RX_CH 3 |
Definition at line 62 of file RTE_Device.h.
#define RTE_I2C2_DMA_RX_DMA_BASE DMA0 |
Definition at line 65 of file RTE_Device.h.
#define RTE_I2C2_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 64 of file RTE_Device.h.
#define RTE_I2C2_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C2 |
Definition at line 63 of file RTE_Device.h.
#define RTE_I2C2_DMA_TX_CH 2 |
Definition at line 58 of file RTE_Device.h.
#define RTE_I2C2_DMA_TX_DMA_BASE DMA0 |
Definition at line 61 of file RTE_Device.h.
#define RTE_I2C2_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 60 of file RTE_Device.h.
#define RTE_I2C2_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C2 |
Definition at line 59 of file RTE_Device.h.
#define RTE_I2C3 0 |
Definition at line 17 of file RTE_Device.h.
#define RTE_I2C3_DMA_EN 0 |
Definition at line 18 of file RTE_Device.h.
#define RTE_I2C3_DMA_RX_CH 5 |
Definition at line 71 of file RTE_Device.h.
#define RTE_I2C3_DMA_RX_DMA_BASE DMA0 |
Definition at line 74 of file RTE_Device.h.
#define RTE_I2C3_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 73 of file RTE_Device.h.
#define RTE_I2C3_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C3 |
Definition at line 72 of file RTE_Device.h.
#define RTE_I2C3_DMA_TX_CH 4 |
Definition at line 67 of file RTE_Device.h.
#define RTE_I2C3_DMA_TX_DMA_BASE DMA0 |
Definition at line 70 of file RTE_Device.h.
#define RTE_I2C3_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 69 of file RTE_Device.h.
#define RTE_I2C3_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C3 |
Definition at line 68 of file RTE_Device.h.
#define RTE_I2C4 0 |
Definition at line 19 of file RTE_Device.h.
#define RTE_I2C4_DMA_EN 0 |
Definition at line 20 of file RTE_Device.h.
#define RTE_I2C4_DMA_RX_CH 7 |
Definition at line 80 of file RTE_Device.h.
#define RTE_I2C4_DMA_RX_DMA_BASE DMA0 |
Definition at line 83 of file RTE_Device.h.
#define RTE_I2C4_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 82 of file RTE_Device.h.
#define RTE_I2C4_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C4 |
Definition at line 81 of file RTE_Device.h.
#define RTE_I2C4_DMA_TX_CH 6 |
Definition at line 76 of file RTE_Device.h.
#define RTE_I2C4_DMA_TX_DMA_BASE DMA0 |
Definition at line 79 of file RTE_Device.h.
#define RTE_I2C4_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 78 of file RTE_Device.h.
#define RTE_I2C4_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPI2C4 |
Definition at line 77 of file RTE_Device.h.
#define RTE_SPI1 1 |
Definition at line 22 of file RTE_Device.h.
#define RTE_SPI1_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 88 of file RTE_Device.h.
#define RTE_SPI1_DMA_EN 0 |
Definition at line 23 of file RTE_Device.h.
#define RTE_SPI1_DMA_RX_CH 1 |
Definition at line 95 of file RTE_Device.h.
#define RTE_SPI1_DMA_RX_DMA_BASE DMA0 |
Definition at line 98 of file RTE_Device.h.
#define RTE_SPI1_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 97 of file RTE_Device.h.
#define RTE_SPI1_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI1Rx |
Definition at line 96 of file RTE_Device.h.
#define RTE_SPI1_DMA_TX_CH 0 |
Definition at line 91 of file RTE_Device.h.
#define RTE_SPI1_DMA_TX_DMA_BASE DMA0 |
Definition at line 94 of file RTE_Device.h.
#define RTE_SPI1_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 93 of file RTE_Device.h.
#define RTE_SPI1_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI1Tx |
Definition at line 92 of file RTE_Device.h.
#define RTE_SPI1_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 89 of file RTE_Device.h.
#define RTE_SPI1_PCS_TO_SCK_DELAY 1000 |
Definition at line 86 of file RTE_Device.h.
#define RTE_SPI1_SCK_TO_PSC_DELAY 1000 |
Definition at line 87 of file RTE_Device.h.
#define RTE_SPI1_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 90 of file RTE_Device.h.
#define RTE_SPI2 0 |
Definition at line 24 of file RTE_Device.h.
#define RTE_SPI2_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 102 of file RTE_Device.h.
#define RTE_SPI2_DMA_EN 0 |
Definition at line 25 of file RTE_Device.h.
#define RTE_SPI2_DMA_RX_CH 3 |
Definition at line 109 of file RTE_Device.h.
#define RTE_SPI2_DMA_RX_DMA_BASE DMA0 |
Definition at line 112 of file RTE_Device.h.
#define RTE_SPI2_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 111 of file RTE_Device.h.
#define RTE_SPI2_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI2Tx |
Definition at line 110 of file RTE_Device.h.
#define RTE_SPI2_DMA_TX_CH 2 |
Definition at line 105 of file RTE_Device.h.
#define RTE_SPI2_DMA_TX_DMA_BASE DMA0 |
Definition at line 108 of file RTE_Device.h.
#define RTE_SPI2_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 107 of file RTE_Device.h.
#define RTE_SPI2_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI2Tx |
Definition at line 106 of file RTE_Device.h.
#define RTE_SPI2_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 103 of file RTE_Device.h.
#define RTE_SPI2_PCS_TO_SCK_DELAY 1000 |
Definition at line 100 of file RTE_Device.h.
#define RTE_SPI2_SCK_TO_PSC_DELAY 1000 |
Definition at line 101 of file RTE_Device.h.
#define RTE_SPI2_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 104 of file RTE_Device.h.
#define RTE_SPI3 0 |
Definition at line 26 of file RTE_Device.h.
#define RTE_SPI3_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 116 of file RTE_Device.h.
#define RTE_SPI3_DMA_EN 0 |
Definition at line 27 of file RTE_Device.h.
#define RTE_SPI3_DMA_RX_CH 5 |
Definition at line 123 of file RTE_Device.h.
#define RTE_SPI3_DMA_RX_DMA_BASE DMA0 |
Definition at line 126 of file RTE_Device.h.
#define RTE_SPI3_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 125 of file RTE_Device.h.
#define RTE_SPI3_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI3Rx |
Definition at line 124 of file RTE_Device.h.
#define RTE_SPI3_DMA_TX_CH 4 |
Definition at line 119 of file RTE_Device.h.
#define RTE_SPI3_DMA_TX_DMA_BASE DMA0 |
Definition at line 122 of file RTE_Device.h.
#define RTE_SPI3_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 121 of file RTE_Device.h.
#define RTE_SPI3_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI3Tx |
Definition at line 120 of file RTE_Device.h.
#define RTE_SPI3_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 117 of file RTE_Device.h.
#define RTE_SPI3_PCS_TO_SCK_DELAY 1000 |
Definition at line 114 of file RTE_Device.h.
#define RTE_SPI3_SCK_TO_PSC_DELAY 1000 |
Definition at line 115 of file RTE_Device.h.
#define RTE_SPI3_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 118 of file RTE_Device.h.
#define RTE_SPI4 0 |
Definition at line 28 of file RTE_Device.h.
#define RTE_SPI4_BETWEEN_TRANSFER_DELAY 1000 |
Definition at line 130 of file RTE_Device.h.
#define RTE_SPI4_DMA_EN 0 |
Definition at line 29 of file RTE_Device.h.
#define RTE_SPI4_DMA_RX_CH 7 |
Definition at line 137 of file RTE_Device.h.
#define RTE_SPI4_DMA_RX_DMA_BASE DMA0 |
Definition at line 140 of file RTE_Device.h.
#define RTE_SPI4_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 139 of file RTE_Device.h.
#define RTE_SPI4_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI4Rx |
Definition at line 138 of file RTE_Device.h.
#define RTE_SPI4_DMA_TX_CH 6 |
Definition at line 133 of file RTE_Device.h.
#define RTE_SPI4_DMA_TX_DMA_BASE DMA0 |
Definition at line 136 of file RTE_Device.h.
#define RTE_SPI4_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 135 of file RTE_Device.h.
#define RTE_SPI4_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPSPI4Tx |
Definition at line 134 of file RTE_Device.h.
#define RTE_SPI4_MASTER_PCS_PIN_SEL (kLPSPI_MasterPcs0) |
Definition at line 131 of file RTE_Device.h.
#define RTE_SPI4_PCS_TO_SCK_DELAY 1000 |
Definition at line 128 of file RTE_Device.h.
#define RTE_SPI4_SCK_TO_PSC_DELAY 1000 |
Definition at line 129 of file RTE_Device.h.
#define RTE_SPI4_SLAVE_PCS_PIN_SEL (kLPSPI_SlavePcs0) |
Definition at line 132 of file RTE_Device.h.
#define RTE_USART1 1 |
Definition at line 31 of file RTE_Device.h.
#define RTE_USART1_DMA_EN 0 |
Definition at line 32 of file RTE_Device.h.
#define RTE_USART1_DMA_RX_CH 1 |
Definition at line 147 of file RTE_Device.h.
#define RTE_USART1_DMA_RX_DMA_BASE DMA0 |
Definition at line 150 of file RTE_Device.h.
#define RTE_USART1_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 149 of file RTE_Device.h.
#define RTE_USART1_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART1Rx |
Definition at line 148 of file RTE_Device.h.
#define RTE_USART1_DMA_TX_CH 0 |
Definition at line 143 of file RTE_Device.h.
#define RTE_USART1_DMA_TX_DMA_BASE DMA0 |
Definition at line 146 of file RTE_Device.h.
#define RTE_USART1_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 145 of file RTE_Device.h.
#define RTE_USART1_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART1Tx |
Definition at line 144 of file RTE_Device.h.
#define RTE_USART2 0 |
Definition at line 33 of file RTE_Device.h.
#define RTE_USART2_DMA_EN 0 |
Definition at line 34 of file RTE_Device.h.
#define RTE_USART2_DMA_RX_CH 1 |
Definition at line 156 of file RTE_Device.h.
#define RTE_USART2_DMA_RX_DMA_BASE DMA0 |
Definition at line 159 of file RTE_Device.h.
#define RTE_USART2_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 158 of file RTE_Device.h.
#define RTE_USART2_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART2Rx |
Definition at line 157 of file RTE_Device.h.
#define RTE_USART2_DMA_TX_CH 0 |
Definition at line 152 of file RTE_Device.h.
#define RTE_USART2_DMA_TX_DMA_BASE DMA0 |
Definition at line 155 of file RTE_Device.h.
#define RTE_USART2_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 154 of file RTE_Device.h.
#define RTE_USART2_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART2Tx |
Definition at line 153 of file RTE_Device.h.
#define RTE_USART3 0 |
Definition at line 35 of file RTE_Device.h.
#define RTE_USART3_DMA_EN 0 |
Definition at line 36 of file RTE_Device.h.
#define RTE_USART3_DMA_RX_CH 1 |
Definition at line 165 of file RTE_Device.h.
#define RTE_USART3_DMA_RX_DMA_BASE DMA0 |
Definition at line 168 of file RTE_Device.h.
#define RTE_USART3_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 167 of file RTE_Device.h.
#define RTE_USART3_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART3Rx |
Definition at line 166 of file RTE_Device.h.
#define RTE_USART3_DMA_TX_CH 0 |
Definition at line 161 of file RTE_Device.h.
#define RTE_USART3_DMA_TX_DMA_BASE DMA0 |
Definition at line 164 of file RTE_Device.h.
#define RTE_USART3_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 163 of file RTE_Device.h.
#define RTE_USART3_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART3Tx |
Definition at line 162 of file RTE_Device.h.
#define RTE_USART4 0 |
Definition at line 37 of file RTE_Device.h.
#define RTE_USART4_DMA_EN 0 |
Definition at line 38 of file RTE_Device.h.
#define RTE_USART4_DMA_RX_CH 1 |
Definition at line 174 of file RTE_Device.h.
#define RTE_USART4_DMA_RX_DMA_BASE DMA0 |
Definition at line 177 of file RTE_Device.h.
#define RTE_USART4_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 176 of file RTE_Device.h.
#define RTE_USART4_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART4Rx |
Definition at line 175 of file RTE_Device.h.
#define RTE_USART4_DMA_TX_CH 0 |
Definition at line 170 of file RTE_Device.h.
#define RTE_USART4_DMA_TX_DMA_BASE DMA0 |
Definition at line 173 of file RTE_Device.h.
#define RTE_USART4_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 172 of file RTE_Device.h.
#define RTE_USART4_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART4Tx |
Definition at line 171 of file RTE_Device.h.
#define RTE_USART5 0 |
Definition at line 39 of file RTE_Device.h.
#define RTE_USART5_DMA_EN 0 |
Definition at line 40 of file RTE_Device.h.
#define RTE_USART5_DMA_RX_CH 1 |
Definition at line 183 of file RTE_Device.h.
#define RTE_USART5_DMA_RX_DMA_BASE DMA0 |
Definition at line 186 of file RTE_Device.h.
#define RTE_USART5_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 185 of file RTE_Device.h.
#define RTE_USART5_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART5Rx |
Definition at line 184 of file RTE_Device.h.
#define RTE_USART5_DMA_TX_CH 0 |
Definition at line 179 of file RTE_Device.h.
#define RTE_USART5_DMA_TX_DMA_BASE DMA0 |
Definition at line 182 of file RTE_Device.h.
#define RTE_USART5_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 181 of file RTE_Device.h.
#define RTE_USART5_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART5Tx |
Definition at line 180 of file RTE_Device.h.
#define RTE_USART6 0 |
Definition at line 41 of file RTE_Device.h.
#define RTE_USART6_DMA_EN 0 |
Definition at line 42 of file RTE_Device.h.
#define RTE_USART6_DMA_RX_CH 1 |
Definition at line 192 of file RTE_Device.h.
#define RTE_USART6_DMA_RX_DMA_BASE DMA0 |
Definition at line 195 of file RTE_Device.h.
#define RTE_USART6_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 194 of file RTE_Device.h.
#define RTE_USART6_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART6Rx |
Definition at line 193 of file RTE_Device.h.
#define RTE_USART6_DMA_TX_CH 0 |
Definition at line 188 of file RTE_Device.h.
#define RTE_USART6_DMA_TX_DMA_BASE DMA0 |
Definition at line 191 of file RTE_Device.h.
#define RTE_USART6_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 190 of file RTE_Device.h.
#define RTE_USART6_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART6Tx |
Definition at line 189 of file RTE_Device.h.
#define RTE_USART7 0 |
Definition at line 43 of file RTE_Device.h.
#define RTE_USART7_DMA_EN 0 |
Definition at line 44 of file RTE_Device.h.
#define RTE_USART7_DMA_RX_CH 1 |
Definition at line 201 of file RTE_Device.h.
#define RTE_USART7_DMA_RX_DMA_BASE DMA0 |
Definition at line 204 of file RTE_Device.h.
#define RTE_USART7_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 203 of file RTE_Device.h.
#define RTE_USART7_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART7Rx |
Definition at line 202 of file RTE_Device.h.
#define RTE_USART7_DMA_TX_CH 0 |
Definition at line 197 of file RTE_Device.h.
#define RTE_USART7_DMA_TX_DMA_BASE DMA0 |
Definition at line 200 of file RTE_Device.h.
#define RTE_USART7_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 199 of file RTE_Device.h.
#define RTE_USART7_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART7Tx |
Definition at line 198 of file RTE_Device.h.
#define RTE_USART8 0 |
Definition at line 45 of file RTE_Device.h.
#define RTE_USART8_DMA_EN 0 |
Definition at line 46 of file RTE_Device.h.
#define RTE_USART8_DMA_RX_CH 1 |
Definition at line 210 of file RTE_Device.h.
#define RTE_USART8_DMA_RX_DMA_BASE DMA0 |
Definition at line 213 of file RTE_Device.h.
#define RTE_USART8_DMA_RX_DMAMUX_BASE DMAMUX |
Definition at line 212 of file RTE_Device.h.
#define RTE_USART8_DMA_RX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART8Rx |
Definition at line 211 of file RTE_Device.h.
#define RTE_USART8_DMA_TX_CH 0 |
Definition at line 206 of file RTE_Device.h.
#define RTE_USART8_DMA_TX_DMA_BASE DMA0 |
Definition at line 209 of file RTE_Device.h.
#define RTE_USART8_DMA_TX_DMAMUX_BASE DMAMUX |
Definition at line 208 of file RTE_Device.h.
#define RTE_USART8_DMA_TX_PERI_SEL (uint8_t) kDmaRequestMuxLPUART8Tx |
Definition at line 207 of file RTE_Device.h.