![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
Go to the source code of this file.
Macros | |
#define | SHIELD_NAME "FRDMSTBC-A8471" |
#define | FXLS8471_INT1 D2 |
#define | FXLS8471_INT2 D8 |
#define | FXLS8471_SPI_CS D10 |
#define FXLS8471_INT1 D2 |
Definition at line 22 of file frdm_stbc_a8471_shield.h.
#define FXLS8471_INT2 D8 |
Definition at line 23 of file frdm_stbc_a8471_shield.h.
#define FXLS8471_SPI_CS D10 |
Definition at line 24 of file frdm_stbc_a8471_shield.h.
#define SHIELD_NAME "FRDMSTBC-A8471" |
Definition at line 19 of file frdm_stbc_a8471_shield.h.