![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDMSTBC-A8491" |
| #define | MMA8491_I2C_ADDR 0x55 |
| #define | MMA8491_EN A1 |
| #define | MMA8491_XOUT D2 |
| #define | MMA8491_YOUT D5 |
| #define | MMA8491_ZOUT D8 |
| #define MMA8491_EN A1 |
Definition at line 22 of file frdm_stbc_a8491_shield.h.
| #define MMA8491_I2C_ADDR 0x55 |
Definition at line 21 of file frdm_stbc_a8491_shield.h.
| #define MMA8491_XOUT D2 |
Definition at line 23 of file frdm_stbc_a8491_shield.h.
| #define MMA8491_YOUT D5 |
Definition at line 24 of file frdm_stbc_a8491_shield.h.
| #define MMA8491_ZOUT D8 |
Definition at line 25 of file frdm_stbc_a8491_shield.h.
| #define SHIELD_NAME "FRDMSTBC-A8491" |
Definition at line 18 of file frdm_stbc_a8491_shield.h.