![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|

Go to the source code of this file.
Macros | |
| #define | SHIELD_NAME "FRDMSTBC-P3115" |
| #define | MPL3115_I2C_ADDR 0x60 |
| #define | MPL3115_INT1 D5 |
| #define | MPL3115_INT2 D2 |
| #define MPL3115_I2C_ADDR 0x60 |
Definition at line 22 of file frdm_stbc_p3115_shield.h.
| #define MPL3115_INT1 D5 |
Definition at line 23 of file frdm_stbc_p3115_shield.h.
| #define MPL3115_INT2 D2 |
Definition at line 24 of file frdm_stbc_p3115_shield.h.
| #define SHIELD_NAME "FRDMSTBC-P3115" |
Definition at line 19 of file frdm_stbc_p3115_shield.h.