![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
Go to the source code of this file.
Macros | |
| #define | FMSTR_PLATFORM_CORTEX_M 1 /* Cortex-M platform (see freemaster.h for list of all supported platforms) */ |
| #define | FMSTR_DEMO_ENOUGH_ROM 1 /* Platform has enough ROM to show most of the FreeMASTER features */ |
| Set the demo configuration. More... | |
| #define | FMSTR_DEMO_LARGE_ROM 1 /* Platform has large ROM enough to store the extended data structures used in FreeMASTER demo */ |
| #define | FMSTR_DEMO_SUPPORT_I64 1 /* support for long long type */ |
| #define | FMSTR_DEMO_SUPPORT_FLT 1 /* support for float type */ |
| #define | FMSTR_DEMO_SUPPORT_DBL 1 /* support for double type */ |
| #define | FMSTR_DISABLE 0 |
| Enable/Disable FreeMASTER functionalities. More... | |
| #define | FMSTR_LONG_INTR 0 |
| Select interrupt or poll-driven serial communication. More... | |
| #define | FMSTR_SHORT_INTR 1 |
| Queuing done in interrupt. More... | |
| #define | FMSTR_POLL_DRIVEN 0 |
| No interrupt needed, polling only. More... | |
| #define | FMSTR_TRANSPORT FMSTR_SERIAL |
| Select communication interface. More... | |
| #define | FMSTR_SERIAL_DRV FMSTR_SERIAL_MCUX_UART |
| Use serial driver for UART */. More... | |
| #define | FMSTR_FLEXCAN_TXMB 0 |
| Define communication interface base address or leave undefined for runtime setting. More... | |
| #define | FMSTR_FLEXCAN_RXMB 1 |
| #define | FMSTR_COMM_BUFFER_SIZE 0 |
| Input/output communication buffer size. More... | |
| #define | FMSTR_COMM_RQUEUE_SIZE 32 |
| Receive FIFO queue size (use with FMSTR_SHORT_INTR only) More... | |
| #define | FMSTR_USE_APPCMD 1 |
| Support for Application Commands. More... | |
| #define | FMSTR_APPCMD_BUFF_SIZE 32 |
| App.Command data buffer size. More... | |
| #define | FMSTR_MAX_APPCMD_CALLS 4 |
| How many app.cmd callbacks? (0=disable) More... | |
| #define | FMSTR_USE_SCOPE 2 |
| Oscilloscope support. More... | |
| #define | FMSTR_MAX_SCOPE_VARS 8 |
| Specify maximum number of scope variables per one oscilloscope. More... | |
| #define | FMSTR_USE_RECORDER 2 |
| Recorder support. More... | |
| #define | FMSTR_REC_BUFF_SIZE 1024 |
| Built-in recorder buffer. More... | |
| #define | FMSTR_REC_TIMEBASE FMSTR_REC_BASE_MILLISEC(0) |
| Recorder time base, specifies how often the recorder is called in the user app. More... | |
| #define | FMSTR_REC_FLOAT_TRIG 1 |
| Enable/disable floating point triggering. More... | |
| #define | FMSTR_USE_TSA 1 |
| Enable TSA functionality. More... | |
| #define | FMSTR_USE_TSA_INROM 1 |
| TSA tables declared as const (put to ROM) More... | |
| #define | FMSTR_USE_TSA_SAFETY 1 |
| Enable/Disable TSA memory protection. More... | |
| #define | FMSTR_USE_TSA_DYNAMIC 1 |
| Enable/Disable TSA entries to be added also in runtime. More... | |
| #define | FMSTR_USE_PIPES 3 |
| Specify number of supported pipe objects. More... | |
| #define | FMSTR_USE_READMEM 1 |
| Enable read memory commands. More... | |
| #define | FMSTR_USE_WRITEMEM 1 |
| Enable write memory commands. More... | |
| #define | FMSTR_USE_WRITEMEMMASK 1 |
| Enable write memory bits commands. More... | |
| #define | FMSTR_USE_HASHED_PASSWORDS 0 |
| When non-zero, the passwords above are specified as a pointer to 20-byte SHA1 hash of password text. More... | |
| #define FMSTR_APPCMD_BUFF_SIZE 32 |
App.Command data buffer size.
Definition at line 69 of file freemaster_cfg.h.
| #define FMSTR_COMM_BUFFER_SIZE 0 |
Input/output communication buffer size.
Set to 0 for "automatic"
Definition at line 62 of file freemaster_cfg.h.
| #define FMSTR_COMM_RQUEUE_SIZE 32 |
Receive FIFO queue size (use with FMSTR_SHORT_INTR only)
Set to 0 for "default"
Definition at line 65 of file freemaster_cfg.h.
| #define FMSTR_DEMO_ENOUGH_ROM 1 /* Platform has enough ROM to show most of the FreeMASTER features */ |
Set the demo configuration.
Definition at line 20 of file freemaster_cfg.h.
| #define FMSTR_DEMO_LARGE_ROM 1 /* Platform has large ROM enough to store the extended data structures used in FreeMASTER demo */ |
Definition at line 21 of file freemaster_cfg.h.
| #define FMSTR_DEMO_SUPPORT_DBL 1 /* support for double type */ |
Definition at line 24 of file freemaster_cfg.h.
| #define FMSTR_DEMO_SUPPORT_FLT 1 /* support for float type */ |
Definition at line 23 of file freemaster_cfg.h.
| #define FMSTR_DEMO_SUPPORT_I64 1 /* support for long long type */ |
Definition at line 22 of file freemaster_cfg.h.
| #define FMSTR_DISABLE 0 |
Enable/Disable FreeMASTER functionalities.
To disable all FreeMASTER functionalities
Definition at line 28 of file freemaster_cfg.h.
| #define FMSTR_FLEXCAN_RXMB 1 |
Definition at line 59 of file freemaster_cfg.h.
| #define FMSTR_FLEXCAN_TXMB 0 |
Define communication interface base address or leave undefined for runtime setting.
FlexCAN-specific, communication message buffers
Definition at line 58 of file freemaster_cfg.h.
| #define FMSTR_LONG_INTR 0 |
Select interrupt or poll-driven serial communication.
Complete message processing in interrupt
Definition at line 31 of file freemaster_cfg.h.
| #define FMSTR_MAX_APPCMD_CALLS 4 |
How many app.cmd callbacks? (0=disable)
Definition at line 70 of file freemaster_cfg.h.
| #define FMSTR_MAX_SCOPE_VARS 8 |
Specify maximum number of scope variables per one oscilloscope.
Definition at line 74 of file freemaster_cfg.h.
| #define FMSTR_PLATFORM_CORTEX_M 1 /* Cortex-M platform (see freemaster.h for list of all supported platforms) */ |
Definition at line 17 of file freemaster_cfg.h.
| #define FMSTR_POLL_DRIVEN 0 |
No interrupt needed, polling only.
Definition at line 33 of file freemaster_cfg.h.
| #define FMSTR_REC_BUFF_SIZE 1024 |
Built-in recorder buffer.
Built-in buffer size. Set to zero to disable using embedded buffer for recorder 0.
Definition at line 80 of file freemaster_cfg.h.
| #define FMSTR_REC_FLOAT_TRIG 1 |
Enable/disable floating point triggering.
Target-side address translation (TSA)
Definition at line 84 of file freemaster_cfg.h.
| #define FMSTR_REC_TIMEBASE FMSTR_REC_BASE_MILLISEC(0) |
Recorder time base, specifies how often the recorder is called in the user app.
0 = "unknown"
Definition at line 83 of file freemaster_cfg.h.
| #define FMSTR_SERIAL_DRV FMSTR_SERIAL_MCUX_UART |
Use serial driver for UART */.
Definition at line 51 of file freemaster_cfg.h.
| #define FMSTR_SHORT_INTR 1 |
Queuing done in interrupt.
Definition at line 32 of file freemaster_cfg.h.
| #define FMSTR_TRANSPORT FMSTR_SERIAL |
Select communication interface.
List of implemented standard FreeMASTER transports and its drivers FMSTR_SERIAL - Standard serial transport protocol (Used by various types of UART peripherals as USB CDC implementation) FMSTR_SERIAL_MCUX_UART - MCUXSDK driver for UART peripheral FMSTR_SERIAL_MCUX_LPUART - MCUXSDK driver for LPUART peripheral FMSTR_SERIAL_MCUX_USART - MCUXSDK driver for USART peripheral FMSTR_SERIAL_MCUX_MINIUSART -MCUXSDK driver for MINIUSART peripheral FMSTR_SERIAL_MCUX_USB - MCUXSDK driver for USB peripheral with CDC class FMSTR_CAN - Standard CAN transport protocol (Used by various types of CAN peripherals) FMSTR_CAN_MCUX_FLEXCAN - MCUXSDK driver for FlexCAN peripheral FMSTR_CAN_MCUX_MCAN - MCUXSDK driver for MCAN peripheral FMSTR_CAN_MCUX_MSCAN - MCUXSDK driver for msCAN peripheral FMSTR_PDBDM - Packet Driven BDM (Background debug memory access using JTAG, SWD or BDM debug probes). This transport does not use low-level driver. Use serial transport layer */
Definition at line 50 of file freemaster_cfg.h.
| #define FMSTR_USE_APPCMD 1 |
Support for Application Commands.
Enable/disable App.Commands support
Definition at line 68 of file freemaster_cfg.h.
| #define FMSTR_USE_HASHED_PASSWORDS 0 |
When non-zero, the passwords above are specified as a pointer to 20-byte SHA1 hash of password text.
Definition at line 108 of file freemaster_cfg.h.
| #define FMSTR_USE_PIPES 3 |
Specify number of supported pipe objects.
Enable/Disable read/write memory commands
Definition at line 93 of file freemaster_cfg.h.
| #define FMSTR_USE_READMEM 1 |
Enable read memory commands.
Definition at line 96 of file freemaster_cfg.h.
| #define FMSTR_USE_RECORDER 2 |
Recorder support.
Specify number of supported recorders
Definition at line 77 of file freemaster_cfg.h.
| #define FMSTR_USE_SCOPE 2 |
Oscilloscope support.
Specify number of supported oscilloscopes
Definition at line 73 of file freemaster_cfg.h.
| #define FMSTR_USE_TSA 1 |
Enable TSA functionality.
Definition at line 87 of file freemaster_cfg.h.
| #define FMSTR_USE_TSA_DYNAMIC 1 |
Enable/Disable TSA entries to be added also in runtime.
Pipes as data streaming over FreeMASTER protocol
Definition at line 90 of file freemaster_cfg.h.
| #define FMSTR_USE_TSA_INROM 1 |
TSA tables declared as const (put to ROM)
Definition at line 88 of file freemaster_cfg.h.
| #define FMSTR_USE_TSA_SAFETY 1 |
Enable/Disable TSA memory protection.
Definition at line 89 of file freemaster_cfg.h.
| #define FMSTR_USE_WRITEMEM 1 |
Enable write memory commands.
Definition at line 97 of file freemaster_cfg.h.
| #define FMSTR_USE_WRITEMEMMASK 1 |
Enable write memory bits commands.
Definition at line 98 of file freemaster_cfg.h.