![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | esai_edma_handle_t |
| ESAI DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | esai_edma_callback_t )(ESAI_Type *base, esai_edma_handle_t *handle, status_t status, void *userData) |
| ESAI eDMA transfer callback function for finish and error. | |
Driver version | |
| #define | FSL_ESAI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| Version 2.0.0. | |
eDMA Transactional | |
| void | ESAI_TransferTxCreateHandleEDMA (ESAI_Type *base, esai_edma_handle_t *handle, esai_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) |
| Initializes the ESAI eDMA handle. More... | |
| void | ESAI_TransferRxCreateHandleEDMA (ESAI_Type *base, esai_edma_handle_t *handle, esai_edma_callback_t callback, void *userData, edma_handle_t *dmaHandle) |
| Initializes the ESAI Rx eDMA handle. More... | |
| void | ESAI_TransferTxSetFormatEDMA (ESAI_Type *base, esai_edma_handle_t *handle, esai_format_t *format, uint32_t hckClockHz, uint32_t hclkSourceClockHz) |
| Configures the ESAI Tx audio format. More... | |
| void | ESAI_TransferRxSetFormatEDMA (ESAI_Type *base, esai_edma_handle_t *handle, esai_format_t *format, uint32_t hckClockHz, uint32_t hclkSourceClockHz) |
| Configures the ESAI Rx audio format. More... | |
| status_t | ESAI_TransferSendEDMA (ESAI_Type *base, esai_edma_handle_t *handle, esai_transfer_t *xfer) |
| Performs a non-blocking ESAI transfer using DMA. More... | |
| status_t | ESAI_TransferReceiveEDMA (ESAI_Type *base, esai_edma_handle_t *handle, esai_transfer_t *xfer) |
| Performs a non-blocking ESAI receive using eDMA. More... | |
| void | ESAI_TransferAbortSendEDMA (ESAI_Type *base, esai_edma_handle_t *handle) |
| Aborts a ESAI transfer using eDMA. More... | |
| void | ESAI_TransferAbortReceiveEDMA (ESAI_Type *base, esai_edma_handle_t *handle) |
| Aborts a ESAI receive using eDMA. More... | |
| status_t | ESAI_TransferGetSendCountEDMA (ESAI_Type *base, esai_edma_handle_t *handle, size_t *count) |
| Gets byte count sent by ESAI. More... | |
| status_t | ESAI_TransferGetReceiveCountEDMA (ESAI_Type *base, esai_edma_handle_t *handle, size_t *count) |
| Gets byte count received by ESAI. More... | |
| struct _esai_edma_handle |
Data Fields | |
| edma_handle_t * | dmaHandle |
| DMA handler for ESAI send. | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t | bitWidth |
| Bit width for transfer, 8/16/24/32 bits. | |
| uint8_t | slotLen |
| Slot length of the audio data. | |
| uint8_t | count |
| The transfer data count in a DMA request. | |
| uint8_t | sectionMap |
| Section enabled for transfer. | |
| uint32_t | state |
| Internal state for ESAI eDMA transfer. | |
| esai_edma_callback_t | callback |
| Callback for users while transfer finish or error occurs. | |
| void * | userData |
| User callback parameter. | |
| edma_tcd_t | tcd [ESAI_XFER_QUEUE_SIZE+1U] |
| TCD pool for eDMA transfer. More... | |
| esai_transfer_t | esaiQueue [ESAI_XFER_QUEUE_SIZE] |
| Transfer queue storing queued transfer. More... | |
| size_t | transferSize [ESAI_XFER_QUEUE_SIZE] |
| Data bytes need to transfer. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. More... | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| uint8_t esai_edma_handle_t::nbytes |
| edma_tcd_t esai_edma_handle_t::tcd[ESAI_XFER_QUEUE_SIZE+1U] |
| esai_transfer_t esai_edma_handle_t::esaiQueue[ESAI_XFER_QUEUE_SIZE] |
| volatile uint8_t esai_edma_handle_t::queueUser |
| void ESAI_TransferTxCreateHandleEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| esai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaHandle | ||
| ) |
This function initializes the ESAI master DMA handle, which can be used for other ESAI master transactional APIs. Usually, for a specified ESAI instance, call this API once to get the initialized handle.
| base | ESAI base pointer. |
| handle | ESAI eDMA handle pointer. |
| base | ESAI peripheral base address. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| dmaHandle | eDMA handle pointer, this handle shall be static allocated by users. |
| void ESAI_TransferRxCreateHandleEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| esai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaHandle | ||
| ) |
This function initializes the ESAI slave DMA handle, which can be used for other ESAI master transactional APIs. Usually, for a specified ESAI instance, call this API once to get the initialized handle.
| base | ESAI base pointer. |
| handle | ESAI eDMA handle pointer. |
| base | ESAI peripheral base address. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| dmaHandle | eDMA handle pointer, this handle shall be static allocated by users. |
| void ESAI_TransferTxSetFormatEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| esai_format_t * | format, | ||
| uint32_t | hckClockHz, | ||
| uint32_t | hclkSourceClockHz | ||
| ) |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to formatting requirements.
| base | ESAI base pointer. |
| handle | ESAI eDMA handle pointer. |
| format | Pointer to ESAI audio data format structure. |
| hckClockHz | HCK clock frequency in Hz. |
| hclkSourceClockHz | HCK clock source frequency in Hz. |
| kStatus_Success | Audio format set successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| void ESAI_TransferRxSetFormatEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| esai_format_t * | format, | ||
| uint32_t | hckClockHz, | ||
| uint32_t | hclkSourceClockHz | ||
| ) |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to formatting requirements.
| base | ESAI base pointer. |
| handle | ESAI eDMA handle pointer. |
| format | Pointer to ESAI audio data format structure. |
| hckClockHz | HCK clock frequency in Hz. |
| hclkSourceClockHz | HCK clock source frequency in Hz. |
| kStatus_Success | Audio format set successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| status_t ESAI_TransferSendEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| esai_transfer_t * | xfer | ||
| ) |
| base | ESAI base pointer. |
| handle | ESAI eDMA handle pointer. |
| xfer | Pointer to the DMA transfer structure. |
| kStatus_Success | Start a ESAI eDMA send successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_TxBusy | ESAI is busy sending data. |
| status_t ESAI_TransferReceiveEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| esai_transfer_t * | xfer | ||
| ) |
| base | ESAI base pointer |
| handle | ESAI eDMA handle pointer. |
| xfer | Pointer to DMA transfer structure. |
| kStatus_Success | Start a ESAI eDMA receive successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_RxBusy | ESAI is busy receiving data. |
| void ESAI_TransferAbortSendEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle | ||
| ) |
| base | ESAI base pointer. |
| handle | ESAI eDMA handle pointer. |
| void ESAI_TransferAbortReceiveEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle | ||
| ) |
| base | ESAI base pointer |
| handle | ESAI eDMA handle pointer. |
| status_t ESAI_TransferGetSendCountEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | ESAI base pointer. |
| handle | ESAI eDMA handle pointer. |
| count | Bytes count sent by ESAI. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |
| status_t ESAI_TransferGetReceiveCountEDMA | ( | ESAI_Type * | base, |
| esai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | ESAI base pointer |
| handle | ESAI eDMA handle pointer. |
| count | Bytes count received by ESAI. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |