The MCUXpresso SDK provides a peripheral driver for the CACHE Controller of MCUXpresso SDK devices.
The CACHE driver is created to help the user more easily operate the cache memory. The APIs for basic operations are including the following three levels: 1L. The L1 cache driver API. This level provides the level 1 caches controller drivers. The L1 caches in this arch is the previous the local memory controller (LMEM).
2L. The unified cache driver API. This level provides many APIs for unified cache driver APIs for combined L1 and L2 cache maintain operations. This is provided for SDK drivers (DMA, ENET, USDHC, etc) which should do the cache maintenance in their transactional APIs. Because in this arch, there is no L2 cache so the unified cache driver API directly calls only L1 driver APIs.
Function groups
L1 CACHE Operation {#L1CACHE MaintainOperation}
The L1 CACHE has both code cache and data cache. This function group provides two independent API groups for both code cache and data cache. There are Enable/Disable APIs for code cache and data cache control and cache maintenance operations as Invalidate/Clean/CleanInvalidate by all and by address range.
| #define FSL_CACHE_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
| #define L1CODEBUSCACHE_LINESIZE_BYTE FSL_FEATURE_L1ICACHE_LINESIZE_BYTE |
The code bus CACHE line size is 16B = 128b.
| void L1CACHE_InvalidateCodeCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be invalidated. |
- Note
- Address and size should be aligned to "L1CODCACHE_LINESIZE_BYTE". The startAddr here will be forced to align to L1CODEBUSCACHE_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| void L1CACHE_CleanCodeCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be cleaned. |
- Note
- Address and size should be aligned to "L1CODEBUSCACHE_LINESIZE_BYTE". The startAddr here will be forced to align to L1CODEBUSCACHE_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| void L1CACHE_CleanInvalidateCodeCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be Cleaned and Invalidated. |
- Note
- Address and size should be aligned to "L1CODEBUSCACHE_LINESIZE_BYTE". The startAddr here will be forced to align to L1CODEBUSCACHE_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void L1CACHE_EnableCodeCacheWriteBuffer |
( |
bool |
enable | ) |
|
|
inlinestatic |
- Parameters
-
| enable | The enable or disable flag. true - enable the code bus write buffer. false - disable the code bus write buffer. |
| void L1CACHE_InvalidateSystemCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be invalidated. |
- Note
- Address and size should be aligned to "L1SYSTEMBUSCACHE_LINESIZE_BYTE". The startAddr here will be forced to align to L1SYSTEMBUSCACHE_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| void L1CACHE_CleanSystemCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be cleaned. |
- Note
- Address and size should be aligned to "L1SYSTEMBUSCACHE_LINESIZE_BYTE". The startAddr here will be forced to align to L1SYSTEMBUSCACHE_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| void L1CACHE_CleanInvalidateSystemCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The physical address of cache. |
| size_byte | size of the memory to be Clean and Invalidated. |
- Note
- Address and size should be aligned to "L1SYSTEMBUSCACHE_LINESIZE_BYTE". The startAddr here will be forced to align to L1SYSTEMBUSCACHE_LINESIZE_BYTE if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void L1CACHE_EnableSystemCacheWriteBuffer |
( |
bool |
enable | ) |
|
|
inlinestatic |
- Parameters
-
| enable | The enable or disable flag. true - enable the code bus write buffer. false - disable the code bus write buffer. |
| void L1CACHE_InvalidateICacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The start address of the memory to be invalidated. |
| size_byte | The memory size. |
- Note
- The start address and size_byte should be 16-Byte(FSL_FEATURE_L1ICACHE_LINESIZE_BYTE) aligned.
| static void L1CACHE_InvalidateDCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The start address of the memory to be invalidated. |
| size_byte | The memory size. |
- Note
- The start address and size_byte should be 16-Byte(FSL_FEATURE_L1DCACHE_LINESIZE_BYTE) aligned.
| void L1CACHE_CleanDCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The start address of the memory to be cleaned. |
| size_byte | The memory size. |
- Note
- The start address and size_byte should be 16-Byte(FSL_FEATURE_L1DCACHE_LINESIZE_BYTE) aligned.
| void L1CACHE_CleanInvalidateDCacheByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
- Parameters
-
| address | The start address of the memory to be clean and invalidated. |
| size_byte | The memory size. |
- Note
- The start address and size_byte should be 16-Byte(FSL_FEATURE_L1DCACHE_LINESIZE_BYTE) aligned.
| static void ICACHE_InvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be invalidated. |
- Note
- Address and size should be aligned to 16-Byte due to the cache operation unit FSL_FEATURE_L1ICACHE_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void DCACHE_InvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be invalidated. |
- Note
- Address and size should be aligned to 16-Byte due to the cache operation unit FSL_FEATURE_L1DCACHE_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void DCACHE_CleanByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be cleaned. |
- Note
- Address and size should be aligned to 16-Byte due to the cache operation unit FSL_FEATURE_L1DCACHE_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.
| static void DCACHE_CleanInvalidateByRange |
( |
uint32_t |
address, |
|
|
uint32_t |
size_byte |
|
) |
| |
|
inlinestatic |
- Parameters
-
| address | The physical address. |
| size_byte | size of the memory to be Cleaned and Invalidated. |
- Note
- Address and size should be aligned to 16-Byte due to the cache operation unit FSL_FEATURE_L1DCACHE_LINESIZE_BYTE. The startAddr here will be forced to align to the cache line size if startAddr is not aligned. For the size_byte, application should make sure the alignment or make sure the right operation order if the size_byte is not aligned.