![]() |
MCUXpresso SDK API Reference Manual
Rev. 1
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Interrupt Request Steering (IRQSTEER) module of MCUXpresso SDK devices. The IrqSteer module redirects/steers the incoming interrupts to output interrupts of a selected/designated channel as specified by a set of configuration registers.
Macros | |
| #define | IRQSTEER_INT_SRC_REG_WIDTH 32U |
| IRQSTEER interrupt source register width. More... | |
| #define | IRQSTEER_INT_SRC_REG_INDEX(irq) |
| IRQSTEER interrupt source mapping register index. More... | |
| #define | IRQSTEER_INT_SRC_BIT_OFFSET(irq) ((irq - FSL_FEATURE_IRQSTEER_IRQ_START_INDEX) % IRQSTEER_INT_SRC_REG_WIDTH) |
| IRQSTEER interrupt source mapping bit offset. More... | |
| #define | IRQSTEER_INT_SRC_NUM(regIndex, bitOffset) (((FSL_FEATURE_IRQSTEER_CHn_MASK_COUNT - 1U - (regIndex)) * IRQSTEER_INT_SRC_REG_WIDTH) + (bitOffset)) |
| IRQSTEER interrupt source number. More... | |
Driver version | |
| #define | FSL_IRQSTEER_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
| < Version 2.0.1. More... | |
Initialization and deinitialization | |
| void | IRQSTEER_Init (IRQSTEER_Type *base) |
| Initializes the IRQSTEER module. More... | |
| void | IRQSTEER_Deinit (IRQSTEER_Type *base) |
| Deinitializes an IRQSTEER instance for operation. More... | |
Sources | |
| static void | IRQSTEER_EnableInterrupt (IRQSTEER_Type *base, IRQn_Type irq) |
| Enables an interrupt source. More... | |
| static void | IRQSTEER_DisableInterrupt (IRQSTEER_Type *base, IRQn_Type irq) |
| Disables an interrupt source. More... | |
| static void | IRQSTEER_SetInterrupt (IRQSTEER_Type *base, IRQn_Type irq, bool set) |
| Sets/Forces an interrupt. More... | |
| static void | IRQSTEER_EnableMasterInterrupt (IRQSTEER_Type *base, irqsteer_int_master_t intMasterIndex) |
| Enables a master interrupt. More... | |
| static void | IRQSTEER_DisableMasterInterrupt (IRQSTEER_Type *base, irqsteer_int_master_t intMasterIndex) |
| Disables a master interrupt. More... | |
Status | |
| static bool | IRQSTEER_IsInterruptSet (IRQSTEER_Type *base, IRQn_Type irq) |
| Checks the status of one specific IRQSTEER interrupt. More... | |
| static bool | IRQSTEER_IsMasterInterruptSet (IRQSTEER_Type *base) |
| Checks the status of IRQSTEER master interrupt. More... | |
| static uint32_t | IRQSTEER_GetGroupInterruptStatus (IRQSTEER_Type *base, irqsteer_int_group_t intGroupIndex) |
| Gets the status of IRQSTEER group interrupt. More... | |
| IRQn_Type | IRQSTEER_GetMasterNextInterrupt (IRQSTEER_Type *base, irqsteer_int_master_t intMasterIndex) |
| Gets the next interrupt source (currently set) of one specific master. More... | |
| #define FSL_IRQSTEER_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
| #define IRQSTEER_INT_SRC_REG_WIDTH 32U |
| #define IRQSTEER_INT_SRC_REG_INDEX | ( | irq | ) |
| #define IRQSTEER_INT_SRC_BIT_OFFSET | ( | irq | ) | ((irq - FSL_FEATURE_IRQSTEER_IRQ_START_INDEX) % IRQSTEER_INT_SRC_REG_WIDTH) |
| #define IRQSTEER_INT_SRC_NUM | ( | regIndex, | |
| bitOffset | |||
| ) | (((FSL_FEATURE_IRQSTEER_CHn_MASK_COUNT - 1U - (regIndex)) * IRQSTEER_INT_SRC_REG_WIDTH) + (bitOffset)) |
| enum irqsteer_int_group_t |
| void IRQSTEER_Init | ( | IRQSTEER_Type * | base | ) |
This function enables the clock gate for the specified IRQSTEER.
| base | IRQSTEER peripheral base address. |
| void IRQSTEER_Deinit | ( | IRQSTEER_Type * | base | ) |
The clock gate for the specified IRQSTEER is disabled.
| base | IRQSTEER peripheral base address. |
|
inlinestatic |
| base | IRQSTEER peripheral base address. |
| irq | Interrupt to be routed. The interrupt must be an IRQSTEER source. |
|
inlinestatic |
| base | IRQSTEER peripheral base address. |
| intSrc | Interrupt source number. The interrupt must be an IRQSTEER source. |
|
inlinestatic |
| base | IRQSTEER peripheral base address. |
| intSrc | Interrupt to be set/forced. The interrupt must be an IRQSTEER source. |
| set | Switcher of the interrupt set/force function. "true" means to set. "false" means not (normal operation). |
|
inlinestatic |
By default, all the master interrupts are enabled.
| base | IRQSTEER peripheral base address. |
| intMasterIndex | Master index of interrupt sources to be routed. "irqsteer_int_master_t". |
For example, to enable the interrupt sources of master 1:
|
inlinestatic |
| base | IRQSTEER peripheral base address. |
| intMasterIndex | Master index of interrupt sources to be disabled. "irqsteer_int_master_t". |
For example, to disable the interrupt sources of master 1:
|
inlinestatic |
| base | IRQSTEER peripheral base address. |
| intSrc | Interrupt source status to be checked. The interrupt must be an IRQSTEER source. |
For example, to check whether interrupt from output 0 of Display 1 is set:
|
inlinestatic |
The master interrupt status represents at least one interrupt is asserted or not among ALL interrupts.
| base | IRQSTEER peripheral base address. |
|
inlinestatic |
The group interrupt status represents all the interrupt status within the group specified. This API aims for facilitating the status return of one set of interrupts.
| base | IRQSTEER peripheral base address. |
| intGroupIndex | Index of the interrupt group status to get. |
| IRQn_Type IRQSTEER_GetMasterNextInterrupt | ( | IRQSTEER_Type * | base, |
| irqsteer_int_master_t | intMasterIndex | ||
| ) |
| base | IRQSTEER peripheral base address. |
| intMasterIndex | Master index of interrupt sources. "irqsteer_int_master_t". |