The MCUXpresso SDK provides a driver for the MU module of MCUXpresso SDK devices.
Function description
The MU driver provides these functions:
- Functions to initialize the MU module.
- Functions to send and receive messages.
- Functions for MU flags for both MU sides.
- Functions for status flags and interrupts.
- Other miscellaneous functions.
MU initialization
The function MU_Init() initializes the MU module and enables the MU clock. It should be called before any other MU functions.
The function MU_Deinit() deinitializes the MU module and disables the MU clock. No MU functions can be called after this function.
MU message
The MU message must be sent when the transmit register is empty. The MU driver provides blocking API and non-blocking API to send message.
The MU_SendMsgNonBlocking() function writes a message to the MU transmit register without checking the transmit register status. The upper layer should check that the transmit register is empty before calling this function. This function can be used in the ISR for better performance.
The MU_SendMsg() function is a blocking function. It waits until the transmit register is empty and sends the message.
Correspondingly, there are blocking and non-blocking APIs for receiving a message. The MU_ReadMsgNonBlocking() function is a non-blocking API. The MU_ReadMsg() function is the blocking API.
MU flags
The MU driver provides 3-bit general purpose flags. When the flags are set on one side, they are reflected on the other side.
The MU flags must be set when the previous flags have been updated to the other side. The MU driver provides a non-blocking function and a blocking function. The blocking function MU_SetFlags() waits until previous flags have been updated to the other side and then sets flags. The non-blocking function sets the flags directly. Ensure that the kMU_FlagsUpdatingFlag is not pending before calling this function.
The function MU_GetFlags() gets the MU flags on the current side.
Status and interrupt
The function MU_GetStatusFlags() returns all MU status flags. Use the _mu_status_flags to check for specific flags, for example, to check RX0 and RX1 register full, use the following code:
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mu The receive full flags are cleared automatically after messages are read out. The transmit empty flags are cleared automatically after new messages are written to the transmit register. The general purpose interrupt flags must be cleared manually using the function MU_ClearStatusFlags().
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mu To enable or disable a specific interrupt, use MU_EnableInterrupts() and MU_DisableInterrupts() functions. The interrupts to enable or disable should be passed in as a bit mask of the _mu_interrupt_enable.
The MU_TriggerInterrupts() function triggers general purpose interrupts and NMI to the other core. The interrupts to trigger are passed in as a bit mask of the _mu_interrupt_trigger. If previously triggered interrupts have not been processed by the other side, this function returns an error.
MU misc functions
The MU_BootCoreB() and MU_HoldCoreBReset() functions should only be used from A side. They are used to boot the core B or to hold core B in reset.
The MU_ResetBothSides() function resets MU at both A and B sides. However, only the A side can call this function.
If a core enters stop mode, the platform clock of this core is disabled by default. The function MU_SetClockOnOtherCoreEnable() forces the other core's platform clock to remain enabled even after that core has entered a stop mode. In this case, the other core's platform clock keeps running until the current core enters stop mode too.
Function MU_GetOtherCorePowerMode() gets the power mode of the other core.
|
| enum | _mu_status_flags {
kMU_Tx0EmptyFlag = (1U << (MU_SR_TEn_SHIFT + 3U)),
kMU_Tx1EmptyFlag = (1U << (MU_SR_TEn_SHIFT + 2U)),
kMU_Tx2EmptyFlag = (1U << (MU_SR_TEn_SHIFT + 1U)),
kMU_Tx3EmptyFlag = (1U << (MU_SR_TEn_SHIFT + 0U)),
kMU_Rx0FullFlag = (1U << (MU_SR_RFn_SHIFT + 3U)),
kMU_Rx1FullFlag = (1U << (MU_SR_RFn_SHIFT + 2U)),
kMU_Rx2FullFlag = (1U << (MU_SR_RFn_SHIFT + 1U)),
kMU_Rx3FullFlag = (1U << (MU_SR_RFn_SHIFT + 0U)),
kMU_GenInt0Flag = (1U << (MU_SR_GIPn_SHIFT + 3U)),
kMU_GenInt1Flag = (1U << (MU_SR_GIPn_SHIFT + 2U)),
kMU_GenInt2Flag = (1U << (MU_SR_GIPn_SHIFT + 1U)),
kMU_GenInt3Flag = (1U << (MU_SR_GIPn_SHIFT + 0U)),
kMU_EventPendingFlag = MU_SR_EP_MASK,
kMU_FlagsUpdatingFlag = MU_SR_FUP_MASK
} |
| | MU status flags. More...
|
| |
| enum | _mu_interrupt_enable {
kMU_Tx0EmptyInterruptEnable = (1U << (MU_CR_TIEn_SHIFT + 3U)),
kMU_Tx1EmptyInterruptEnable = (1U << (MU_CR_TIEn_SHIFT + 2U)),
kMU_Tx2EmptyInterruptEnable = (1U << (MU_CR_TIEn_SHIFT + 1U)),
kMU_Tx3EmptyInterruptEnable = (1U << (MU_CR_TIEn_SHIFT + 0U)),
kMU_Rx0FullInterruptEnable = (1U << (MU_CR_RIEn_SHIFT + 3U)),
kMU_Rx1FullInterruptEnable = (1U << (MU_CR_RIEn_SHIFT + 2U)),
kMU_Rx2FullInterruptEnable = (1U << (MU_CR_RIEn_SHIFT + 1U)),
kMU_Rx3FullInterruptEnable = (1U << (MU_CR_RIEn_SHIFT + 0U)),
kMU_GenInt0InterruptEnable = (1U << (MU_CR_GIEn_SHIFT + 3U)),
kMU_GenInt1InterruptEnable = (1U << (MU_CR_GIEn_SHIFT + 2U)),
kMU_GenInt2InterruptEnable = (1U << (MU_CR_GIEn_SHIFT + 1U)),
kMU_GenInt3InterruptEnable = (1U << (MU_CR_GIEn_SHIFT + 0U))
} |
| | MU interrupt source to enable. More...
|
| |
| enum | _mu_interrupt_trigger {
kMU_NmiInterruptTrigger = MU_CR_NMI_MASK,
kMU_GenInt0InterruptTrigger = (1U << (MU_CR_GIRn_SHIFT + 3U)),
kMU_GenInt1InterruptTrigger = (1U << (MU_CR_GIRn_SHIFT + 2U)),
kMU_GenInt2InterruptTrigger = (1U << (MU_CR_GIRn_SHIFT + 1U)),
kMU_GenInt3InterruptTrigger = (1U << (MU_CR_GIRn_SHIFT + 0U))
} |
| | MU interrupt that could be triggered to the other core. More...
|
| |
|
| static void | MU_SetFlagsNonBlocking (MU_Type *base, uint32_t flags) |
| | Sets the 3-bit MU flags reflect on the other MU side. More...
|
| |
| void | MU_SetFlags (MU_Type *base, uint32_t flags) |
| | Blocks setting the 3-bit MU flags reflect on the other MU side. More...
|
| |
| static uint32_t | MU_GetFlags (MU_Type *base) |
| | Gets the current value of the 3-bit MU flags set by the other side. More...
|
| |
| #define FSL_MU_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| Enumerator |
|---|
| kMU_Tx0EmptyFlag |
TX0 empty.
|
| kMU_Tx1EmptyFlag |
TX1 empty.
|
| kMU_Tx2EmptyFlag |
TX2 empty.
|
| kMU_Tx3EmptyFlag |
TX3 empty.
|
| kMU_Rx0FullFlag |
RX0 full.
|
| kMU_Rx1FullFlag |
RX1 full.
|
| kMU_Rx2FullFlag |
RX2 full.
|
| kMU_Rx3FullFlag |
RX3 full.
|
| kMU_GenInt0Flag |
General purpose interrupt 0 pending.
|
| kMU_GenInt1Flag |
General purpose interrupt 0 pending.
|
| kMU_GenInt2Flag |
General purpose interrupt 0 pending.
|
| kMU_GenInt3Flag |
General purpose interrupt 0 pending.
|
| kMU_EventPendingFlag |
MU event pending.
|
| kMU_FlagsUpdatingFlag |
MU flags update is on-going.
|
| Enumerator |
|---|
| kMU_Tx0EmptyInterruptEnable |
TX0 empty.
|
| kMU_Tx1EmptyInterruptEnable |
TX1 empty.
|
| kMU_Tx2EmptyInterruptEnable |
TX2 empty.
|
| kMU_Tx3EmptyInterruptEnable |
TX3 empty.
|
| kMU_Rx0FullInterruptEnable |
RX0 full.
|
| kMU_Rx1FullInterruptEnable |
RX1 full.
|
| kMU_Rx2FullInterruptEnable |
RX2 full.
|
| kMU_Rx3FullInterruptEnable |
RX3 full.
|
| kMU_GenInt0InterruptEnable |
General purpose interrupt 0.
|
| kMU_GenInt1InterruptEnable |
General purpose interrupt 1.
|
| kMU_GenInt2InterruptEnable |
General purpose interrupt 2.
|
| kMU_GenInt3InterruptEnable |
General purpose interrupt 3.
|
| Enumerator |
|---|
| kMU_NmiInterruptTrigger |
NMI interrupt.
|
| kMU_GenInt0InterruptTrigger |
General purpose interrupt 0.
|
| kMU_GenInt1InterruptTrigger |
General purpose interrupt 1.
|
| kMU_GenInt2InterruptTrigger |
General purpose interrupt 2.
|
| kMU_GenInt3InterruptTrigger |
General purpose interrupt 3.
|
| void MU_Init |
( |
MU_Type * |
base | ) |
|
This function enables the MU clock only.
- Parameters
-
| base | MU peripheral base address. |
| void MU_Deinit |
( |
MU_Type * |
base | ) |
|
This function disables the MU clock only.
- Parameters
-
| base | MU peripheral base address. |
| static void MU_SendMsgNonBlocking |
( |
MU_Type * |
base, |
|
|
uint32_t |
regIndex, |
|
|
uint32_t |
msg |
|
) |
| |
|
inlinestatic |
This function writes a message to the specific TX register. It does not check whether the TX register is empty or not. The upper layer should make sure the TX register is empty before calling this function. This function can be used in ISR for better performance.
- Parameters
-
| base | MU peripheral base address. |
| regIndex | TX register index. |
| msg | Message to send. |
| void MU_SendMsg |
( |
MU_Type * |
base, |
|
|
uint32_t |
regIndex, |
|
|
uint32_t |
msg |
|
) |
| |
This function waits until the TX register is empty and sends the message.
- Parameters
-
| base | MU peripheral base address. |
| regIndex | TX register index. |
| msg | Message to send. |
| static uint32_t MU_ReceiveMsgNonBlocking |
( |
MU_Type * |
base, |
|
|
uint32_t |
regIndex |
|
) |
| |
|
inlinestatic |
This function reads a message from the specific RX register. It does not check whether the RX register is full or not. The upper layer should make sure the RX register is full before calling this function. This function can be used in ISR for better performance.
* uint32_t msg;
* {
* }
*
*
- Parameters
-
| base | MU peripheral base address. |
| regIndex | TX register index. |
- Returns
- The received message.
| uint32_t MU_ReceiveMsg |
( |
MU_Type * |
base, |
|
|
uint32_t |
regIndex |
|
) |
| |
This function waits until the RX register is full and receives the message.
- Parameters
-
| base | MU peripheral base address. |
| regIndex | RX register index. |
- Returns
- The received message.
| static void MU_SetFlagsNonBlocking |
( |
MU_Type * |
base, |
|
|
uint32_t |
flags |
|
) |
| |
|
inlinestatic |
This function sets the 3-bit MU flags directly. Every time the 3-bit MU flags are changed, the status flag kMU_FlagsUpdatingFlag asserts indicating the 3-bit MU flags are updating to the other side. After the 3-bit MU flags are updated, the status flag kMU_FlagsUpdatingFlag is cleared by hardware. During the flags updating period, the flags cannot be changed. The upper layer should make sure the status flag kMU_FlagsUpdatingFlag is cleared before calling this function.
- Parameters
-
| base | MU peripheral base address. |
| flags | The 3-bit MU flags to set. |
| void MU_SetFlags |
( |
MU_Type * |
base, |
|
|
uint32_t |
flags |
|
) |
| |
This function blocks setting the 3-bit MU flags. Every time the 3-bit MU flags are changed, the status flag kMU_FlagsUpdatingFlag asserts indicating the 3-bit MU flags are updating to the other side. After the 3-bit MU flags are updated, the status flag kMU_FlagsUpdatingFlag is cleared by hardware. During the flags updating period, the flags cannot be changed. This function waits for the MU status flag kMU_FlagsUpdatingFlag cleared and sets the 3-bit MU flags.
- Parameters
-
| base | MU peripheral base address. |
| flags | The 3-bit MU flags to set. |
| static uint32_t MU_GetFlags |
( |
MU_Type * |
base | ) |
|
|
inlinestatic |
This function gets the current 3-bit MU flags on the current side.
- Parameters
-
| base | MU peripheral base address. |
- Returns
- flags Current value of the 3-bit flags.
| static uint32_t MU_GetStatusFlags |
( |
MU_Type * |
base | ) |
|
|
inlinestatic |
This function returns the bit mask of the MU status flags. See _mu_status_flags.
* uint32_t flags;
* {
*
* }
* {
*
* }
*
- Parameters
-
| base | MU peripheral base address. |
- Returns
- Bit mask of the MU status flags, see _mu_status_flags.
| static void MU_ClearStatusFlags |
( |
MU_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
This function clears the specific MU status flags. The flags to clear should be passed in as bit mask. See _mu_status_flags.
- Parameters
-
| base | MU peripheral base address. |
| mask | Bit mask of the MU status flags. See _mu_status_flags. The following flags are cleared by hardware, this function could not clear them.
- kMU_Tx0EmptyFlag
- kMU_Tx1EmptyFlag
- kMU_Tx2EmptyFlag
- kMU_Tx3EmptyFlag
- kMU_Rx0FullFlag
- kMU_Rx1FullFlag
- kMU_Rx2FullFlag
- kMU_Rx3FullFlag
- kMU_EventPendingFlag
- kMU_FlagsUpdatingFlag
- kMU_OtherSideInResetFlag
|
| static void MU_EnableInterrupts |
( |
MU_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
This function enables the specific MU interrupts. The interrupts to enable should be passed in as bit mask. See _mu_interrupt_enable.
- Parameters
-
| base | MU peripheral base address. |
| mask | Bit mask of the MU interrupts. See _mu_interrupt_enable. |
| static void MU_DisableInterrupts |
( |
MU_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
This function disables the specific MU interrupts. The interrupts to disable should be passed in as bit mask. See _mu_interrupt_enable.
- Parameters
-
| base | MU peripheral base address. |
| mask | Bit mask of the MU interrupts. See _mu_interrupt_enable. |
| status_t MU_TriggerInterrupts |
( |
MU_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
This function triggers the specific interrupts to the other core. The interrupts to trigger are passed in as bit mask. See _mu_interrupt_trigger. The MU should not trigger an interrupt to the other core when the previous interrupt has not been processed by the other core. This function checks whether the previous interrupts have been processed. If not, it returns an error.
- Parameters
-
| base | MU peripheral base address. |
| mask | Bit mask of the interrupts to trigger. See _mu_interrupt_trigger. |
- Return values
-
| kStatus_Success | Interrupts have been triggered successfully. |
| kStatus_Fail | Previous interrupts have not been accepted. |
| static void MU_ClearNmi |
( |
MU_Type * |
base | ) |
|
|
inlinestatic |
This function clears non-maskable interrupt (NMI) sent by the other core.
- Parameters
-
| base | MU peripheral base address. |
| void MU_BootCoreB |
( |
MU_Type * |
base, |
|
|
mu_core_boot_mode_t |
mode |
|
) |
| |
This function sets the B side core's boot configuration and releases the core from reset.
- Parameters
-
| base | MU peripheral base address. |
| mode | Core B boot mode. |
- Note
- Only MU side A can use this function.
| static void MU_HoldCoreBReset |
( |
MU_Type * |
base | ) |
|
|
inlinestatic |
This function causes the core of B side to be held in reset following any reset event.
- Parameters
-
| base | MU peripheral base address. |
- Note
- Only A side could call this function.
| void MU_BootOtherCore |
( |
MU_Type * |
base, |
|
|
mu_core_boot_mode_t |
mode |
|
) |
| |
This function boots the other core with a boot configuration.
- Parameters
-
| base | MU peripheral base address. |
| mode | The other core boot mode. |
| static void MU_HoldOtherCoreReset |
( |
MU_Type * |
base | ) |
|
|
inlinestatic |
This function causes the other core to be held in reset following any reset event.
- Parameters
-
| base | MU peripheral base address. |
| static void MU_ResetBothSides |
( |
MU_Type * |
base | ) |
|
|
inlinestatic |
This function resets the MU for both A side and B side. Before reset, it is recommended to interrupt processor B, because this function may affect the ongoing processor B programs.
- Parameters
-
| base | MU peripheral base address. |
- Note
- For some platforms, only MU side A could use this function, check reference manual for details.
| void MU_HardwareResetOtherCore |
( |
MU_Type * |
base, |
|
|
bool |
waitReset, |
|
|
bool |
holdReset, |
|
|
mu_core_boot_mode_t |
bootMode |
|
) |
| |
This function resets the other core, the other core could mask the hardware reset by calling MU_MaskHardwareReset. The hardware reset mask feature is only available for some platforms. This function could be used together with MU_BootOtherCore to control the other core reset workflow.
Example 1: Reset the other core, and no hold reset
In this example, the core at MU side B will reset with the specified boot mode.
Example 2: Reset the other core and hold it, then boot the other core later.
- Parameters
-
| base | MU peripheral base address. |
| waitReset | Wait the other core enters reset.
- true: Wait until the other core enters reset, if the other core has masked the hardware reset, then this function will be blocked.
- false: Don't wait the reset.
|
| holdReset | Hold the other core reset or not.
- true: Hold the other core in reset, this function returns directly when the other core enters reset.
- false: Don't hold the other core in reset, this function waits until the other core out of reset.
|
| bootMode | Boot mode of the other core, if holdReset is true, this parameter is useless. |
| static void MU_SetClockOnOtherCoreEnable |
( |
MU_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
This function enables or disables the platform clock on the other core when that core enters a stop mode. If disabled, the platform clock for the other core is disabled when it enters stop mode. If enabled, the platform clock keeps running on the other core in stop mode, until this core also enters stop mode.
- Parameters
-
| base | MU peripheral base address. |
| enable | Enable or disable the clock on the other core. |
| static mu_power_mode_t MU_GetOtherCorePowerMode |
( |
MU_Type * |
base | ) |
|
|
inlinestatic |
This function gets the power mode of the other core.
- Parameters
-
| base | MU peripheral base address. |
- Returns
- Power mode of the other core.