The MCUXpresso SDK provides a peripheral driver for the 10/100 Mbps Ethernet MAC (ENET) module of MCUXpresso SDK devices.
The MII interface is the interface connected with MAC and PHY. the Serial management interface - MII management interface should be set before any access to the external PHY chip register. Call ENET_SetSMI() to initialize MII management interface. Use ENET_StartSMIRead(), ENET_StartSMIWrite(), and ENET_ReadSMIData() to read/write to PHY registers. This function group sets up the MII and serial management SMI interface, gets data from the SMI interface, and starts the SMI read and write command. Use ENET_SetMII() to configure the MII before successfully getting data from the external PHY.
This group sets/gets the ENET mac address and the multicast group address filter. ENET_AddMulticastGroup() should be called to add the ENET MAC to the multicast group. The IEEE 1588 feature requires receiving the PTP message.
For ENET receive, the ENET_GetRxFrameSize() function must be called to get the received data size. Then, call the ENET_ReadFrame() function to get the received data. If the received error occurs, call the ENET_GetRxErrBeforeReadFrame() function after ENET_GetRxFrameSize() and before ENET_ReadFrame() functions to get the detailed error information.
For ENET transmit, call the ENET_SendFrame() function to send the data out. The transmit data error information is only accessible for the IEEE 1588 enhanced buffer descriptor mode. When the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE is defined, the ENET_GetTxErrAfterSendFrame() can be used to get the detail transmit error information. The transmit error information can only be updated by uDMA after the data is transmitted. The ENET_GetTxErrAfterSendFrame() function is recommended to be called on the transmit interrupt handler.
This function group configures the PTP IEEE 1588 feature, starts/stops/gets/sets/adjusts the PTP IEEE 1588 timer, gets the receive/transmit frame timestamp, and PTP IEEE 1588 timer channel feature setting.
The ENET_Ptp1588Configure() function must be called when the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE is defined and the IEEE 1588 feature is required. The ENET_GetRxFrameTime() and ENET_GetTxFrameTime() functions are called by the PTP stack to get the timestamp captured by the ENET driver.
Typical use case
ENET Initialization, receive, and transmit operations
For the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE undefined use case, use the legacy type buffer descriptor transmit/receive the frame as follows. 
  uint32_t length = 0;
  uint32_t sysClock;
  uint32_t phyAddr = 0;
  bool link = false;
  phy_speed_t speed;
  phy_duplex_t duplex;
  enet_status_t result;
  
  {
      ENET_RXBD_NUM,
      ENET_TXBD_NUM,
      ENET_BuffSizeAlign(ENET_RXBUFF_SIZE),
      ENET_BuffSizeAlign(ENET_TXBUFF_SIZE),
      &RxBuffDescrip[0],  
      &TxBuffDescrip[0],  
      &RxDataBuff[0][0],  
      &TxDataBuff[0][0],  
  };
  
  PHY_Init(EXAMPLE_ENET, 0, sysClock);
  
  PHY_GetLinkStatus(EXAMPLE_ENET, phyAddr, &link);
  if (link)
  {
      PHY_GetLinkSpeedDuplex(EXAMPLE_ENET, phyAddr, &speed, &duplex);
  }
  ENET_Init(EXAMPLE_ENET, &handle, &config, &buffCfg, &macAddr[0], sysClock);
 
  while (1)
  {
      
      
      if (length != 0)
      {
          
          uint8_t *data = (uint8_t *)malloc(length);
          
          .........
          free(data);
      }
      else if (result == kStatus_ENET_RxFrameErr)
      {
         
         
      }
     
     if(kStatus_Success == PHY_GetLinkStatus(EXAMPLE_ENET, phyAddr, &link))
     {
        if(link)
        {
        }
    }
}
 For the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE defined use case, add the PTP IEEE 1588 configuration to enable the PTP IEEE 1588 feature. The initialization occurs as follows. 
uint32_t length = 0;
uint32_t sysClock;
uint32_t phyAddr = 0;
bool link = false;
phy_speed_t speed;
phy_duplex_t duplex;
enet_status_t result;
enet_data_err_stats_t eErrStatic;
{
    ENET_RXBD_NUM,
    ENET_TXBD_NUM,
    ENET_BuffSizeAlign(ENET_RXBUFF_SIZE),
    ENET_BuffSizeAlign(ENET_TXBUFF_SIZE),
    &RxBuffDescrip[0],
    &TxBuffDescrip[0],
    &RxDataBuff[0][0],
    &TxDataBuff[0][0],
};
enet_ptp_config_t ptpConfig =
{
    ENET_RXBD_NUM,
    ENET_TXBD_NUM,
    &g_rxPtpTsBuff[0],
    &g_txPtpTsBuff[0],
    kENET_PtpTimerChannel1,
    ptpClock,
};
PHY_Init(EXAMPLE_ENET, 0, sysClock);
PHY_GetLinkStatus(EXAMPLE_ENET, phyAddr, &link);
if (link)
{
    PHY_GetLinkSpeedDuplex(EXAMPLE_ENET, phyAddr, &speed, &duplex);
}
ENET_Init(EXAMPLE_ENET, &handle, &config, &buffCfg, &macAddr[0], sysClock);
 
ENET_Ptp1588Configure(EXAMPLE_ENET, &handle, &ptpConfig);
  
 | 
| enum   | _enet_status {  
  kStatus_ENET_RxFrameError = MAKE_STATUS(kStatusGroup_ENET, 0U), 
 
  kStatus_ENET_RxFrameFail = MAKE_STATUS(kStatusGroup_ENET, 1U), 
 
  kStatus_ENET_RxFrameEmpty = MAKE_STATUS(kStatusGroup_ENET, 2U), 
 
  kStatus_ENET_TxFrameBusy, 
 
  kStatus_ENET_TxFrameFail = MAKE_STATUS(kStatusGroup_ENET, 4U)
 
 } | 
|   | Defines the status return codes for transaction.  More...
  | 
|   | 
| enum   | enet_mii_mode_t {  
  kENET_MiiMode = 0U, 
 
  kENET_RmiiMode
 
 } | 
|   | Defines the RMII or MII mode for data interface between the MAC and the PHY.  More...
  | 
|   | 
| enum   | enet_mii_speed_t {  
  kENET_MiiSpeed10M = 0U, 
 
  kENET_MiiSpeed100M
 
 } | 
|   | Defines the 10 Mbps or 100 Mbps speed for the MII data interface.  More...
  | 
|   | 
| enum   | enet_mii_duplex_t {  
  kENET_MiiHalfDuplex = 0U, 
 
  kENET_MiiFullDuplex
 
 } | 
|   | Defines the half or full duplex for the MII data interface.  More...
  | 
|   | 
| enum   | enet_mii_write_t {  
  kENET_MiiWriteNoCompliant = 0U, 
 
  kENET_MiiWriteValidFrame
 
 } | 
|   | Defines the write operation for the MII management frame.  More...
  | 
|   | 
| enum   | enet_mii_read_t {  
  kENET_MiiReadValidFrame = 2U, 
 
  kENET_MiiReadNoCompliant = 3U
 
 } | 
|   | Defines the read operation for the MII management frame.  More...
  | 
|   | 
| enum   | enet_special_control_flag_t {  
  kENET_ControlFlowControlEnable = 0x0001U, 
 
  kENET_ControlRxPayloadCheckEnable = 0x0002U, 
 
  kENET_ControlRxPadRemoveEnable = 0x0004U, 
 
  kENET_ControlRxBroadCastRejectEnable = 0x0008U, 
 
  kENET_ControlMacAddrInsert = 0x0010U, 
 
  kENET_ControlStoreAndFwdDisable = 0x0020U, 
 
  kENET_ControlSMIPreambleDisable = 0x0040U, 
 
  kENET_ControlPromiscuousEnable = 0x0080U, 
 
  kENET_ControlMIILoopEnable = 0x0100U, 
 
  kENET_ControlVLANTagEnable = 0x0200U
 
 } | 
|   | Defines a special configuration for ENET MAC controller.  More...
  | 
|   | 
| enum   | enet_interrupt_enable_t {  
  kENET_BabrInterrupt = ENET_EIR_BABR_MASK, 
 
  kENET_BabtInterrupt = ENET_EIR_BABT_MASK, 
 
  kENET_GraceStopInterrupt = ENET_EIR_GRA_MASK, 
 
  kENET_TxFrameInterrupt = ENET_EIR_TXF_MASK, 
 
  kENET_TxBufferInterrupt = ENET_EIR_TXB_MASK, 
 
  kENET_RxFrameInterrupt = ENET_EIR_RXF_MASK, 
 
  kENET_RxBufferInterrupt = ENET_EIR_RXB_MASK, 
 
  kENET_MiiInterrupt = ENET_EIR_MII_MASK, 
 
  kENET_EBusERInterrupt = ENET_EIR_EBERR_MASK, 
 
  kENET_LateCollisionInterrupt = ENET_EIR_LC_MASK, 
 
  kENET_RetryLimitInterrupt = ENET_EIR_RL_MASK, 
 
  kENET_UnderrunInterrupt = ENET_EIR_UN_MASK, 
 
  kENET_PayloadRxInterrupt = ENET_EIR_PLR_MASK, 
 
  kENET_WakeupInterrupt = ENET_EIR_WAKEUP_MASK, 
 
  kENET_TsAvailInterrupt = ENET_EIR_TS_AVAIL_MASK, 
 
  kENET_TsTimerInterrupt = ENET_EIR_TS_TIMER_MASK
 
 } | 
|   | List of interrupts supported by the peripheral.  More...
  | 
|   | 
| enum   | enet_event_t {  
  kENET_RxEvent, 
 
  kENET_TxEvent, 
 
  kENET_ErrEvent, 
 
  kENET_WakeUpEvent, 
 
  kENET_TimeStampEvent, 
 
  kENET_TimeStampAvailEvent
 
 } | 
|   | Defines the common interrupt event for callback use.  More...
  | 
|   | 
| enum   | enet_tx_accelerator_t {  
  kENET_TxAccelIsShift16Enabled = ENET_TACC_SHIFT16_MASK, 
 
  kENET_TxAccelIpCheckEnabled = ENET_TACC_IPCHK_MASK, 
 
  kENET_TxAccelProtoCheckEnabled = ENET_TACC_PROCHK_MASK
 
 } | 
|   | Defines the transmit accelerator configuration.  More...
  | 
|   | 
| enum   | enet_rx_accelerator_t {  
  kENET_RxAccelPadRemoveEnabled = ENET_RACC_PADREM_MASK, 
 
  kENET_RxAccelIpCheckEnabled = ENET_RACC_IPDIS_MASK, 
 
  kENET_RxAccelProtoCheckEnabled = ENET_RACC_PRODIS_MASK, 
 
  kENET_RxAccelMacCheckEnabled = ENET_RACC_LINEDIS_MASK, 
 
  kENET_RxAccelisShift16Enabled = ENET_RACC_SHIFT16_MASK
 
 } | 
|   | Defines the receive accelerator configuration.  More...
  | 
|   | 
 | 
| void  | ENET_SetMII (ENET_Type *base, enet_mii_speed_t speed, enet_mii_duplex_t duplex) | 
|   | Sets the ENET MII speed and duplex.  More...
  | 
|   | 
| void  | ENET_SetSMI (ENET_Type *base, uint32_t srcClock_Hz, bool isPreambleDisabled) | 
|   | Sets the ENET SMI (serial management interface) - MII management interface.  More...
  | 
|   | 
| static bool  | ENET_GetSMI (ENET_Type *base) | 
|   | Gets the ENET SMI- MII management interface configuration.  More...
  | 
|   | 
| static uint32_t  | ENET_ReadSMIData (ENET_Type *base) | 
|   | Reads data from the PHY register through an SMI interface.  More...
  | 
|   | 
| void  | ENET_StartSMIRead (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, enet_mii_read_t operation) | 
|   | Starts an SMI (Serial Management Interface) read command.  More...
  | 
|   | 
| void  | ENET_StartSMIWrite (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, enet_mii_write_t operation, uint32_t data) | 
|   | Starts an SMI write command.  More...
  | 
|   | 
 | 
| static void  | ENET_ActiveRead (ENET_Type *base) | 
|   | Activates ENET read or receive.  More...
  | 
|   | 
| static void  | ENET_EnableSleepMode (ENET_Type *base, bool enable) | 
|   | Enables/disables the MAC to enter sleep mode.  More...
  | 
|   | 
| static void  | ENET_GetAccelFunction (ENET_Type *base, uint32_t *txAccelOption, uint32_t *rxAccelOption) | 
|   | Gets ENET transmit and receive accelerator functions from the MAC controller.  More...
  | 
|   | 
 | 
| void  | ENET_SetCallback (enet_handle_t *handle, enet_callback_t callback, void *userData) | 
|   | Sets the callback function.  More...
  | 
|   | 
| void  | ENET_GetRxErrBeforeReadFrame (enet_handle_t *handle, enet_data_error_stats_t *eErrorStatic) | 
|   | Gets the ENET the error statistics of a received frame.  More...
  | 
|   | 
| status_t  | ENET_GetRxFrameSize (enet_handle_t *handle, uint32_t *length) | 
|   | Gets the size of the read frame.  More...
  | 
|   | 
| status_t  | ENET_ReadFrame (ENET_Type *base, enet_handle_t *handle, uint8_t *data, uint32_t length) | 
|   | Reads a frame from the ENET device.  More...
  | 
|   | 
| status_t  | ENET_SendFrame (ENET_Type *base, enet_handle_t *handle, uint8_t *data, uint32_t length) | 
|   | Transmits an ENET frame.  More...
  | 
|   | 
| void  | ENET_TransmitIRQHandler (ENET_Type *base, enet_handle_t *handle) | 
|   | The transmit IRQ handler.  More...
  | 
|   | 
| void  | ENET_ReceiveIRQHandler (ENET_Type *base, enet_handle_t *handle) | 
|   | The receive IRQ handler.  More...
  | 
|   | 
| void  | ENET_ErrorIRQHandler (ENET_Type *base, enet_handle_t *handle) | 
|   | The error IRQ handler.  More...
  | 
|   | 
| void  | ENET_CommonFrame0IRQHandler (ENET_Type *base) | 
|   | the common IRQ handler for the tx/rx/error etc irq handler.  More...
  | 
|   | 
      
        
          | struct enet_rx_bd_struct_t | 
        
      
 
      
        
          | uint16_t enet_rx_bd_struct_t::length | 
        
      
 
 
      
        
          | uint16_t enet_rx_bd_struct_t::control | 
        
      
 
 
      
        
          | uint8_t* enet_rx_bd_struct_t::buffer | 
        
      
 
 
 
 
      
        
          | struct enet_tx_bd_struct_t | 
        
      
 
      
        
          | uint16_t enet_tx_bd_struct_t::length | 
        
      
 
 
      
        
          | uint16_t enet_tx_bd_struct_t::control | 
        
      
 
 
      
        
          | uint8_t* enet_tx_bd_struct_t::buffer | 
        
      
 
 
 
 
      
        
          | struct enet_data_error_stats_t | 
        
      
 
      
        
          | uint32_t enet_data_error_stats_t::statsRxLenGreaterErr | 
        
      
 
 
      
        
          | uint32_t enet_data_error_stats_t::statsRxFcsErr | 
        
      
 
 
      
        
          | uint32_t enet_data_error_stats_t::statsRxOverRunErr | 
        
      
 
 
      
        
          | uint32_t enet_data_error_stats_t::statsRxTruncateErr | 
        
      
 
 
 
 
      
        
          | struct enet_buffer_config_t | 
        
      
 
Note that for the internal DMA requirements, the buffers have a corresponding alignment requirements.
- The aligned receive and transmit buffer size must be evenly divisible by ENET_BUFF_ALIGNMENT. when the data buffers are in cacheable region when cache is enabled, all those size should be aligned to the maximum value of "ENET_BUFF_ALIGNMENT" and the cache line size.
 
- The aligned transmit and receive buffer descriptor start address must be at least 64 bit aligned. However, it's recommended to be evenly divisible by ENET_BUFF_ALIGNMENT. buffer descriptors should be put in non-cacheable region when cache is enabled.
 
- The aligned transmit and receive data buffer start address must be evenly divisible by ENET_BUFF_ALIGNMENT. Receive buffers should be continuous with the total size equal to "rxBdNumber * rxBuffSizeAlign". Transmit buffers should be continuous with the total size equal to "txBdNumber * txBuffSizeAlign". when the data buffers are in cacheable region when cache is enabled, all those size should be aligned to the maximum value of "ENET_BUFF_ALIGNMENT" and the cache line size. 
 
 
      
        
          | uint16_t enet_buffer_config_t::rxBdNumber | 
        
      
 
 
      
        
          | uint16_t enet_buffer_config_t::txBdNumber | 
        
      
 
 
      
        
          | uint32_t enet_buffer_config_t::rxBuffSizeAlign | 
        
      
 
 
      
        
          | uint32_t enet_buffer_config_t::txBuffSizeAlign | 
        
      
 
 
      
        
          | uint8_t* enet_buffer_config_t::rxBufferAlign | 
        
      
 
 
      
        
          | uint8_t* enet_buffer_config_t::txBufferAlign | 
        
      
 
 
 
 
Note:
- macSpecialConfig is used for a special control configuration, a logical OR of "enet_special_control_flag_t". For a special configuration for MAC, set this parameter to 0.
 
- txWatermark is used for a cut-through operation. It is in steps of 64 bytes. 0/1 - 64 bytes written to TX FIFO before transmission of a frame begins. 2 - 128 bytes written to TX FIFO .... 3 - 192 bytes written to TX FIFO .... The maximum of txWatermark is 0x2F - 4032 bytes written to TX FIFO. txWatermark allows minimizing the transmit latency to set the txWatermark to 0 or 1 or for larger bus access latency 3 or larger due to contention for the system bus.
 
- rxFifoFullThreshold is similar to the txWatermark for cut-through operation in RX. It is in 64-bit words. The minimum is ENET_FIFO_MIN_RX_FULL and the maximum is 0xFF. If the end of the frame is stored in FIFO and the frame size if smaller than the txWatermark, the frame is still transmitted. The rule is the same for rxFifoFullThreshold in the receive direction.
 
- When "kENET_ControlFlowControlEnable" is set in the macSpecialConfig, ensure that the pauseDuration, rxFifoEmptyThreshold, and rxFifoStatEmptyThreshold are set for flow control enabled case.
 
- When "kENET_ControlStoreAndFwdDisabled" is set in the macSpecialConfig, ensure that the rxFifoFullThreshold and txFifoWatermark are set for store and forward disable.
 
- The rxAccelerConfig and txAccelerConfig default setting with 0 - accelerator are disabled. The "enet_tx_accelerator_t" and "enet_rx_accelerator_t" are recommended to be used to enable the transmit and receive accelerator. After the accelerators are enabled, the store and forward feature should be enabled. As a result, kENET_ControlStoreAndFwdDisabled should not be set. 
 
 
      
        
          | uint32_t enet_config_t::macSpecialConfig | 
        
      
 
A logical OR of "enet_special_control_flag_t". 
 
 
      
        
          | uint32_t enet_config_t::interrupt | 
        
      
 
A logical OR of "enet_interrupt_enable_t". 
 
 
      
        
          | uint16_t enet_config_t::rxMaxFrameLen | 
        
      
 
 
      
        
          | uint8_t enet_config_t::rxAccelerConfig | 
        
      
 
 
      
        
          | uint8_t enet_config_t::txAccelerConfig | 
        
      
 
 
      
        
          | uint16_t enet_config_t::pauseDuration | 
        
      
 
 
      
        
          | uint8_t enet_config_t::rxFifoEmptyThreshold | 
        
      
 
 
      
        
          | uint8_t enet_config_t::rxFifoStatEmptyThreshold | 
        
      
 
If the limit is reached, reception continues and a pause frame is triggered. 
 
 
      
        
          | uint8_t enet_config_t::rxFifoFullThreshold | 
        
      
 
 
      
        
          | uint8_t enet_config_t::txFifoWatermark | 
        
      
 
 
 
 
      
        
          | uint32_t enet_handle_t::rxBuffSizeAlign | 
        
      
 
 
      
        
          | uint32_t enet_handle_t::txBuffSizeAlign | 
        
      
 
 
      
        
          | void* enet_handle_t::userData | 
        
      
 
 
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_EMPTY_MASK   0x8000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_SOFTOWNER1_MASK   0x4000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_WRAP_MASK   0x2000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_SOFTOWNER2_Mask   0x1000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_LAST_MASK   0x0800U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_MISS_MASK   0x0100U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_BROADCAST_MASK   0x0080U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_MULTICAST_MASK   0x0040U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_LENVLIOLATE_MASK   0x0020U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_NOOCTET_MASK   0x0010U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_CRC_MASK   0x0004U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_OVERRUN_MASK   0x0002U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_TRUNC_MASK   0x0001U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_TX_READY_MASK   0x8000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_TX_SOFTOWENER1_MASK   0x4000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_TX_WRAP_MASK   0x2000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_TX_SOFTOWENER2_MASK   0x1000U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_TX_LAST_MASK   0x0800U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_TX_TRANMITCRC_MASK   0x0400U | 
        
      
 
 
      
        
          | #define ENET_BUFFDESCRIPTOR_RX_ERR_MASK | 
        
      
 
Value:
#define ENET_BUFFDESCRIPTOR_RX_LENVLIOLATE_MASK
Length violation mask. 
Definition: fsl_enet.h:61
 
#define ENET_BUFFDESCRIPTOR_RX_TRUNC_MASK
Frame is truncated mask. 
Definition: fsl_enet.h:65
 
#define ENET_BUFFDESCRIPTOR_RX_OVERRUN_MASK
FIFO overrun mask. 
Definition: fsl_enet.h:64
 
#define ENET_BUFFDESCRIPTOR_RX_NOOCTET_MASK
Non-octet aligned frame mask. 
Definition: fsl_enet.h:62
 
#define ENET_BUFFDESCRIPTOR_RX_CRC_MASK
CRC error mask. 
Definition: fsl_enet.h:63
 
 
 
 
      
        
          | #define ENET_FRAME_MAX_FRAMELEN   1518U | 
        
      
 
 
      
        
          | #define ENET_FIFO_MIN_RX_FULL   5U | 
        
      
 
 
      
        
          | #define ENET_RX_MIN_BUFFERSIZE   256U | 
        
      
 
 
      
        
          | #define ENET_PHY_MAXADDRESS   (ENET_MMFR_PA_MASK >> ENET_MMFR_PA_SHIFT) | 
        
      
 
 
      
        
          | typedef void(* enet_callback_t)(ENET_Type *base, enet_handle_t *handle, enet_event_t event, void *userData) | 
        
      
 
 
| Enumerator | 
|---|
| kStatus_ENET_RxFrameError  | 
 A frame received but data error happen.  
 | 
| kStatus_ENET_RxFrameFail  | 
 Failed to receive a frame.  
 | 
| kStatus_ENET_RxFrameEmpty  | 
 No frame arrive.  
 | 
| kStatus_ENET_TxFrameBusy  | 
 Transmit buffer descriptors are under process.  
 | 
| kStatus_ENET_TxFrameFail  | 
 Transmit frame fail.  
 | 
 
 
| Enumerator | 
|---|
| kENET_MiiMode  | 
 MII mode for data interface.  
 | 
| kENET_RmiiMode  | 
 RMII mode for data interface.  
 | 
 
 
| Enumerator | 
|---|
| kENET_MiiSpeed10M  | 
 Speed 10 Mbps.  
 | 
| kENET_MiiSpeed100M  | 
 Speed 100 Mbps.  
 | 
 
 
| Enumerator | 
|---|
| kENET_MiiHalfDuplex  | 
 Half duplex mode.  
 | 
| kENET_MiiFullDuplex  | 
 Full duplex mode.  
 | 
 
 
| Enumerator | 
|---|
| kENET_MiiWriteNoCompliant  | 
 Write frame operation, but not MII-compliant.  
 | 
| kENET_MiiWriteValidFrame  | 
 Write frame operation for a valid MII management frame.  
 | 
 
 
| Enumerator | 
|---|
| kENET_MiiReadValidFrame  | 
 Read frame operation for a valid MII management frame.  
 | 
| kENET_MiiReadNoCompliant  | 
 Read frame operation, but not MII-compliant.  
 | 
 
 
These control flags are provided for special user requirements. Normally, these control flags are unused for ENET initialization. For special requirements, set the flags to macSpecialConfig in the enet_config_t. The kENET_ControlStoreAndFwdDisable is used to disable the FIFO store and forward. FIFO store and forward means that the FIFO read/send is started when a complete frame is stored in TX/RX FIFO. If this flag is set, configure rxFifoFullThreshold and txFifoWatermark in the enet_config_t. 
| Enumerator | 
|---|
| kENET_ControlFlowControlEnable  | 
 Enable ENET flow control: pause frame.  
 | 
| kENET_ControlRxPayloadCheckEnable  | 
 Enable ENET receive payload length check.  
 | 
| kENET_ControlRxPadRemoveEnable  | 
 Padding is removed from received frames.  
 | 
| kENET_ControlRxBroadCastRejectEnable  | 
 Enable broadcast frame reject.  
 | 
| kENET_ControlMacAddrInsert  | 
 Enable MAC address insert.  
 | 
| kENET_ControlStoreAndFwdDisable  | 
 Enable FIFO store and forward.  
 | 
| kENET_ControlSMIPreambleDisable  | 
 Enable SMI preamble.  
 | 
| kENET_ControlPromiscuousEnable  | 
 Enable promiscuous mode.  
 | 
| kENET_ControlMIILoopEnable  | 
 Enable ENET MII loop back.  
 | 
| kENET_ControlVLANTagEnable  | 
 Enable VLAN tag frame.  
 | 
 
 
This enumeration uses one-bot encoding to allow a logical OR of multiple members. Members usually map to interrupt enable bits in one or more peripheral registers. 
| Enumerator | 
|---|
| kENET_BabrInterrupt  | 
 Babbling receive error interrupt source.  
 | 
| kENET_BabtInterrupt  | 
 Babbling transmit error interrupt source.  
 | 
| kENET_GraceStopInterrupt  | 
 Graceful stop complete interrupt source.  
 | 
| kENET_TxFrameInterrupt  | 
 TX FRAME interrupt source.  
 | 
| kENET_TxBufferInterrupt  | 
 TX BUFFER interrupt source.  
 | 
| kENET_RxFrameInterrupt  | 
 RX FRAME interrupt source.  
 | 
| kENET_RxBufferInterrupt  | 
 RX BUFFER interrupt source.  
 | 
| kENET_MiiInterrupt  | 
 MII interrupt source.  
 | 
| kENET_EBusERInterrupt  | 
 Ethernet bus error interrupt source.  
 | 
| kENET_LateCollisionInterrupt  | 
 Late collision interrupt source.  
 | 
| kENET_RetryLimitInterrupt  | 
 Collision Retry Limit interrupt source.  
 | 
| kENET_UnderrunInterrupt  | 
 Transmit FIFO underrun interrupt source.  
 | 
| kENET_PayloadRxInterrupt  | 
 Payload Receive interrupt source.  
 | 
| kENET_WakeupInterrupt  | 
 WAKEUP interrupt source.  
 | 
| kENET_TsAvailInterrupt  | 
 TS AVAIL interrupt source for PTP.  
 | 
| kENET_TsTimerInterrupt  | 
 TS WRAP interrupt source for PTP.  
 | 
 
 
| Enumerator | 
|---|
| kENET_RxEvent  | 
 Receive event.  
 | 
| kENET_TxEvent  | 
 Transmit event.  
 | 
| kENET_ErrEvent  | 
 Error event: BABR/BABT/EBERR/LC/RL/UN/PLR .  
 | 
| kENET_WakeUpEvent  | 
 Wake up from sleep mode event.  
 | 
| kENET_TimeStampEvent  | 
 Time stamp event.  
 | 
| kENET_TimeStampAvailEvent  | 
 Time stamp available event.  
 | 
 
 
| Enumerator | 
|---|
| kENET_TxAccelIsShift16Enabled  | 
 Transmit FIFO shift-16.  
 | 
| kENET_TxAccelIpCheckEnabled  | 
 Insert IP header checksum.  
 | 
| kENET_TxAccelProtoCheckEnabled  | 
 Insert protocol checksum.  
 | 
 
 
| Enumerator | 
|---|
| kENET_RxAccelPadRemoveEnabled  | 
 Padding removal for short IP frames.  
 | 
| kENET_RxAccelIpCheckEnabled  | 
 Discard with wrong IP header checksum.  
 | 
| kENET_RxAccelProtoCheckEnabled  | 
 Discard with wrong protocol checksum.  
 | 
| kENET_RxAccelMacCheckEnabled  | 
 Discard with Mac layer errors.  
 | 
| kENET_RxAccelisShift16Enabled  | 
 Receive FIFO shift-16.  
 | 
 
 
The purpose of this API is to get the default ENET MAC controller configuration structure for ENET_Init(). Users may use the initialized structure unchanged in ENET_Init() or modify fields of the structure before calling ENET_Init(). This is an example. 
 - Parameters
 - 
  
    | config | The ENET mac controller configuration structure pointer.  | 
  
   
 
 
      
        
          | void ENET_Init  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          enet_handle_t *  | 
          handle,  | 
        
        
           | 
           | 
          const enet_config_t *  | 
          config,  | 
        
        
           | 
           | 
          const enet_buffer_config_t *  | 
          bufferConfig,  | 
        
        
           | 
           | 
          uint8_t *  | 
          macAddr,  | 
        
        
           | 
           | 
          uint32_t  | 
          srcClock_Hz  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
This function ungates the module clock and initializes it with the ENET configuration.
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | handle | ENET handler pointer.  | 
    | config | ENET Mac configuration structure pointer. The "enet_config_t" type mac configuration return from ENET_GetDefaultConfig can be used directly. It is also possible to verify the Mac configuration using other methods.  | 
    | bufferConfig | ENET buffer configuration structure pointer. The buffer configuration should be prepared for ENET Initialization.  | 
    | macAddr | ENET mac address of the Ethernet device. This Mac address should be provided.  | 
    | srcClock_Hz | The internal module clock source for MII clock. | 
  
   
- Note
 - ENET has two buffer descriptors legacy buffer descriptors and enhanced IEEE 1588 buffer descriptors. The legacy descriptor is used by default. To use the IEEE 1588 feature, use the enhanced IEEE 1588 buffer descriptor by defining "ENET_ENHANCEDBUFFERDESCRIPTOR_MODE" and calling ENET_Ptp1588Configure() to configure the 1588 feature and related buffers after calling ENET_Init(). 
 
 
 
      
        
          | void ENET_Deinit  | 
          ( | 
          ENET_Type *  | 
          base | ) | 
           | 
        
      
 
This function gates the module clock, clears ENET interrupts, and disables the ENET module.
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
  
   
 
 
  
  
      
        
          | static void ENET_Reset  | 
          ( | 
          ENET_Type *  | 
          base | ) | 
           | 
         
       
   | 
  
inlinestatic   | 
  
 
This function restores the ENET module to the reset state. Note that this function sets all registers to the reset state. As a result, the ENET module can't work after calling this function.
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
  
   
 
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | speed | The speed of the RMII mode.  | 
    | duplex | The duplex of the RMII mode.  | 
  
   
 
 
      
        
          | void ENET_SetSMI  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint32_t  | 
          srcClock_Hz,  | 
        
        
           | 
           | 
          bool  | 
          isPreambleDisabled  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | srcClock_Hz | This is the ENET module clock frequency. Normally it's the system clock. See clock distribution.  | 
    | isPreambleDisabled | The preamble disable flag.
- true Enables the preamble.
 
- false Disables the preamble. 
 
 
 | 
  
   
 
 
  
  
      
        
          | static bool ENET_GetSMI  | 
          ( | 
          ENET_Type *  | 
          base | ) | 
           | 
         
       
   | 
  
inlinestatic   | 
  
 
This API is used to get the SMI configuration to check whether the MII management interface has been set.
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
  
   
- Returns
 - The SMI setup status true or false. 
 
 
 
  
  
      
        
          | static uint32_t ENET_ReadSMIData  | 
          ( | 
          ENET_Type *  | 
          base | ) | 
           | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
  
   
- Returns
 - The data read from PHY 
 
 
 
      
        
          | void ENET_StartSMIRead  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint32_t  | 
          phyAddr,  | 
        
        
           | 
           | 
          uint32_t  | 
          phyReg,  | 
        
        
           | 
           | 
          enet_mii_read_t  | 
          operation  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | phyAddr | The PHY address.  | 
    | phyReg | The PHY register.  | 
    | operation | The read operation.  | 
  
   
 
 
      
        
          | void ENET_StartSMIWrite  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint32_t  | 
          phyAddr,  | 
        
        
           | 
           | 
          uint32_t  | 
          phyReg,  | 
        
        
           | 
           | 
          enet_mii_write_t  | 
          operation,  | 
        
        
           | 
           | 
          uint32_t  | 
          data  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | phyAddr | The PHY address.  | 
    | phyReg | The PHY register.  | 
    | operation | The write operation.  | 
    | data | The data written to PHY.  | 
  
   
 
 
      
        
          | void ENET_SetMacAddr  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint8_t *  | 
          macAddr  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | macAddr | The six-byte Mac address pointer. The pointer is allocated by application and input into the API.  | 
  
   
 
 
      
        
          | void ENET_GetMacAddr  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint8_t *  | 
          macAddr  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | macAddr | The six-byte Mac address pointer. The pointer is allocated by application and input into the API.  | 
  
   
 
 
      
        
          | void ENET_AddMulticastGroup  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint8_t *  | 
          address  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | address | The six-byte multicast group address which is provided by application.  | 
  
   
 
 
      
        
          | void ENET_LeaveMulticastGroup  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint8_t *  | 
          address  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | address | The six-byte multicast group address which is provided by application.  | 
  
   
 
 
  
  
      
        
          | static void ENET_ActiveRead  | 
          ( | 
          ENET_Type *  | 
          base | ) | 
           | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | ENET peripheral base address. | 
  
   
- Note
 - This must be called after the MAC configuration and state are ready. It must be called after the ENET_Init() and ENET_Ptp1588Configure(). This should be called when the ENET receive required. 
 
 
 
  
  
      
        
          | static void ENET_EnableSleepMode  | 
          ( | 
          ENET_Type *  | 
          base,  | 
         
        
           | 
           | 
          bool  | 
          enable  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function is used to set the MAC enter sleep mode. When entering sleep mode, the magic frame wakeup interrupt should be enabled to wake up MAC from the sleep mode and reset it to normal mode.
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | enable | True enable sleep mode, false disable sleep mode.  | 
  
   
 
 
  
  
      
        
          | static void ENET_GetAccelFunction  | 
          ( | 
          ENET_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t *  | 
          txAccelOption,  | 
         
        
           | 
           | 
          uint32_t *  | 
          rxAccelOption  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | txAccelOption | The transmit accelerator option. The "enet_tx_accelerator_t" is recommended as the mask to get the exact the accelerator option.  | 
    | rxAccelOption | The receive accelerator option. The "enet_rx_accelerator_t" is recommended as the mask to get the exact the accelerator option.  | 
  
   
 
 
  
  
      
        
          | static void ENET_EnableInterrupts  | 
          ( | 
          ENET_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          mask  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function enables the ENET interrupt according to the provided mask. The mask is a logical OR of enumeration members. See enet_interrupt_enable_t. For example, to enable the TX frame interrupt and RX frame interrupt, do the following. 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | mask | ENET interrupts to enable. This is a logical OR of the enumeration :: enet_interrupt_enable_t.  | 
  
   
 
 
  
  
      
        
          | static void ENET_DisableInterrupts  | 
          ( | 
          ENET_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          mask  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function disables the ENET interrupts according to the provided mask. The mask is a logical OR of enumeration members. See enet_interrupt_enable_t. For example, to disable the TX frame interrupt and RX frame interrupt, do the following. 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | mask | ENET interrupts to disable. This is a logical OR of the enumeration :: enet_interrupt_enable_t.  | 
  
   
 
 
  
  
      
        
          | static uint32_t ENET_GetInterruptStatus  | 
          ( | 
          ENET_Type *  | 
          base | ) | 
           | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
  
   
- Returns
 - The event status of the interrupt source. This is the logical OR of members of the enumeration :: enet_interrupt_enable_t. 
 
 
 
  
  
      
        
          | static void ENET_ClearInterruptStatus  | 
          ( | 
          ENET_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          mask  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function clears enabled ENET interrupts according to the provided mask. The mask is a logical OR of enumeration members. See the enet_interrupt_enable_t. For example, to clear the TX frame interrupt and RX frame interrupt, do the following. 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | mask | ENET interrupt source to be cleared. This is the logical OR of members of the enumeration :: enet_interrupt_enable_t.  | 
  
   
 
 
      
        
          | void ENET_SetCallback  | 
          ( | 
          enet_handle_t *  | 
          handle,  | 
        
        
           | 
           | 
          enet_callback_t  | 
          callback,  | 
        
        
           | 
           | 
          void *  | 
          userData  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
This API is provided for the application callback required case when ENET interrupt is enabled. This API should be called after calling ENET_Init.
- Parameters
 - 
  
    | handle | ENET handler pointer. Should be provided by application.  | 
    | callback | The ENET callback function.  | 
    | userData | The callback function parameter.  | 
  
   
 
 
This API must be called after the ENET_GetRxFrameSize and before the ENET_ReadFrame(). If the ENET_GetRxFrameSize returns kStatus_ENET_RxFrameError, the ENET_GetRxErrBeforeReadFrame can be used to get the exact error statistics. This is an example. 
 - Parameters
 - 
  
    | handle | The ENET handler structure pointer. This is the same handler pointer used in the ENET_Init.  | 
    | eErrorStatic | The error statistics structure pointer.  | 
  
   
 
 
      
        
          | status_t ENET_GetRxFrameSize  | 
          ( | 
          enet_handle_t *  | 
          handle,  | 
        
        
           | 
           | 
          uint32_t *  | 
          length  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
This function gets a received frame size from the ENET buffer descriptors. 
- Note
 - The FCS of the frame is automatically removed by Mac and the size is the length without the FCS. After calling ENET_GetRxFrameSize, ENET_ReadFrame() should be called to update the receive buffers If the result is not "kStatus_ENET_RxFrameEmpty".
 
- Parameters
 - 
  
    | handle | The ENET handler structure. This is the same handler pointer used in the ENET_Init.  | 
    | length | The length of the valid frame received.  | 
  
   
- Return values
 - 
  
    | kStatus_ENET_RxFrameEmpty | No frame received. Should not call ENET_ReadFrame to read frame.  | 
    | kStatus_ENET_RxFrameError | Data error happens. ENET_ReadFrame should be called with NULL data and NULL length to update the receive buffers.  | 
    | kStatus_Success | Receive a frame Successfully then the ENET_ReadFrame should be called with the right data buffer and the captured data length input.  | 
  
   
 
 
      
        
          | status_t ENET_ReadFrame  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          enet_handle_t *  | 
          handle,  | 
        
        
           | 
           | 
          uint8_t *  | 
          data,  | 
        
        
           | 
           | 
          uint32_t  | 
          length  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
This function reads a frame (both the data and the length) from the ENET buffer descriptors. The ENET_GetRxFrameSize should be used to get the size of the prepared data buffer. This is an example. 
*       uint32_t length;
*       enet_handle_t g_handle;
*       
*       if (length != 0)
*       {
*           
*           uint8_t *data = memory allocate interface;
*           if (!data)
*           {
*               
*           }
*           else
*           {
*              
*           }
*       }
*       {
*          
*       }
* 
  - Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | handle | The ENET handler structure. This is the same handler pointer used in the ENET_Init.  | 
    | data | The data buffer provided by user to store the frame which memory size should be at least "length".  | 
    | length | The size of the data buffer which is still the length of the received frame.  | 
  
   
- Returns
 - The execute status, successful or failure. 
 
 
 
      
        
          | status_t ENET_SendFrame  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          enet_handle_t *  | 
          handle,  | 
        
        
           | 
           | 
          uint8_t *  | 
          data,  | 
        
        
           | 
           | 
          uint32_t  | 
          length  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Note
 - The CRC is automatically appended to the data. Input the data to send without the CRC.
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | handle | The ENET handler pointer. This is the same handler pointer used in the ENET_Init.  | 
    | data | The data buffer provided by user to be send.  | 
    | length | The length of the data to be send.  | 
  
   
- Return values
 - 
  
    | kStatus_Success | Send frame succeed.  | 
    | kStatus_ENET_TxFrameBusy | Transmit buffer descriptor is busy under transmission. The transmit busy happens when the data send rate is over the MAC capacity. The waiting mechanism is recommended to be added after each call return with kStatus_ENET_TxFrameBusy.  | 
  
   
 
 
      
        
          | void ENET_TransmitIRQHandler  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          enet_handle_t *  | 
          handle  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | handle | The ENET handler pointer.  | 
  
   
 
 
      
        
          | void ENET_ReceiveIRQHandler  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          enet_handle_t *  | 
          handle  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | handle | The ENET handler pointer.  | 
  
   
 
 
      
        
          | void ENET_ErrorIRQHandler  | 
          ( | 
          ENET_Type *  | 
          base,  | 
        
        
           | 
           | 
          enet_handle_t *  | 
          handle  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | base | ENET peripheral base address.  | 
    | handle | The ENET handler pointer.  | 
  
   
 
 
      
        
          | void ENET_CommonFrame0IRQHandler  | 
          ( | 
          ENET_Type *  | 
          base | ) | 
           | 
        
      
 
This is used for the combined tx/rx/error interrupt for single ring (ring 0).
- Parameters
 - 
  
    | base | ENET peripheral base address.  |