MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Quad Serial Peripheral Interface DMA Driver

Overview

Data Structures

struct  qspi_dma_handle_t
 QSPI DMA transfer handle, users should not touch the content of the handle. More...
 

Typedefs

typedef void(* qspi_dma_callback_t )(QuadSPI_Type *base, qspi_dma_handle_t *handle, status_t status, void *userData)
 QSPI DMA transfer callback function for finish and error.
 

Driver version

#define FSL_QSPI_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 QSPI DMA driver version 2.0.0. More...
 

DMA Transactional

void QSPI_TransferTxCreateHandleDMA (QuadSPI_Type *base, qspi_dma_handle_t *handle, qspi_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle)
 Initializes the QSPI handle for send which is used in transactional functions and set the callback. More...
 
status_t QSPI_TransferSendDMA (QuadSPI_Type *base, qspi_dma_handle_t *handle, qspi_transfer_t *xfer)
 Transfers QSPI data using an DMA non-blocking method. More...
 
void QSPI_TransferAbortSendDMA (QuadSPI_Type *base, qspi_dma_handle_t *handle)
 Aborts the sent data using DMA. More...
 
status_t QSPI_TransferGetSendCountDMA (QuadSPI_Type *base, qspi_dma_handle_t *handle, size_t *count)
 Gets the transferred counts of send. More...
 

Data Structure Documentation

struct _qspi_dma_handle

Data Fields

dma_handle_t * dmaHandle
 DMA handler start pointer for QSPI send.
 
size_t transferSize
 Bytes need to transfer. More...
 
uint32_t state
 Internal state for QSPI DMA transfer.
 
qspi_dma_callback_t callback
 Callback for users while transfer finish or error occurred.
 
void * userData
 User callback parameter.
 

Field Documentation

size_t qspi_dma_handle_t::transferSize

Macro Definition Documentation

#define FSL_QSPI_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Function Documentation

void QSPI_TransferTxCreateHandleDMA ( QuadSPI_Type *  base,
qspi_dma_handle_t *  handle,
qspi_dma_callback_t  callback,
void *  userData,
dma_handle_t *  dmaHandle 
)
Parameters
baseQSPI peripheral base address
handlePointer to qspi_dma_handle_t structure
callbackQSPI callback, NULL means no callback.
userDataUser callback function data.
dmaHandleUser requested DMA handle start pointer for DMA transfer
handleCountCount for dma Handle.
status_t QSPI_TransferSendDMA ( QuadSPI_Type *  base,
qspi_dma_handle_t *  handle,
qspi_transfer_t *  xfer 
)

This function writes data to the QSPI transmit FIFO. This function is non-blocking.

Parameters
basePointer to QuadSPI Type.
handlePointer to qspi_dma_handle_t structure
xferQSPI transfer structure.
void QSPI_TransferAbortSendDMA ( QuadSPI_Type *  base,
qspi_dma_handle_t *  handle 
)

This function aborts the sent data using DMA.

Parameters
baseQSPI peripheral base address.
handlePointer to qspi_dma_handle_t structure
status_t QSPI_TransferGetSendCountDMA ( QuadSPI_Type *  base,
qspi_dma_handle_t *  handle,
size_t *  count 
)
Parameters
basePointer to QuadSPI Type.
handlePointer to qspi_dma_handle_t structure.
countBytes sent.
Return values
kStatus_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.