MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
SDRAMC: Synchronous DRAM Controller Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Synchronous DRAM Controller block of MCUXpresso SDK devices.

The SDRAM controller commands include the initialization MRS command, precharge command, enter/exit self-refresh command, and enable/disable auto-refresh command. Use the SDRAMC_SendCommand() to send these commands to SDRAM to initialize it. The SDRAMC_EnableWriteProtect() is provided to enable/disable the write protection. The SDRAMC_EnableOperateValid() is provided to enable/disable the operation valid.

Typical use case

This example shows how to use the SDRAM Controller driver to initialize the external 16 bit port-size 8-column SDRAM chip. Initialize the SDRAM controller and run the initialization sequence. The external SDRAM is initialized and the SDRAM read and write is available.

First, initialize the SDRAM Controller. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sdramc Then, run the initialization sequence.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sdramc

Data Structures

struct  sdramc_blockctl_config_t
 SDRAM controller block control configuration structure. More...
 
struct  sdramc_refresh_config_t
 SDRAM controller refresh timing configuration structure. More...
 
struct  sdramc_config_t
 SDRAM controller configuration structure. More...
 

Enumerations

enum  sdramc_refresh_time_t {
  kSDRAMC_RefreshThreeClocks = 0x0U,
  kSDRAMC_RefreshSixClocks,
  kSDRAMC_RefreshNineClocks
}
 SDRAM controller auto-refresh timing. More...
 
enum  sdramc_latency_t {
  kSDRAMC_LatencyZero = 0x0U,
  kSDRAMC_LatencyOne,
  kSDRAMC_LatencyTwo,
  kSDRAMC_LatencyThree
}
 Setting latency for SDRAM controller timing specifications. More...
 
enum  sdramc_command_bit_location_t {
  kSDRAMC_Commandbit17 = 0x0U,
  kSDRAMC_Commandbit18,
  kSDRAMC_Commandbit19,
  kSDRAMC_Commandbit20,
  kSDRAMC_Commandbit21,
  kSDRAMC_Commandbit22,
  kSDRAMC_Commandbit23,
  kSDRAMC_Commandbit24
}
 SDRAM controller command bit location. More...
 
enum  sdramc_command_t {
  kSDRAMC_ImrsCommand = 0x0U,
  kSDRAMC_PrechargeCommand,
  kSDRAMC_SelfrefreshEnterCommand,
  kSDRAMC_SelfrefreshExitCommand,
  kSDRAMC_AutoRefreshEnableCommand,
  kSDRAMC_AutoRefreshDisableCommand
}
 SDRAM controller command. More...
 
enum  sdramc_port_size_t {
  kSDRAMC_PortSize32Bit = 0x0U,
  kSDRAMC_PortSize8Bit,
  kSDRAMC_PortSize16Bit
}
 SDRAM port size. More...
 
enum  sdramc_block_selection_t {
  kSDRAMC_Block0 = 0x0U,
  kSDRAMC_Block1
}
 SDRAM controller block selection. More...
 

Driver version

#define FSL_SDRAMC_DRIVER_VERSION   (MAKE_VERSION(2, 1, 0))
 SDRAMC driver version 2.1.0. More...
 

SDRAM Controller Initialization and De-initialization

void SDRAMC_Init (SDRAM_Type *base, sdramc_config_t *configure)
 Initializes the SDRAM controller. More...
 
void SDRAMC_Deinit (SDRAM_Type *base)
 Deinitializes the SDRAM controller module and gates the clock. More...
 

SDRAM Controller Basic Operation

void SDRAMC_SendCommand (SDRAM_Type *base, sdramc_block_selection_t block, sdramc_command_t command)
 Sends the SDRAM command. More...
 
static void SDRAMC_EnableWriteProtect (SDRAM_Type *base, sdramc_block_selection_t block, bool enable)
 Enables/disables the write protection. More...
 
static void SDRAMC_EnableOperateValid (SDRAM_Type *base, sdramc_block_selection_t block, bool enable)
 Enables/disables the valid operation. More...
 

Data Structure Documentation

struct sdramc_blockctl_config_t

Data Fields

sdramc_block_selection_t block
 The block number. More...
 
sdramc_port_size_t portSize
 The port size of the associated SDRAM block. More...
 
sdramc_command_bit_location_t location
 The command bit location. More...
 
sdramc_latency_t latency
 The latency for some timing specifications. More...
 
uint32_t address
 The base address of the SDRAM block. More...
 
uint32_t addressMask
 The base address mask of the SDRAM block. More...
 

Field Documentation

sdramc_block_selection_t sdramc_blockctl_config_t::block
sdramc_port_size_t sdramc_blockctl_config_t::portSize
sdramc_command_bit_location_t sdramc_blockctl_config_t::location
sdramc_latency_t sdramc_blockctl_config_t::latency
uint32_t sdramc_blockctl_config_t::address
uint32_t sdramc_blockctl_config_t::addressMask
struct sdramc_refresh_config_t

Data Fields

sdramc_refresh_time_t refreshTime
 Trc:The number of bus clocks inserted between a REF and next ACTIVE command. More...
 
uint32_t sdramRefreshRow
 The SDRAM refresh time each row: ns/row. More...
 
uint32_t busClock_Hz
 The bus clock for SDRAMC. More...
 

Field Documentation

sdramc_refresh_time_t sdramc_refresh_config_t::refreshTime
uint32_t sdramc_refresh_config_t::sdramRefreshRow
uint32_t sdramc_refresh_config_t::busClock_Hz
struct sdramc_config_t

Defines a configure structure and uses the SDRAMC_Configure() function to make necessary initializations.

Data Fields

sdramc_refresh_config_t * refreshConfig
 Refresh timing configure structure pointer. More...
 
sdramc_blockctl_config_t * blockConfig
 Block configure structure pointer. More...
 
uint8_t numBlockConfig
 SDRAM block numbers for configuration. More...
 

Field Documentation

sdramc_refresh_config_t* sdramc_config_t::refreshConfig
sdramc_blockctl_config_t* sdramc_config_t::blockConfig

If both SDRAM blocks are used, use the two continuous blockConfig.

uint8_t sdramc_config_t::numBlockConfig

Macro Definition Documentation

#define FSL_SDRAMC_DRIVER_VERSION   (MAKE_VERSION(2, 1, 0))

Enumeration Type Documentation

Enumerator
kSDRAMC_RefreshThreeClocks 

The refresh timing with three bus clocks.

kSDRAMC_RefreshSixClocks 

The refresh timing with six bus clocks.

kSDRAMC_RefreshNineClocks 

The refresh timing with nine bus clocks.

The latency setting affects the following SDRAM timing specifications:

  • trcd: SRAS assertion to SCAS assertion
  • tcasl: SCAS assertion to data out
  • tras: ACTV command to Precharge command
  • trp: Precharge command to ACTV command
  • trwl, trdl: Last data input to Precharge command
  • tep: Last data out to Precharge command
    The details of the latency setting and timing specifications are shown in the following table list.
    latency trcd: tcasl tras trp trwl,trdl tep
    0 1 bus clock 1 bus clock 2 bus clocks 1 bus clock 1 bus clock 1 bus clock
    1 2 bus clock 2 bus clock 4 bus clocks 2 bus clock 1 bus clock 1 bus clock
    2 3 bus clock 3 bus clock 6 bus clocks 3 bus clock 1 bus clock 1 bus clock
    3 3 bus clock 3 bus clock 6 bus clocks 3 bus clock 1 bus clock 1 bus clock
Enumerator
kSDRAMC_LatencyZero 

Latency 0.

kSDRAMC_LatencyOne 

Latency 1.

kSDRAMC_LatencyTwo 

Latency 2.

kSDRAMC_LatencyThree 

Latency 3.

Enumerator
kSDRAMC_Commandbit17 

Command bit location is bit 17.

kSDRAMC_Commandbit18 

Command bit location is bit 18.

kSDRAMC_Commandbit19 

Command bit location is bit 19.

kSDRAMC_Commandbit20 

Command bit location is bit 20.

kSDRAMC_Commandbit21 

Command bit location is bit 21.

kSDRAMC_Commandbit22 

Command bit location is bit 22.

kSDRAMC_Commandbit23 

Command bit location is bit 23.

kSDRAMC_Commandbit24 

Command bit location is bit 24.

Enumerator
kSDRAMC_ImrsCommand 

Initiate MRS command.

kSDRAMC_PrechargeCommand 

Initiate precharge command.

kSDRAMC_SelfrefreshEnterCommand 

Enter self-refresh command.

kSDRAMC_SelfrefreshExitCommand 

Exit self-refresh command.

kSDRAMC_AutoRefreshEnableCommand 

Enable Auto refresh command.

kSDRAMC_AutoRefreshDisableCommand 

Disable Auto refresh command.

Enumerator
kSDRAMC_PortSize32Bit 

32-Bit port size.

kSDRAMC_PortSize8Bit 

8-Bit port size.

kSDRAMC_PortSize16Bit 

16-Bit port size.

Enumerator
kSDRAMC_Block0 

Select SDRAM block 0.

kSDRAMC_Block1 

Select SDRAM block 1.

Function Documentation

void SDRAMC_Init ( SDRAM_Type *  base,
sdramc_config_t *  configure 
)

This function ungates the SDRAM controller clock and initializes the SDRAM controller. This function must be called before calling any other SDRAM controller driver functions. Example

refreshConfig.refreshTime = kSDRAM_RefreshThreeClocks;
refreshConfig.sdramRefreshRow = 15625;
refreshConfig.busClock = 60000000;
blockConfig.block = kSDRAMC_Block0;
blockConfig.address = SDRAM_START_ADDRESS;
blockConfig.addressMask = 0x7c0000;
config.refreshConfig = &refreshConfig,
config.blockConfig = &blockConfig,
config.totalBlocks = 1;
SDRAMC_Init(SDRAM, &config);
Parameters
baseSDRAM controller peripheral base address.
configureThe SDRAM configuration structure pointer.
void SDRAMC_Deinit ( SDRAM_Type *  base)

This function gates the SDRAM controller clock. As a result, the SDRAM controller module doesn't work after calling this function.

Parameters
baseSDRAM controller peripheral base address.
void SDRAMC_SendCommand ( SDRAM_Type *  base,
sdramc_block_selection_t  block,
sdramc_command_t  command 
)

This function sends commands to SDRAM. The commands are precharge command, initialization MRS command, auto-refresh enable/disable command, and self-refresh enter/exit commands. Note that the self-refresh enter/exit commands are all blocks setting and "block" is ignored. Ensure to set the correct "block" when send other commands.

Parameters
baseSDRAM controller peripheral base address.
blockThe block selection.
commandThe SDRAM command, see "sdramc_command_t". kSDRAMC_ImrsCommand - Initialize MRS command
kSDRAMC_PrechargeCommand - Initialize precharge command
kSDRAMC_SelfrefreshEnterCommand - Enter self-refresh command
kSDRAMC_SelfrefreshExitCommand - Exit self-refresh command
kSDRAMC_AutoRefreshEnableCommand - Enable auto refresh command
kSDRAMC_AutoRefreshDisableCommand - Disable auto refresh command
static void SDRAMC_EnableWriteProtect ( SDRAM_Type *  base,
sdramc_block_selection_t  block,
bool  enable 
)
inlinestatic
Parameters
baseSDRAM peripheral base address.
blockThe block which is selected.
enableTrue enable write protection, false disable write protection.
static void SDRAMC_EnableOperateValid ( SDRAM_Type *  base,
sdramc_block_selection_t  block,
bool  enable 
)
inlinestatic
Parameters
baseSDRAM peripheral base address.
blockThe block which is selected.
enableTrue enable the valid operation; false disable the valid operation.