MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
MCUXpresso SDK provides the Peripheral driver for the Cyclic Redundancy Check (CRC) module of MCUXpresso SDK devices.
The cyclic redundancy check (CRC) module generates 16/32-bit CRC code for error detection. The CRC module provides three variants of polynomials, a programmable seed and other parameters required to implement a 16-bit or 32-bit CRC standard.
CRC_Init() function enables the clock for the CRC module in the LPC SYSCON block and fully (re-)configures the CRC module according to configuration structure. It also starts checksum computation by writing the seed.
The seed member of the configuration structure is the initial checksum for which new data can be added to. When starting new checksum computation, the seed shall be set to the initial checksum per the CRC protocol specification. For continued checksum operation, the seed shall be set to the intermediate checksum value as obtained from previous calls to CRC_GetConfig() function. After CRC_Init(), one or multiple CRC_WriteData() calls follow to update checksum with data, then CRC_Get16bitResult() or CRC_Get32bitResult() follows to read the result. CRC_Init() can be called as many times as required, thus, allows for runtime changes of CRC protocol.
CRC_GetDefaultConfig() function can be used to set the module configuration structure with parameters for CRC-16/CCITT-FALSE protocol.
CRC_Deinit() function disables clock to the CRC module.
CRC_Reset() performs hardware reset of the CRC module.
The CRC_WriteData() function is used to add data to actual CRC. Internally it tries to use 32-bit reads and writes for all aligned data in the user buffer and it uses 8-bit reads and writes for all unaligned data in the user buffer. This function can update CRC with user supplied data chunks of arbitrary size, so one can update CRC byte by byte or with all bytes at once. Prior call of CRC configuration function CRC_Init() fully specifies the CRC module configuration for CRC_WriteData() call.
The CRC_Get16bitResult() or CRC_Get32bitResult() function is used to read the CRC module checksum register. The bit reverse and 1's complement operations are already applied to the result if previously configured. Use CRC_GetConfig() function to get the actual checksum without bit reverse and 1's complement applied so it can be used as seed when resuming calculation later.
CRC_Init() / CRC_WriteData() / CRC_Get16bitResult() to get final checksum.
CRC_Init() / CRC_WriteData() / ... / CRC_WriteData() / CRC_Get16bitResult() to get final checksum.
CRC_Init() / CRC_WriteData() / CRC_GetConfig() to get intermediate checksum to be used as seed value in future.
CRC_Init() / CRC_WriteData() / ... / CRC_WriteData() / CRC_GetConfig() to get intermediate checksum.
If multiple RTOS tasks share the CRC module to compute checksums with different data and/or protocols, the following needs to be implemented by the user:
The triplets
CRC_Init() / CRC_WriteData() / CRC_Get16bitResult() or CRC_Get32bitResult() or CRC_GetConfig()
shall be protected by RTOS mutex to protect CRC module against concurrent accesses from different tasks. Example:
Alternatively, the context switch handler could read original configuration and restore it when switching back to original task/thread:
All APIs can be used from interrupt handler although execution time shall be considered (interrupt latency of equal and lower priority interrupts increases). Protection against concurrent accesses from different interrupt handlers and/or tasks shall be assured by the user.
Simple example with default CRC-16/CCITT-FALSE protocol
Simple example with CRC-32 protocol configuration
Per-partes data updates with context switch between. Assuming we have 3 tasks/threads, each using CRC module to compute checksums of different protocol, with context switches.
Firstly, we prepare 3 CRC configurations for 3 different protocols: CRC-16 (ARC), CRC-16/CCITT-FALSE and CRC-32. Table below lists the individual protocol specifications. See also: http://reveng.sourceforge.net/crc-catalogue/
CRC-16/CCITT-FALSE | CRC-16 | CRC-32 | |
---|---|---|---|
Width | 16 bits | 16 bits | 32 bits |
Polynomial | 0x1021 | 0x8005 | 0x04C11DB7 |
Initial seed | 0xFFFF | 0x0000 | 0xFFFFFFFF |
Complement checksum | No | No | Yes |
Reflect In | No | Yes | Yes |
Reflect Out | No | Yes | Yes |
Corresponding functions to get configurations:
The following context switches show possible API usage:
Files | |
file | fsl_crc.h |
Data Structures | |
struct | crc_config_t |
CRC protocol configuration. More... | |
Macros | |
#define | CRC_DRIVER_USE_CRC16_CCITT_FALSE_AS_DEFAULT 1 |
Default configuration structure filled by CRC_GetDefaultConfig(). More... | |
Enumerations | |
enum | crc_polynomial_t { kCRC_Polynomial_CRC_CCITT = 0U, kCRC_Polynomial_CRC_16 = 1U, kCRC_Polynomial_CRC_32 = 2U } |
CRC polynomials to use. More... | |
Functions | |
void | CRC_Init (CRC_Type *base, const crc_config_t *config) |
Enables and configures the CRC peripheral module. More... | |
static void | CRC_Deinit (CRC_Type *base) |
Disables the CRC peripheral module. More... | |
void | CRC_Reset (CRC_Type *base) |
resets CRC peripheral module. More... | |
void | CRC_GetDefaultConfig (crc_config_t *config) |
Loads default values to CRC protocol configuration structure. More... | |
void | CRC_GetConfig (CRC_Type *base, crc_config_t *config) |
Loads actual values configured in CRC peripheral to CRC protocol configuration structure. More... | |
void | CRC_WriteData (CRC_Type *base, const uint8_t *data, size_t dataSize) |
Writes data to the CRC module. More... | |
static uint32_t | CRC_Get32bitResult (CRC_Type *base) |
Reads 32-bit checksum from the CRC module. More... | |
static uint16_t | CRC_Get16bitResult (CRC_Type *base) |
Reads 16-bit checksum from the CRC module. More... | |
Driver version | |
#define | FSL_CRC_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
CRC driver version. More... | |
struct crc_config_t |
This structure holds the configuration for the CRC protocol.
Data Fields | |
crc_polynomial_t | polynomial |
CRC polynomial. More... | |
bool | reverseIn |
Reverse bits on input. More... | |
bool | complementIn |
Perform 1's complement on input. More... | |
bool | reverseOut |
Reverse bits on output. More... | |
bool | complementOut |
Perform 1's complement on output. More... | |
uint32_t | seed |
Starting checksum value. More... | |
crc_polynomial_t crc_config_t::polynomial |
bool crc_config_t::reverseIn |
bool crc_config_t::complementIn |
bool crc_config_t::reverseOut |
bool crc_config_t::complementOut |
uint32_t crc_config_t::seed |
#define FSL_CRC_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
Version 2.0.1.
Current version: 2.0.1
Change log:
#define CRC_DRIVER_USE_CRC16_CCITT_FALSE_AS_DEFAULT 1 |
Uses CRC-16/CCITT-FALSE as default.
enum crc_polynomial_t |
void CRC_Init | ( | CRC_Type * | base, |
const crc_config_t * | config | ||
) |
This functions enables the CRC peripheral clock in the LPC SYSCON block. It also configures the CRC engine and starts checksum computation by writing the seed.
base | CRC peripheral address. |
config | CRC module configuration structure. |
|
inlinestatic |
This functions disables the CRC peripheral clock in the LPC SYSCON block.
base | CRC peripheral address. |
void CRC_Reset | ( | CRC_Type * | base | ) |
base | CRC peripheral address. |
void CRC_GetDefaultConfig | ( | crc_config_t * | config | ) |
Loads default values to CRC protocol configuration structure. The default values are:
config | CRC protocol configuration structure |
void CRC_GetConfig | ( | CRC_Type * | base, |
crc_config_t * | config | ||
) |
The values, including seed, can be used to resume CRC calculation later.
base | CRC peripheral address. |
config | CRC protocol configuration structure |
void CRC_WriteData | ( | CRC_Type * | base, |
const uint8_t * | data, | ||
size_t | dataSize | ||
) |
Writes input data buffer bytes to CRC data register.
base | CRC peripheral address. |
data | Input data stream, MSByte in data[0]. |
dataSize | Size of the input data buffer in bytes. |
|
inlinestatic |
Reads CRC data register.
base | CRC peripheral address. |
|
inlinestatic |
Reads CRC data register.
base | CRC peripheral address. |