![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | i2c_slave_address_t |
Data structure with 7-bit Slave address and Slave address disable. More... | |
struct | i2c_slave_config_t |
Structure with settings to initialize the I2C slave module. More... | |
struct | i2c_slave_transfer_t |
I2C slave transfer structure. More... | |
struct | i2c_slave_handle_t |
I2C slave handle structure. More... | |
Typedefs | |
typedef void(* | i2c_slave_transfer_callback_t )(I2C_Type *base, volatile i2c_slave_transfer_t *transfer, void *userData) |
Slave event callback function pointer type. More... | |
Slave initialization and deinitialization | |
void | I2C_SlaveGetDefaultConfig (i2c_slave_config_t *slaveConfig) |
Provides a default configuration for the I2C slave peripheral. More... | |
status_t | I2C_SlaveInit (I2C_Type *base, const i2c_slave_config_t *slaveConfig, uint32_t srcClock_Hz) |
Initializes the I2C slave peripheral. More... | |
void | I2C_SlaveSetAddress (I2C_Type *base, i2c_slave_address_register_t addressRegister, uint8_t address, bool addressDisable) |
Configures Slave Address n register. More... | |
void | I2C_SlaveDeinit (I2C_Type *base) |
Deinitializes the I2C slave peripheral. More... | |
static void | I2C_SlaveEnable (I2C_Type *base, bool enable) |
Enables or disables the I2C module as slave. More... | |
Slave status | |
static void | I2C_SlaveClearStatusFlags (I2C_Type *base, uint32_t statusMask) |
Clears the I2C status flag state. More... | |
Slave bus operations | |
status_t | I2C_SlaveWriteBlocking (I2C_Type *base, const uint8_t *txBuff, size_t txSize) |
Performs a polling send transfer on the I2C bus. More... | |
status_t | I2C_SlaveReadBlocking (I2C_Type *base, uint8_t *rxBuff, size_t rxSize) |
Performs a polling receive transfer on the I2C bus. More... | |
Slave non-blocking | |
void | I2C_SlaveTransferCreateHandle (I2C_Type *base, i2c_slave_handle_t *handle, i2c_slave_transfer_callback_t callback, void *userData) |
Creates a new handle for the I2C slave non-blocking APIs. More... | |
status_t | I2C_SlaveTransferNonBlocking (I2C_Type *base, i2c_slave_handle_t *handle, uint32_t eventMask) |
Starts accepting slave transfers. More... | |
status_t | I2C_SlaveSetSendBuffer (I2C_Type *base, volatile i2c_slave_transfer_t *transfer, const void *txData, size_t txSize, uint32_t eventMask) |
Starts accepting master read from slave requests. More... | |
status_t | I2C_SlaveSetReceiveBuffer (I2C_Type *base, volatile i2c_slave_transfer_t *transfer, void *rxData, size_t rxSize, uint32_t eventMask) |
Starts accepting master write to slave requests. More... | |
static uint32_t | I2C_SlaveGetReceivedAddress (I2C_Type *base, volatile i2c_slave_transfer_t *transfer) |
Returns the slave address sent by the I2C master. More... | |
void | I2C_SlaveTransferAbort (I2C_Type *base, i2c_slave_handle_t *handle) |
Aborts the slave non-blocking transfers. More... | |
status_t | I2C_SlaveTransferGetCount (I2C_Type *base, i2c_slave_handle_t *handle, size_t *count) |
Gets the slave transfer remaining bytes during a interrupt non-blocking transfer. More... | |
Slave IRQ handler | |
void | I2C_SlaveTransferHandleIRQ (I2C_Type *base, i2c_slave_handle_t *handle) |
Reusable routine to handle slave interrupts. More... | |
struct i2c_slave_address_t |
Data Fields | |
uint8_t | address |
7-bit Slave address SLVADR. More... | |
bool | addressDisable |
Slave address disable SADISABLE. More... | |
uint8_t i2c_slave_address_t::address |
bool i2c_slave_address_t::addressDisable |
struct i2c_slave_config_t |
This structure holds configuration settings for the I2C slave peripheral. To initialize this structure to reasonable defaults, call the I2C_SlaveGetDefaultConfig() function and pass a pointer to your configuration structure instance.
The configuration structure can be made constant so it resides in flash.
Data Fields | |
i2c_slave_address_t | address0 |
Slave's 7-bit address and disable. More... | |
i2c_slave_address_t | address1 |
Alternate slave 7-bit address and disable. More... | |
i2c_slave_address_t | address2 |
Alternate slave 7-bit address and disable. More... | |
i2c_slave_address_t | address3 |
Alternate slave 7-bit address and disable. More... | |
i2c_slave_address_qual_mode_t | qualMode |
Qualify mode for slave address 0. More... | |
uint8_t | qualAddress |
Slave address qualifier for address 0. More... | |
i2c_slave_bus_speed_t | busSpeed |
Slave bus speed mode. More... | |
bool | enableSlave |
Enable slave mode. More... | |
i2c_slave_address_t i2c_slave_config_t::address0 |
i2c_slave_address_t i2c_slave_config_t::address1 |
i2c_slave_address_t i2c_slave_config_t::address2 |
i2c_slave_address_t i2c_slave_config_t::address3 |
i2c_slave_address_qual_mode_t i2c_slave_config_t::qualMode |
uint8_t i2c_slave_config_t::qualAddress |
i2c_slave_bus_speed_t i2c_slave_config_t::busSpeed |
If the slave function stretches SCL to allow for software response, it must provide sufficient data setup time to the master before releasing the stretched clock. This is accomplished by inserting one clock time of CLKDIV at that point. The busSpeed value is used to configure CLKDIV such that one clock time is greater than the tSU;DAT value noted in the I2C bus specification for the I2C mode that is being used. If the busSpeed mode is unknown at compile time, use the longest data setup time kI2C_SlaveStandardMode (250 ns)
bool i2c_slave_config_t::enableSlave |
struct i2c_slave_transfer_t |
Data Fields | |
i2c_slave_handle_t * | handle |
Pointer to handle that contains this transfer. More... | |
i2c_slave_transfer_event_t | event |
Reason the callback is being invoked. More... | |
uint8_t | receivedAddress |
Matching address send by master. More... | |
uint32_t | eventMask |
Mask of enabled events. More... | |
uint8_t * | rxData |
Transfer buffer for receive data. | |
const uint8_t * | txData |
Transfer buffer for transmit data. | |
size_t | txSize |
Transfer size. | |
size_t | rxSize |
Transfer size. | |
size_t | transferredCount |
Number of bytes transferred during this transfer. More... | |
status_t | completionStatus |
Success or error code describing how the transfer completed. More... | |
i2c_slave_handle_t* i2c_slave_transfer_t::handle |
i2c_slave_transfer_event_t i2c_slave_transfer_t::event |
uint8_t i2c_slave_transfer_t::receivedAddress |
7-bits plus R/nW bit0
uint32_t i2c_slave_transfer_t::eventMask |
size_t i2c_slave_transfer_t::transferredCount |
status_t i2c_slave_transfer_t::completionStatus |
Only applies for kI2C_SlaveCompletionEvent.
struct _i2c_slave_handle |
I2C slave handle typedef.
Data Fields | |
volatile i2c_slave_transfer_t | transfer |
I2C slave transfer. More... | |
volatile bool | isBusy |
Whether transfer is busy. More... | |
volatile i2c_slave_fsm_t | slaveFsm |
slave transfer state machine. More... | |
i2c_slave_transfer_callback_t | callback |
Callback function called at transfer event. More... | |
void * | userData |
Callback parameter passed to callback. More... | |
volatile i2c_slave_transfer_t i2c_slave_handle_t::transfer |
volatile bool i2c_slave_handle_t::isBusy |
volatile i2c_slave_fsm_t i2c_slave_handle_t::slaveFsm |
i2c_slave_transfer_callback_t i2c_slave_handle_t::callback |
void* i2c_slave_handle_t::userData |
typedef void(* i2c_slave_transfer_callback_t)(I2C_Type *base, volatile i2c_slave_transfer_t *transfer, void *userData) |
This callback is used only for the slave non-blocking transfer API. To install a callback, use the I2C_SlaveSetCallback() function after you have created a handle.
base | Base address for the I2C instance on which the event occurred. |
transfer | Pointer to transfer descriptor containing values passed to and/or from the callback. |
userData | Arbitrary pointer-sized value passed from the application. |
enum _i2c_slave_flags |
These event enumerations are used for two related purposes. First, a bit mask created by OR'ing together events is passed to I2C_SlaveTransferNonBlocking() in order to specify which events to enable. Then, when the slave callback is invoked, it is passed the current event through its transfer parameter.
void I2C_SlaveGetDefaultConfig | ( | i2c_slave_config_t * | slaveConfig | ) |
This function provides the following default configuration for the I2C slave peripheral:
After calling this function, override any settings to customize the configuration, prior to initializing the master driver with I2C_SlaveInit(). Be sure to override at least the address0.address member of the configuration structure with the desired slave address.
[out] | slaveConfig | User provided configuration structure that is set to default values. Refer to i2c_slave_config_t. |
status_t I2C_SlaveInit | ( | I2C_Type * | base, |
const i2c_slave_config_t * | slaveConfig, | ||
uint32_t | srcClock_Hz | ||
) |
This function enables the peripheral clock and initializes the I2C slave peripheral as described by the user provided configuration.
base | The I2C peripheral base address. |
slaveConfig | User provided peripheral configuration. Use I2C_SlaveGetDefaultConfig() to get a set of defaults that you can override. |
srcClock_Hz | Frequency in Hertz of the I2C functional clock. Used to calculate CLKDIV value to provide enough data setup time for master when slave stretches the clock. |
void I2C_SlaveSetAddress | ( | I2C_Type * | base, |
i2c_slave_address_register_t | addressRegister, | ||
uint8_t | address, | ||
bool | addressDisable | ||
) |
This function writes new value to Slave Address register.
base | The I2C peripheral base address. |
addressRegister | The module supports multiple address registers. The parameter determines which one shall be changed. |
address | The slave address to be stored to the address register for matching. |
addressDisable | Disable matching of the specified address register. |
void I2C_SlaveDeinit | ( | I2C_Type * | base | ) |
This function disables the I2C slave peripheral and gates the clock. It also performs a software reset to restore the peripheral to reset conditions.
base | The I2C peripheral base address. |
|
inlinestatic |
base | The I2C peripheral base address. |
enable | True to enable or flase to disable. |
|
inlinestatic |
The following status register flags can be cleared:
Attempts to clear other flags has no effect.
base | The I2C peripheral base address. |
statusMask | A bitmask of status flags that are to be cleared. The mask is composed of _i2c_slave_flags enumerators OR'd together. You may pass the result of a previous call to I2C_SlaveGetStatusFlags(). |
status_t I2C_SlaveWriteBlocking | ( | I2C_Type * | base, |
const uint8_t * | txBuff, | ||
size_t | txSize | ||
) |
The function executes blocking address phase and blocking data phase.
base | The I2C peripheral base address. |
txBuff | The pointer to the data to be transferred. |
txSize | The length in bytes of the data to be transferred. |
status_t I2C_SlaveReadBlocking | ( | I2C_Type * | base, |
uint8_t * | rxBuff, | ||
size_t | rxSize | ||
) |
The function executes blocking address phase and blocking data phase.
base | The I2C peripheral base address. |
rxBuff | The pointer to the data to be transferred. |
rxSize | The length in bytes of the data to be transferred. |
void I2C_SlaveTransferCreateHandle | ( | I2C_Type * | base, |
i2c_slave_handle_t * | handle, | ||
i2c_slave_transfer_callback_t | callback, | ||
void * | userData | ||
) |
The creation of a handle is for use with the non-blocking APIs. Once a handle is created, there is not a corresponding destroy handle. If the user wants to terminate a transfer, the I2C_SlaveTransferAbort() API shall be called.
base | The I2C peripheral base address. | |
[out] | handle | Pointer to the I2C slave driver handle. |
callback | User provided pointer to the asynchronous callback function. | |
userData | User provided pointer to the application callback data. |
status_t I2C_SlaveTransferNonBlocking | ( | I2C_Type * | base, |
i2c_slave_handle_t * | handle, | ||
uint32_t | eventMask | ||
) |
Call this API after calling I2C_SlaveInit() and I2C_SlaveTransferCreateHandle() to start processing transactions driven by an I2C master. The slave monitors the I2C bus and pass events to the callback that was passed into the call to I2C_SlaveTransferCreateHandle(). The callback is always invoked from the interrupt context.
If no slave Tx transfer is busy, a master read from slave request invokes kI2C_SlaveTransmitEvent callback. If no slave Rx transfer is busy, a master write to slave request invokes kI2C_SlaveReceiveEvent callback.
The set of events received by the callback is customizable. To do so, set the eventMask parameter to the OR'd combination of i2c_slave_transfer_event_t enumerators for the events you wish to receive. The kI2C_SlaveTransmitEvent and kI2C_SlaveReceiveEvent events are always enabled and do not need to be included in the mask. Alternatively, you can pass 0 to get a default set of only the transmit and receive events that are always enabled. In addition, the kI2C_SlaveAllEvents constant is provided as a convenient way to enable all events.
base | The I2C peripheral base address. |
handle | Pointer to i2c_slave_handle_t structure which stores the transfer state. |
eventMask | Bit mask formed by OR'ing together i2c_slave_transfer_event_t enumerators to specify which events to send to the callback. Other accepted values are 0 to get a default set of only the transmit and receive events, and kI2C_SlaveAllEvents to enable all events. |
kStatus_Success | Slave transfers were successfully started. |
kStatus_I2C_Busy | Slave transfers have already been started on this handle. |
status_t I2C_SlaveSetSendBuffer | ( | I2C_Type * | base, |
volatile i2c_slave_transfer_t * | transfer, | ||
const void * | txData, | ||
size_t | txSize, | ||
uint32_t | eventMask | ||
) |
The function can be called in response to kI2C_SlaveTransmitEvent callback to start a new slave Tx transfer from within the transfer callback.
The set of events received by the callback is customizable. To do so, set the eventMask parameter to the OR'd combination of i2c_slave_transfer_event_t enumerators for the events you wish to receive. The kI2C_SlaveTransmitEvent and kI2C_SlaveReceiveEvent events are always enabled and do not need to be included in the mask. Alternatively, you can pass 0 to get a default set of only the transmit and receive events that are always enabled. In addition, the kI2C_SlaveAllEvents constant is provided as a convenient way to enable all events.
base | The I2C peripheral base address. |
transfer | Pointer to i2c_slave_transfer_t structure. |
txData | Pointer to data to send to master. |
txSize | Size of txData in bytes. |
eventMask | Bit mask formed by OR'ing together i2c_slave_transfer_event_t enumerators to specify which events to send to the callback. Other accepted values are 0 to get a default set of only the transmit and receive events, and kI2C_SlaveAllEvents to enable all events. |
kStatus_Success | Slave transfers were successfully started. |
kStatus_I2C_Busy | Slave transfers have already been started on this handle. |
status_t I2C_SlaveSetReceiveBuffer | ( | I2C_Type * | base, |
volatile i2c_slave_transfer_t * | transfer, | ||
void * | rxData, | ||
size_t | rxSize, | ||
uint32_t | eventMask | ||
) |
The function can be called in response to kI2C_SlaveReceiveEvent callback to start a new slave Rx transfer from within the transfer callback.
The set of events received by the callback is customizable. To do so, set the eventMask parameter to the OR'd combination of i2c_slave_transfer_event_t enumerators for the events you wish to receive. The kI2C_SlaveTransmitEvent and kI2C_SlaveReceiveEvent events are always enabled and do not need to be included in the mask. Alternatively, you can pass 0 to get a default set of only the transmit and receive events that are always enabled. In addition, the kI2C_SlaveAllEvents constant is provided as a convenient way to enable all events.
base | The I2C peripheral base address. |
transfer | Pointer to i2c_slave_transfer_t structure. |
rxData | Pointer to data to store data from master. |
rxSize | Size of rxData in bytes. |
eventMask | Bit mask formed by OR'ing together i2c_slave_transfer_event_t enumerators to specify which events to send to the callback. Other accepted values are 0 to get a default set of only the transmit and receive events, and kI2C_SlaveAllEvents to enable all events. |
kStatus_Success | Slave transfers were successfully started. |
kStatus_I2C_Busy | Slave transfers have already been started on this handle. |
|
inlinestatic |
This function should only be called from the address match event callback kI2C_SlaveAddressMatchEvent.
base | The I2C peripheral base address. |
transfer | The I2C slave transfer. |
void I2C_SlaveTransferAbort | ( | I2C_Type * | base, |
i2c_slave_handle_t * | handle | ||
) |
base | The I2C peripheral base address. |
handle | Pointer to i2c_slave_handle_t structure which stores the transfer state. |
kStatus_Success | |
kStatus_I2C_Idle |
status_t I2C_SlaveTransferGetCount | ( | I2C_Type * | base, |
i2c_slave_handle_t * | handle, | ||
size_t * | count | ||
) |
base | I2C base pointer. |
handle | pointer to i2c_slave_handle_t structure. |
count | Number of bytes transferred so far by the non-blocking transaction. |
kStatus_InvalidArgument | count is Invalid. |
kStatus_Success | Successfully return the count. |
void I2C_SlaveTransferHandleIRQ | ( | I2C_Type * | base, |
i2c_slave_handle_t * | handle | ||
) |
base | The I2C peripheral base address. |
handle | Pointer to i2c_slave_handle_t structure which stores the transfer state. |