![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the Random Number Generator module of MCUXpresso SDK devices.
The Random Number Generator is a hardware module that generates 32-bit random numbers. Internally it is accessed by calling ROM API. A typical consumer is a pseudo random number generator (PRNG) which can be implemented to achieve both true randomness and cryptographic strength random numbers using the RNG output as its entropy seed. The data generated by a RNG is intended for direct use by functions that generate secret keys, per-message secrets, random challenges, and other similar quantities used in cryptographic algorithms.
This example code shows how to get 128-bit random data from the RNG driver.
Functions | |
| static uint32_t | RNG_GetRandomData (void) |
| Gets random data. More... | |
Driver version | |
| #define | FSL_RNG_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| RNG driver version 2.0.0. More... | |
| #define FSL_RNG_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
Current version: 2.0.0
Change log:
|
inlinestatic |
This function returns single 32 bit random number.