MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
LPC_ACOMP: Analog comparator Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Analog comparator (LPC_ACOMP) module of MCUXpresso SDK devices.

Typical use case

Polling Configuration

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/acomp/acomp_basic

Interrupt Configuration

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/acomp/acomp_interrupt

Files

file  fsl_acomp.h
 

Data Structures

struct  acomp_config_t
 The structure for ACOMP basic configuration. More...
 
struct  acomp_ladder_config_t
 The structure for ACOMP voltage ladder. More...
 

Enumerations

enum  acomp_ladder_reference_voltage_t {
  kACOMP_LadderRefVoltagePinVDD = 0U,
  kACOMP_LadderRefVoltagePinVDDCMP = 1U
}
 
enum  acomp_interrupt_enable_t {
  kACOMP_InterruptsFallingEdgeEnable = 0U,
  kACOMP_InterruptsRisingEdgeEnable = 1U,
  kACOMP_InterruptsBothEdgesEnable = 2U,
  kACOMP_InterruptsDisable = 3U
}
 The ACOMP interrupts enable. More...
 
enum  acomp_hysteresis_selection_t {
  kACOMP_HysteresisNoneSelection = 0U,
  kACOMP_Hysteresis5MVSelection = 1U,
  kACOMP_Hysteresis10MVSelection = 2U,
  kACOMP_Hysteresis15MVSelection = 3U
}
 The ACOMP hysteresis selection. More...
 

Variables

bool acomp_config_t::enableSyncToBusClk
 If true, Comparator output is synchronized to the bus clock for output to other modules. More...
 
acomp_hysteresis_selection_t acomp_config_t::hysteresisSelection
 Controls the hysteresis of the comparator. More...
 
uint8_t acomp_ladder_config_t::ladderValue
 Voltage ladder value. More...
 
acomp_ladder_reference_voltage_t acomp_ladder_config_t::referenceVoltage
 Selects the reference voltage(Vref) for the voltage ladder. More...
 

Driver version

#define FSL_ACOMP_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 ACOMP driver version 2.0.2. More...
 

Initialization

void ACOMP_Init (ACOMP_Type *base, const acomp_config_t *config)
 Initialize the ACOMP module. More...
 
void ACOMP_Deinit (ACOMP_Type *base)
 De-initialize the ACOMP module. More...
 
void ACOMP_GetDefaultConfig (acomp_config_t *config)
 Gets an available pre-defined settings for the ACOMP's configuration. More...
 
void ACOMP_EnableInterrupts (ACOMP_Type *base, acomp_interrupt_enable_t enable)
 Enable ACOMP interrupts. More...
 
static bool ACOMP_GetInterruptsStatusFlags (ACOMP_Type *base)
 Get interrupts status flags. More...
 
static void ACOMP_ClearInterruptsStatusFlags (ACOMP_Type *base)
 Clear the ACOMP interrupts status flags. More...
 
static bool ACOMP_GetOutputStatusFlags (ACOMP_Type *base)
 Get ACOMP output status flags. More...
 
static void ACOMP_SetInputChannel (ACOMP_Type *base, uint32_t postiveInputChannel, uint32_t negativeInputChannel)
 Set the ACOMP postive and negative input channel. More...
 
void ACOMP_SetLadderConfig (ACOMP_Type *base, const acomp_ladder_config_t *config)
 Set the voltage ladder configuration. More...
 

Data Structure Documentation

struct acomp_config_t

Data Fields

bool enableSyncToBusClk
 If true, Comparator output is synchronized to the bus clock for output to other modules. More...
 
acomp_hysteresis_selection_t hysteresisSelection
 Controls the hysteresis of the comparator. More...
 
struct acomp_ladder_config_t

Data Fields

uint8_t ladderValue
 Voltage ladder value. More...
 
acomp_ladder_reference_voltage_t referenceVoltage
 Selects the reference voltage(Vref) for the voltage ladder. More...
 

Macro Definition Documentation

#define FSL_ACOMP_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))

Enumeration Type Documentation

Enumerator
kACOMP_LadderRefVoltagePinVDD 

Supply from pin VDD.

kACOMP_LadderRefVoltagePinVDDCMP 

Supply from pin VDDCMP.

Enumerator
kACOMP_InterruptsFallingEdgeEnable 

Enable the falling edge interrupts.

kACOMP_InterruptsRisingEdgeEnable 

Enable the rising edge interrupts.

kACOMP_InterruptsBothEdgesEnable 

Enable the both edges interrupts.

kACOMP_InterruptsDisable 

Disable the interrupts.

Enumerator
kACOMP_HysteresisNoneSelection 

None (the output will switch as the voltages cross).

kACOMP_Hysteresis5MVSelection 

5Mv.

kACOMP_Hysteresis10MVSelection 

10Mv.

kACOMP_Hysteresis15MVSelection 

15Mv.

Function Documentation

void ACOMP_Init ( ACOMP_Type *  base,
const acomp_config_t *  config 
)
Parameters
baseACOMP peripheral base address.
configPointer to "acomp_config_t" structure.
void ACOMP_Deinit ( ACOMP_Type *  base)
Parameters
baseACOMP peripheral base address.
void ACOMP_GetDefaultConfig ( acomp_config_t *  config)

This function initializes the converter configuration structure with available settings. The default values are:

* config->enableSyncToBusClk = false;
* config->hysteresisSelection = kACOMP_hysteresisNoneSelection;
*

In default configuration, the ACOMP's output would be used directly and switch as the voltages cross.

Parameters
baseACOMP peripheral base address.
configPointer to the configuration structure.
void ACOMP_EnableInterrupts ( ACOMP_Type *  base,
acomp_interrupt_enable_t  enable 
)
Parameters
baseACOMP peripheral base address.
enableEnable/Disable interrupt feature.
static bool ACOMP_GetInterruptsStatusFlags ( ACOMP_Type *  base)
inlinestatic
Parameters
baseACOMP peripheral base address.
Returns
Reflect the state ACOMP edge-detect status, true or false.
static void ACOMP_ClearInterruptsStatusFlags ( ACOMP_Type *  base)
inlinestatic
Parameters
baseACOMP peripheral base address.
static bool ACOMP_GetOutputStatusFlags ( ACOMP_Type *  base)
inlinestatic
Parameters
baseACOMP peripheral base address.
Returns
Reflect the state of the comparator output, true or false.
static void ACOMP_SetInputChannel ( ACOMP_Type *  base,
uint32_t  postiveInputChannel,
uint32_t  negativeInputChannel 
)
inlinestatic
Parameters
baseACOMP peripheral base address.
postiveInputChannelThe index of postive input channel.
negativeInputChannelThe index of negative input channel.
void ACOMP_SetLadderConfig ( ACOMP_Type *  base,
const acomp_ladder_config_t *  config 
)
Parameters
baseACOMP peripheral base address.
configThe structure for voltage ladder. If the config is NULL, voltage ladder would be diasbled, otherwise the voltage ladder would be configured and enabled.

Variable Documentation

bool acomp_config_t::enableSyncToBusClk

If false, Comparator output is used directly.

acomp_hysteresis_selection_t acomp_config_t::hysteresisSelection
uint8_t acomp_ladder_config_t::ladderValue

00000 = Vss, 00001 = 1*Vref/31, ..., 11111 = Vref.

acomp_ladder_reference_voltage_t acomp_ladder_config_t::referenceVoltage