![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
This section describes the programming interface of the SPI DMA driver.
Files | |
| file | fsl_spi.h |
Data Structures | |
| struct | spi_fifo_config_t |
| SPI fifo user configure structure. More... | |
| struct | spi_delay_config_t |
| SPI delay time configure structure. More... | |
| struct | spi_master_config_t |
| SPI master user configure structure. More... | |
| struct | spi_slave_config_t |
| SPI slave user configure structure. More... | |
| struct | spi_transfer_t |
| SPI transfer structure. More... | |
| struct | spi_half_duplex_transfer_t |
| SPI half-duplex(master only) transfer structure. More... | |
| struct | spi_config_t |
| Internal configuration structure used in 'spi' and 'spi_dma' driver. More... | |
| struct | spi_master_handle_t |
| SPI transfer handle structure. More... | |
Macros | |
| #define | SPI_DUMMYDATA (0xFFU) |
| SPI dummy transfer data, the data is sent while txBuff is NULL. More... | |
Typedefs | |
| typedef spi_master_handle_t | spi_slave_handle_t |
| Slave handle type. | |
| typedef void(* | spi_master_callback_t )(SPI_Type *base, spi_master_handle_t *handle, status_t status, void *userData) |
| SPI master callback for finished transmit. | |
| typedef void(* | spi_slave_callback_t )(SPI_Type *base, spi_slave_handle_t *handle, status_t status, void *userData) |
| SPI slave callback for finished transmit. | |
Enumerations | |
| enum | spi_xfer_option_t { kSPI_FrameDelay = (SPI_TXDATCTL_EOF_MASK), kSPI_FrameAssert = (SPI_TXDATCTL_EOT_MASK), kSPI_ReceiveIgnore = (SPI_TXDATCTL_RXIGNORE_MASK) } |
| SPI transfer option. More... | |
| enum | spi_shift_direction_t { kSPI_MsbFirst = 0U, kSPI_LsbFirst = 1U } |
| SPI data shifter direction options. More... | |
| enum | spi_clock_polarity_t { kSPI_ClockPolarityActiveHigh = 0x0U, kSPI_ClockPolarityActiveLow = 0x1U } |
| SPI clock polarity configuration. More... | |
| enum | spi_clock_phase_t { kSPI_ClockPhaseFirstEdge = 0x0U, kSPI_ClockPhaseSecondEdge = 0x1U } |
| SPI clock phase configuration. More... | |
| enum | spi_fifo_direction_t { kSPI_FifoTx = 1U, kSPI_FifoRx = 2U } |
| SPI FIFO driection. More... | |
| enum | spi_data_width_t { kSPI_Data1Bits = 0, kSPI_Data2Bits = 1, kSPI_Data3Bits = 2, kSPI_Data4Bits = 3, kSPI_Data5Bits = 4, kSPI_Data6Bits = 5, kSPI_Data7Bits = 6, kSPI_Data8Bits = 7, kSPI_Data9Bits = 8, kSPI_Data10Bits = 9, kSPI_Data11Bits = 10, kSPI_Data12Bits = 11, kSPI_Data13Bits = 12, kSPI_Data14Bits = 13, kSPI_Data15Bits = 14, kSPI_Data16Bits = 15 } |
| Transfer data width. More... | |
| enum | spi_ssel_t { kSPI_Ssel0 = 0, kSPI_Ssel1 = 1, kSPI_Ssel2 = 2, kSPI_Ssel3 = 3 } |
| Slave select. More... | |
| enum | spi_spol_t |
| ssel polarity | |
| enum | _spi_status { kStatus_SPI_Busy = MAKE_STATUS(kStatusGroup_LPC_SPI, 0), kStatus_SPI_Idle = MAKE_STATUS(kStatusGroup_LPC_SPI, 1), kStatus_SPI_Error = MAKE_STATUS(kStatusGroup_LPC_SPI, 2), kStatus_SPI_BaudrateNotSupport } |
| SPI transfer status. More... | |
| enum | _spi_interrupt_enable { kSPI_RxReadyInterruptEnable = SPI_INTENSET_RXRDYEN_MASK, kSPI_TxReadyInterruptEnable = SPI_INTENSET_TXRDYEN_MASK, kSPI_RxOverrunInterruptEnable = SPI_INTENSET_RXOVEN_MASK, kSPI_TxUnderrunInterruptEnable = SPI_INTENSET_TXUREN_MASK, kSPI_SlaveSelectAssertInterruptEnable = SPI_INTENSET_SSAEN_MASK, kSPI_SlaveSelectDeassertInterruptEnable = SPI_INTENSET_SSDEN_MASK, kSPI_MasterIdleInterruptEnable = SPI_INTENSET_MSTIDLEEN_MASK } |
| SPI interrupt sources. More... | |
| enum | _spi_fifo_interrupt_enable { kSPI_RxFifoThresholdInterruptEnable, kSPI_TxFifoThresholdInterruptEnable, kSPI_RxFifoTimeoutInterruptEnable = VFIFO_SPI_CTLSETSPI_RXTIMEOUTINTEN_MASK } |
| SPI FIFO interrupt sources. More... | |
| enum | _spi_status_flags { kSPI_RxReadyFlag = SPI_STAT_RXRDY_MASK, kSPI_TxReadyFlag = SPI_STAT_TXRDY_MASK, kSPI_RxOverrunFlag = SPI_STAT_RXOV_MASK, kSPI_TxUnderrunFlag = SPI_STAT_TXUR_MASK, kSPI_SlaveSelectAssertFlag = SPI_STAT_SSA_MASK, kSPI_SlaveSelectDeassertFlag = SPI_STAT_SSD_MASK, kSPI_StallFlag = SPI_STAT_STALLED_MASK, kSPI_EndTransferFlag = SPI_STAT_ENDTRANSFER_MASK, kSPI_MasterIdleFlag = SPI_STAT_MSTIDLE_MASK } |
| SPI status flags. More... | |
| enum | _spi_fifo_status_flags { kSPI_RxFifoThresholdFlag = (VFIFO_SPI_STATSPI_RXTH_MASK), kSPI_TxFifoThresholdFlag = (VFIFO_SPI_STATSPI_TXTH_MASK), kSPI_RxFifoTimeOutFlag = (VFIFO_SPI_STATSPI_RXTIMEOUT_MASK), kSPI_FifoBusErrorFlag = (VFIFO_SPI_STATSPI_BUSERR_MASK), kSPI_RxFifoEmptyFlag = (VFIFO_SPI_STATSPI_RXEMPTY_MASK), kSPI_TxFifoEmptyFlag = (VFIFO_SPI_STATSPI_TXEMPTY_MASK) } |
| SPI FIFO status flags. More... | |
Functions | |
| uint32_t | SPI_GetInstance (SPI_Type *base) |
| Returns instance number for SPI peripheral base address. More... | |
Variables | |
| volatile uint8_t | s_dummyData [] |
| Global variable for dummy data value setting. More... | |
Driver version | |
| #define | FSL_SPI_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| SPI driver version 2.0.2. More... | |
Initialization and deinitialization | |
| void | SPI_MasterGetDefaultConfig (spi_master_config_t *config) |
| Sets the SPI master configuration structure to default values. More... | |
| status_t | SPI_MasterInit (SPI_Type *base, const spi_master_config_t *config, uint32_t srcClock_Hz) |
| Initializes the SPI with master configuration. More... | |
| void | SPI_SlaveGetDefaultConfig (spi_slave_config_t *config) |
| Sets the SPI slave configuration structure to default values. More... | |
| status_t | SPI_SlaveInit (SPI_Type *base, const spi_slave_config_t *config) |
| Initializes the SPI with slave configuration. More... | |
| void | SPI_Deinit (SPI_Type *base) |
| De-initializes the SPI. More... | |
| static void | SPI_Enable (SPI_Type *base, bool enable) |
| Enable or disable the SPI Master or Slave. More... | |
Status | |
| static uint32_t | SPI_GetStatusFlags (SPI_Type *base) |
| Gets the status flag. More... | |
| uint32_t | SPI_GetFifoStatusFlags (SPI_Type *base) |
| Gets the FIFO status flag for SPI transfer. More... | |
| void | SPI_ClearFifoStatusFlags (SPI_Type *base, uint32_t mask) |
| Clear the FIFO status flag for SPI transfer. More... | |
Interrupts | |
| static void | SPI_EnableInterrupts (SPI_Type *base, uint32_t irqs) |
| Enables the interrupt for the SPI. More... | |
| static void | SPI_DisableInterrupts (SPI_Type *base, uint32_t irqs) |
| Disables the interrupt for the SPI. More... | |
| void | SPI_EnableFifoInterrupts (SPI_Type *base, uint32_t irqs) |
| Enables the FIFO interrupt for the SPI. More... | |
| void | SPI_DisableFifoInterrupts (SPI_Type *base, uint32_t irqs) |
| Disables the FIFO interrupt for the SPI. More... | |
Bus Operations | |
| static bool | SPI_IsMaster (SPI_Type *base) |
| Returns whether the SPI module is in master mode. More... | |
| void * | SPI_GetConfig (SPI_Type *base) |
| Returns the configurations. More... | |
| status_t | SPI_MasterSetBaud (SPI_Type *base, uint32_t baudrate_Bps, uint32_t srcClock_Hz) |
| Sets the baud rate for SPI transfer. More... | |
| void | SPI_WriteData (SPI_Type *base, uint16_t data, uint32_t configFlags) |
| Writes a data into the SPI data register. More... | |
| uint32_t | SPI_ReadData (SPI_Type *base) |
| Gets a data from the SPI data register. More... | |
| void | SPI_SetTransferDelay (SPI_Type *base, const spi_delay_config_t *config) |
| Set delay time for transfer. More... | |
| void | SPI_SetDummyData (SPI_Type *base, uint8_t dummyData) |
| Set up the dummy data. More... | |
FIFO Operations | |
| void | SPI_EnableFifo (SPI_Type *base, const spi_fifo_config_t *config) |
| Enable FIFO for SPI. More... | |
| void | SPI_DisableFifo (SPI_Type *base) |
| Disable FIFO for SPI. More... | |
| bool | SPI_IsTxFifoEnabled (SPI_Type *base) |
| Is TX FIFO enabled. More... | |
| bool | SPI_IsRxFifoEnabled (SPI_Type *base) |
| Is RX FIFO enabled. More... | |
| void | SPI_FifoFlush (SPI_Type *base, uint32_t direction) |
| Flush the FIFO buffer. More... | |
Transactional | |
| status_t | SPI_MasterTransferCreateHandle (SPI_Type *base, spi_master_handle_t *handle, spi_master_callback_t callback, void *userData) |
| Initializes the SPI master handle. More... | |
| status_t | SPI_MasterTransferBlocking (SPI_Type *base, spi_transfer_t *xfer) |
| Transfers a block of data using a polling method. More... | |
| status_t | SPI_MasterTransferNonBlocking (SPI_Type *base, spi_master_handle_t *handle, spi_transfer_t *xfer) |
| Performs a non-blocking SPI interrupt transfer. More... | |
| status_t | SPI_MasterHalfDuplexTransferBlocking (SPI_Type *base, spi_half_duplex_transfer_t *xfer) |
| Transfers a block of data using a polling method. More... | |
| status_t | SPI_MasterHalfDuplexTransferNonBlocking (SPI_Type *base, spi_master_handle_t *handle, spi_half_duplex_transfer_t *xfer) |
| Performs a non-blocking SPI interrupt transfer. More... | |
| status_t | SPI_MasterTransferGetCount (SPI_Type *base, spi_master_handle_t *handle, size_t *count) |
| Gets the master transfer count. More... | |
| void | SPI_MasterTransferAbort (SPI_Type *base, spi_master_handle_t *handle) |
| SPI master aborts a transfer using an interrupt. More... | |
| void | SPI_MasterTransferHandleIRQ (SPI_Type *base, spi_master_handle_t *handle) |
| Interrupts the handler for the SPI. More... | |
| status_t | SPI_SlaveTransferCreateHandle (SPI_Type *base, spi_slave_handle_t *handle, spi_slave_callback_t callback, void *userData) |
| Initializes the SPI slave handle. More... | |
| status_t | SPI_SlaveTransferNonBlocking (SPI_Type *base, spi_slave_handle_t *handle, spi_transfer_t *xfer) |
| Performs a non-blocking SPI slave interrupt transfer. More... | |
| static status_t | SPI_SlaveTransferGetCount (SPI_Type *base, spi_slave_handle_t *handle, size_t *count) |
| Gets the slave transfer count. More... | |
| static void | SPI_SlaveTransferAbort (SPI_Type *base, spi_slave_handle_t *handle) |
| SPI slave aborts a transfer using an interrupt. More... | |
| void | SPI_SlaveTransferHandleIRQ (SPI_Type *base, spi_slave_handle_t *handle) |
| Interrupts a handler for the SPI slave. More... | |
| struct spi_fifo_config_t |
Data Fields | |
| bool | enableTxFifo |
| Enable transmit FIFO. | |
| bool | enableRxFifo |
| Enable receive FIFO. | |
| uint8_t | txFifoSize |
| Configure txFIFO size. | |
| uint8_t | rxFifoSize |
| Configure rxFIFO size. | |
| uint8_t | txFifoThreshold |
| txFIFO threshold | |
| uint8_t | rxFifoThreshold |
| rxFIFO threshold | |
| struct spi_delay_config_t |
Data Fields | |
| uint8_t | preDelay |
| Delay between SSEL assertion and the beginning of transfer. More... | |
| uint8_t | postDelay |
| Delay between the end of transfer and SSEL deassertion. More... | |
| uint8_t | frameDelay |
| Delay between frame to frame. More... | |
| uint8_t | transferDelay |
| Delay between transfer to transfer. More... | |
| uint8_t spi_delay_config_t::preDelay |
| uint8_t spi_delay_config_t::postDelay |
| uint8_t spi_delay_config_t::frameDelay |
| uint8_t spi_delay_config_t::transferDelay |
| struct spi_master_config_t |
Data Fields | |
| bool | enableLoopback |
| Enable loopback for test purpose. | |
| bool | enableMaster |
| Enable SPI at initialization time. | |
| spi_clock_polarity_t | polarity |
| Clock polarity. | |
| spi_clock_phase_t | phase |
| Clock phase. | |
| spi_shift_direction_t | direction |
| MSB or LSB. | |
| uint32_t | baudRate_Bps |
| Baud Rate for SPI in Hz. | |
| spi_data_width_t | dataWidth |
| Width of the data. | |
| spi_ssel_t | sselNum |
| Slave select number. | |
| spi_spol_t | sselPol |
| Configure active CS polarity. | |
| spi_fifo_config_t | fifoConfig |
| Configure for fifo. More... | |
| spi_delay_config_t | delayConfig |
| Configure for delay time. More... | |
| spi_fifo_config_t spi_master_config_t::fifoConfig |
| spi_delay_config_t spi_master_config_t::delayConfig |
| struct spi_slave_config_t |
Data Fields | |
| bool | enableSlave |
| Enable SPI at initialization time. | |
| spi_clock_polarity_t | polarity |
| Clock polarity. | |
| spi_clock_phase_t | phase |
| Clock phase. | |
| spi_shift_direction_t | direction |
| MSB or LSB. | |
| spi_data_width_t | dataWidth |
| Width of the data. | |
| spi_spol_t | sselPol |
| Configure active CS polarity. | |
| spi_fifo_config_t | fifoConfig |
| Configure for fifo. More... | |
| spi_fifo_config_t spi_slave_config_t::fifoConfig |
| struct spi_transfer_t |
Data Fields | |
| uint8_t * | txData |
| Send buffer. | |
| uint8_t * | rxData |
| Receive buffer. | |
| uint32_t | configFlags |
| Additional option to control transfer, spi_xfer_option_t. More... | |
| size_t | dataSize |
| Transfer bytes. | |
| uint32_t spi_transfer_t::configFlags |
| struct spi_half_duplex_transfer_t |
Data Fields | |
| uint8_t * | txData |
| Send buffer. | |
| uint8_t * | rxData |
| Receive buffer. | |
| size_t | txDataSize |
| Transfer bytes for transmit. | |
| size_t | rxDataSize |
| Transfer bytes. | |
| uint32_t | configFlags |
| Transfer configuration flags, spi_xfer_option_t. More... | |
| bool | isPcsAssertInTransfer |
| If PCS pin keep assert between transmit and receive. More... | |
| bool | isTransmitFirst |
| True for transmit first and false for receive first. More... | |
| uint32_t spi_half_duplex_transfer_t::configFlags |
| bool spi_half_duplex_transfer_t::isPcsAssertInTransfer |
true for assert and false for deassert.
| bool spi_half_duplex_transfer_t::isTransmitFirst |
| struct spi_config_t |
| struct _spi_master_handle |
Master handle type.
Data Fields | |
| uint8_t *volatile | txData |
| Transfer buffer. | |
| uint8_t *volatile | rxData |
| Receive buffer. | |
| volatile size_t | txRemainingBytes |
| Number of data to be transmitted [in bytes]. | |
| volatile size_t | rxRemainingBytes |
| Number of data to be received [in bytes]. | |
| size_t | totalByteCount |
| A number of transfer bytes. | |
| volatile uint32_t | state |
| SPI internal state. | |
| spi_master_callback_t | callback |
| SPI callback. | |
| void * | userData |
| Callback parameter. | |
| uint8_t | dataWidth |
| Width of the data [Valid values: 1 to 16]. | |
| uint8_t | sselNum |
| Slave select number to be asserted when transferring data [Valid values: 0 to 3]. | |
| bool | isTxFifoEnabled |
| Is transmit FIFO enabled. More... | |
| bool | isRxFifoEnabled |
| Is receive FIFO enabled. More... | |
| uint8_t | txFifoThreshold |
| txFIFO threshold | |
| uint8_t | rxFifoThreshold |
| rxFIFO threshold | |
| uint8_t | rxFIFOSize |
| rxFIFO size used for protecting received data. More... | |
| uint32_t | commonCommand |
| Command for common transfer bytes. More... | |
| uint32_t | lastCommand |
| Command for last transfer byte. More... | |
| bool spi_master_handle_t::isTxFifoEnabled |
| bool spi_master_handle_t::isRxFifoEnabled |
| uint8_t spi_master_handle_t::rxFIFOSize |
| uint32_t spi_master_handle_t::commonCommand |
| uint32_t spi_master_handle_t::lastCommand |
| #define FSL_SPI_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| #define SPI_DUMMYDATA (0xFFU) |
| enum spi_xfer_option_t |
| enum spi_clock_polarity_t |
| enum spi_clock_phase_t |
| enum spi_fifo_direction_t |
| enum spi_data_width_t |
| enum spi_ssel_t |
| enum _spi_status |
| enum _spi_status_flags |
| uint32_t SPI_GetInstance | ( | SPI_Type * | base | ) |
| void SPI_MasterGetDefaultConfig | ( | spi_master_config_t * | config | ) |
The purpose of this API is to get the configuration structure initialized for use in SPI_MasterInit(). User may use the initialized structure unchanged in SPI_MasterInit(), or modify some fields of the structure before calling SPI_MasterInit(). After calling this API, the master is ready to transfer. Example:
| config | pointer to master config structure |
| status_t SPI_MasterInit | ( | SPI_Type * | base, |
| const spi_master_config_t * | config, | ||
| uint32_t | srcClock_Hz | ||
| ) |
The configuration structure can be filled by user from scratch, or be set with default values by SPI_MasterGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example
| base | SPI base pointer |
| config | pointer to master configuration structure |
| srcClock_Hz | Source clock frequency. |
| void SPI_SlaveGetDefaultConfig | ( | spi_slave_config_t * | config | ) |
The purpose of this API is to get the configuration structure initialized for use in SPI_SlaveInit(). Modify some fields of the structure before calling SPI_SlaveInit(). Example:
| config | pointer to slave configuration structure |
| status_t SPI_SlaveInit | ( | SPI_Type * | base, |
| const spi_slave_config_t * | config | ||
| ) |
The configuration structure can be filled by user from scratch or be set with default values by SPI_SlaveGetDefaultConfig(). After calling this API, the slave is ready to transfer. Example
| base | SPI base pointer |
| config | pointer to slave configuration structure |
| void SPI_Deinit | ( | SPI_Type * | base | ) |
Calling this API resets the SPI module, gates the SPI clock. Disable the fifo if enabled. The SPI module can't work unless calling the SPI_MasterInit/SPI_SlaveInit to initialize module.
| base | SPI base pointer |
|
inlinestatic |
| base | SPI base pointer |
| enable | or disable ( true = enable, false = disable) |
|
inlinestatic |
| base | SPI base pointer |
| uint32_t SPI_GetFifoStatusFlags | ( | SPI_Type * | base | ) |
| base | SPI base pointer |
| void SPI_ClearFifoStatusFlags | ( | SPI_Type * | base, |
| uint32_t | mask | ||
| ) |
Only kSPI_RxFifoTimeOutFlag and kSPI_FifoBusErrorFlag can be cleared.
| base | SPI base pointer |
| mask | use status flag to AND _spi_status_flags could get the related status. |
|
inlinestatic |
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
|
|
inlinestatic |
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
|
| void SPI_EnableFifoInterrupts | ( | SPI_Type * | base, |
| uint32_t | irqs | ||
| ) |
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
|
| void SPI_DisableFifoInterrupts | ( | SPI_Type * | base, |
| uint32_t | irqs | ||
| ) |
| base | SPI base pointer |
| irqs | SPI interrupt source. The parameter can be any combination of the following values:
|
|
inlinestatic |
| base | SPI peripheral address. |
| void* SPI_GetConfig | ( | SPI_Type * | base | ) |
| base | SPI peripheral address. |
| status_t SPI_MasterSetBaud | ( | SPI_Type * | base, |
| uint32_t | baudrate_Bps, | ||
| uint32_t | srcClock_Hz | ||
| ) |
This is only used in master.
| base | SPI base pointer |
| baudrate_Bps | baud rate needed in Hz. |
| srcClock_Hz | SPI source clock frequency in Hz. |
| void SPI_WriteData | ( | SPI_Type * | base, |
| uint16_t | data, | ||
| uint32_t | configFlags | ||
| ) |
| base | SPI base pointer |
| data | needs to be write. |
| configFlags | transfer configuration options spi_xfer_option_t |
| uint32_t SPI_ReadData | ( | SPI_Type * | base | ) |
| base | SPI base pointer |
| void SPI_SetTransferDelay | ( | SPI_Type * | base, |
| const spi_delay_config_t * | config | ||
| ) |
the delay uint is SPI clock time, maximum value is 0xF.
| base | SPI base pointer |
| config | configuration for delay option spi_delay_config_t. |
| void SPI_SetDummyData | ( | SPI_Type * | base, |
| uint8_t | dummyData | ||
| ) |
| base | SPI peripheral address. |
| dummyData | Data to be transferred when tx buffer is NULL. |
| void SPI_EnableFifo | ( | SPI_Type * | base, |
| const spi_fifo_config_t * | config | ||
| ) |
This function will enable the FIFO for SPI according to pointer of the configure struct. Note: If this API is called, please reset the baudrate to adapt your demand after this API was called.
| base | SPI peripheral base address. |
| config | pointer to FIFO configuration structure. |
| void SPI_DisableFifo | ( | SPI_Type * | base | ) |
This function will Disable the FIFO for SPI transfer. disable interrupts, clear status flags, disable the TX/RX FIFO, set fifo size to zero. But will not disable the system FIFO, because other instance like USART may using the FIFO.
| base | SPI peripheral base address. |
| config | pointer to FIFO configuration structure. |
| bool SPI_IsTxFifoEnabled | ( | SPI_Type * | base | ) |
This function will return status if the transmit fifo is enabled. true for enabled and false for not enabled.
| base | SPI peripheral base address. |
| bool SPI_IsRxFifoEnabled | ( | SPI_Type * | base | ) |
This function will return status if the receive fifo is enabled. true for enabled and false for not enabled.
| base | SPI peripheral base address. |
| void SPI_FifoFlush | ( | SPI_Type * | base, |
| uint32_t | direction | ||
| ) |
This function will Flush tHE fifo buffer.
| base | SPI peripheral base address. |
| direction | the fifo direction need to flushed, Tx FIFO or Rx FIFO. |
| status_t SPI_MasterTransferCreateHandle | ( | SPI_Type * | base, |
| spi_master_handle_t * | handle, | ||
| spi_master_callback_t | callback, | ||
| void * | userData | ||
| ) |
This function initializes the SPI master handle which can be used for other SPI master transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.
| base | SPI peripheral base address. |
| handle | SPI handle pointer. |
| callback | Callback function. |
| userData | User data. |
| status_t SPI_MasterTransferBlocking | ( | SPI_Type * | base, |
| spi_transfer_t * | xfer | ||
| ) |
| base | SPI base pointer |
| xfer | pointer to spi_xfer_config_t structure |
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| status_t SPI_MasterTransferNonBlocking | ( | SPI_Type * | base, |
| spi_master_handle_t * | handle, | ||
| spi_transfer_t * | xfer | ||
| ) |
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state |
| xfer | pointer to spi_xfer_config_t structure |
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| kStatus_SPI_Busy | SPI is not idle, is running another transfer. |
| status_t SPI_MasterHalfDuplexTransferBlocking | ( | SPI_Type * | base, |
| spi_half_duplex_transfer_t * | xfer | ||
| ) |
This function will do a half-duplex transfer for SPI master, This is a blocking function, which does not retuen until all transfer have been completed. And data transfer will be half-duplex, users can set transmit first or receive first.
| base | SPI base pointer |
| xfer | pointer to spi_half_duplex_transfer_t structure |
| status_t SPI_MasterHalfDuplexTransferNonBlocking | ( | SPI_Type * | base, |
| spi_master_handle_t * | handle, | ||
| spi_half_duplex_transfer_t * | xfer | ||
| ) |
This function using polling way to do the first half transimission and using interrupts to do the srcond half transimission, the transfer mechanism is half-duplex. When do the second half transimission, code will return right away. When all data is transferred, the callback function is called.
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state |
| xfer | pointer to spi_half_duplex_transfer_t structure |
| status_t SPI_MasterTransferGetCount | ( | SPI_Type * | base, |
| spi_master_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the master transfer count.
| base | SPI peripheral base address. |
| handle | Pointer to the spi_master_handle_t structure which stores the transfer state. |
| count | The number of bytes transferred by using the non-blocking transaction. |
| void SPI_MasterTransferAbort | ( | SPI_Type * | base, |
| spi_master_handle_t * | handle | ||
| ) |
This function aborts a transfer using an interrupt.
| base | SPI peripheral base address. |
| handle | Pointer to the spi_master_handle_t structure which stores the transfer state. |
| void SPI_MasterTransferHandleIRQ | ( | SPI_Type * | base, |
| spi_master_handle_t * | handle | ||
| ) |
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state. |
| status_t SPI_SlaveTransferCreateHandle | ( | SPI_Type * | base, |
| spi_slave_handle_t * | handle, | ||
| spi_slave_callback_t | callback, | ||
| void * | userData | ||
| ) |
This function initializes the SPI slave handle which can be used for other SPI slave transactional APIs. Usually, for a specified SPI instance, call this API once to get the initialized handle.
| base | SPI peripheral base address. |
| handle | SPI handle pointer. |
| callback | Callback function. |
| userData | User data. |
| status_t SPI_SlaveTransferNonBlocking | ( | SPI_Type * | base, |
| spi_slave_handle_t * | handle, | ||
| spi_transfer_t * | xfer | ||
| ) |
| base | SPI peripheral base address. |
| handle | pointer to spi_master_handle_t structure which stores the transfer state |
| xfer | pointer to spi_xfer_config_t structure |
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| kStatus_SPI_Busy | SPI is not idle, is running another transfer. |
|
inlinestatic |
This function gets the slave transfer count.
| base | SPI peripheral base address. |
| handle | Pointer to the spi_master_handle_t structure which stores the transfer state. |
| count | The number of bytes transferred by using the non-blocking transaction. |
|
inlinestatic |
This function aborts a transfer using an interrupt.
| base | SPI peripheral base address. |
| handle | Pointer to the spi_slave_handle_t structure which stores the transfer state. |
| void SPI_SlaveTransferHandleIRQ | ( | SPI_Type * | base, |
| spi_slave_handle_t * | handle | ||
| ) |
| base | SPI peripheral base address. |
| handle | pointer to spi_slave_handle_t structure which stores the transfer state |
| volatile uint8_t s_dummyData[] |