![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
struct | i2c_master_dma_handle_t |
I2C master DMA transfer structure. More... | |
Typedefs | |
typedef void(* | i2c_master_dma_transfer_callback_t )(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) |
I2C master DMA transfer callback typedef. More... | |
Driver version | |
#define | FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 7)) |
I2C DMA driver version 2.0.5. More... | |
I2C Block DMA Transfer Operation | |
void | I2C_MasterTransferCreateHandleDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_dma_transfer_callback_t callback, void *userData, dma_handle_t *dmaHandle) |
Initializes the I2C handle which is used in transactional functions. More... | |
status_t | I2C_MasterTransferDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_transfer_t *xfer) |
Performs a master DMA non-blocking transfer on the I2C bus. More... | |
status_t | I2C_MasterTransferGetCountDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, size_t *count) |
Gets a master transfer status during a DMA non-blocking transfer. More... | |
void | I2C_MasterTransferAbortDMA (I2C_Type *base, i2c_master_dma_handle_t *handle) |
Aborts a master DMA non-blocking transfer early. More... | |
struct _i2c_master_dma_handle |
I2C master DMA handle typedef.
Data Fields | |
i2c_master_transfer_t | transfer |
I2C master transfer struct. More... | |
size_t | transferSize |
Total bytes to be transferred. More... | |
uint8_t | state |
I2C master transfer status. More... | |
dma_handle_t * | dmaHandle |
The DMA handler used. More... | |
i2c_master_dma_transfer_callback_t | completionCallback |
A callback function called after the DMA transfer finished. More... | |
void * | userData |
A callback parameter passed to the callback function. More... | |
i2c_master_transfer_t i2c_master_dma_handle_t::transfer |
size_t i2c_master_dma_handle_t::transferSize |
uint8_t i2c_master_dma_handle_t::state |
dma_handle_t* i2c_master_dma_handle_t::dmaHandle |
i2c_master_dma_transfer_callback_t i2c_master_dma_handle_t::completionCallback |
void* i2c_master_dma_handle_t::userData |
#define FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 7)) |
typedef void(* i2c_master_dma_transfer_callback_t)(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) |
void I2C_MasterTransferCreateHandleDMA | ( | I2C_Type * | base, |
i2c_master_dma_handle_t * | handle, | ||
i2c_master_dma_transfer_callback_t | callback, | ||
void * | userData, | ||
dma_handle_t * | dmaHandle | ||
) |
base | I2C peripheral base address |
handle | Pointer to the i2c_master_dma_handle_t structure |
callback | Pointer to the user callback function |
userData | A user parameter passed to the callback function |
dmaHandle | DMA handle pointer |
status_t I2C_MasterTransferDMA | ( | I2C_Type * | base, |
i2c_master_dma_handle_t * | handle, | ||
i2c_master_transfer_t * | xfer | ||
) |
base | I2C peripheral base address |
handle | A pointer to the i2c_master_dma_handle_t structure |
xfer | A pointer to the transfer structure of the i2c_master_transfer_t |
kStatus_Success | Successfully completes the data transmission. |
kStatus_I2C_Busy | A previous transmission is still not finished. |
kStatus_I2C_Timeout | A transfer error, waits for the signal timeout. |
kStatus_I2C_ArbitrationLost | A transfer error, arbitration lost. |
kStataus_I2C_Nak | A transfer error, receives NAK during transfer. |
status_t I2C_MasterTransferGetCountDMA | ( | I2C_Type * | base, |
i2c_master_dma_handle_t * | handle, | ||
size_t * | count | ||
) |
base | I2C peripheral base address |
handle | A pointer to the i2c_master_dma_handle_t structure |
count | A number of bytes transferred so far by the non-blocking transaction. |
void I2C_MasterTransferAbortDMA | ( | I2C_Type * | base, |
i2c_master_dma_handle_t * | handle | ||
) |
base | I2C peripheral base address |
handle | A pointer to the i2c_master_dma_handle_t structure. |