![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | ecspi_sdma_handle_t |
| ECSPI SDMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | ecspi_sdma_callback_t )(ECSPI_Type *base, ecspi_sdma_handle_t *handle, status_t status, void *userData) |
| ECSPI SDMA callback called at the end of transfer. More... | |
Driver version | |
| #define | FSL_ECSPI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
| ECSPI freertos driver version 2.0.1. More... | |
DMA Transactional | |
| void | ECSPI_MasterTransferCreateHandleSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_sdma_callback_t callback, void *userData, sdma_handle_t *txHandle, sdma_handle_t *rxHandle, uint32_t eventSourceTx, uint32_t eventSourceRx, uint32_t TxChannel, uint32_t RxChannel) |
| Initialize the ECSPI master SDMA handle. More... | |
| void | ECSPI_SlaveTransferCreateHandleSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_sdma_callback_t callback, void *userData, sdma_handle_t *txHandle, sdma_handle_t *rxHandle, uint32_t eventSourceTx, uint32_t eventSourceRx, uint32_t TxChannel, uint32_t RxChannel) |
| Initialize the ECSPI Slave SDMA handle. More... | |
| status_t | ECSPI_MasterTransferSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_transfer_t *xfer) |
| Perform a non-blocking ECSPI master transfer using SDMA. More... | |
| status_t | ECSPI_SlaveTransferSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle, ecspi_transfer_t *xfer) |
| Perform a non-blocking ECSPI slave transfer using SDMA. More... | |
| void | ECSPI_MasterTransferAbortSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle) |
| Abort a ECSPI master transfer using SDMA. More... | |
| void | ECSPI_SlaveTransferAbortSDMA (ECSPI_Type *base, ecspi_sdma_handle_t *handle) |
| Abort a ECSPI slave transfer using SDMA. More... | |
| struct _ecspi_sdma_handle |
Data Fields | |
| bool | txInProgress |
| Send transfer finished. | |
| bool | rxInProgress |
| Receive transfer finished. | |
| sdma_handle_t * | txSdmaHandle |
| DMA handler for ECSPI send. | |
| sdma_handle_t * | rxSdmaHandle |
| DMA handler for ECSPI receive. | |
| ecspi_sdma_callback_t | callback |
| Callback for ECSPI SDMA transfer. | |
| void * | userData |
| User Data for ECSPI SDMA callback. | |
| uint32_t | state |
| Internal state of ECSPI SDMA transfer. | |
| uint32_t | ChannelTx |
| Channel for send handle. | |
| uint32_t | ChannelRx |
| Channel for receive handler. | |
| #define FSL_ECSPI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 0, 1)) |
| typedef void(* ecspi_sdma_callback_t)(ECSPI_Type *base, ecspi_sdma_handle_t *handle, status_t status, void *userData) |
| void ECSPI_MasterTransferCreateHandleSDMA | ( | ECSPI_Type * | base, |
| ecspi_sdma_handle_t * | handle, | ||
| ecspi_sdma_callback_t | callback, | ||
| void * | userData, | ||
| sdma_handle_t * | txHandle, | ||
| sdma_handle_t * | rxHandle, | ||
| uint32_t | eventSourceTx, | ||
| uint32_t | eventSourceRx, | ||
| uint32_t | TxChannel, | ||
| uint32_t | RxChannel | ||
| ) |
This function initializes the ECSPI master SDMA handle which can be used for other SPI master transactional APIs. Usually, for a specified ECSPI instance, user need only call this API once to get the initialized handle.
| base | ECSPI peripheral base address. |
| handle | ECSPI handle pointer. |
| callback | User callback function called at the end of a transfer. |
| userData | User data for callback. |
| txHandle | SDMA handle pointer for ECSPI Tx, the handle shall be static allocated by users. |
| rxHandle | SDMA handle pointer for ECSPI Rx, the handle shall be static allocated by users. |
| eventSourceTx | event source for ECSPI send, which can be found in SDMA mapping. |
| eventSourceRx | event source for ECSPI receive, which can be found in SDMA mapping. |
| TxChannel | SDMA channel for ECSPI send. |
| RxChannel | SDMA channel for ECSPI receive. |
| void ECSPI_SlaveTransferCreateHandleSDMA | ( | ECSPI_Type * | base, |
| ecspi_sdma_handle_t * | handle, | ||
| ecspi_sdma_callback_t | callback, | ||
| void * | userData, | ||
| sdma_handle_t * | txHandle, | ||
| sdma_handle_t * | rxHandle, | ||
| uint32_t | eventSourceTx, | ||
| uint32_t | eventSourceRx, | ||
| uint32_t | TxChannel, | ||
| uint32_t | RxChannel | ||
| ) |
This function initializes the ECSPI Slave SDMA handle which can be used for other SPI Slave transactional APIs. Usually, for a specified ECSPI instance, user need only call this API once to get the initialized handle.
| base | ECSPI peripheral base address. |
| handle | ECSPI handle pointer. |
| callback | User callback function called at the end of a transfer. |
| userData | User data for callback. |
| txHandle | SDMA handle pointer for ECSPI Tx, the handle shall be static allocated by users. |
| rxHandle | SDMA handle pointer for ECSPI Rx, the handle shall be static allocated by users. |
| eventSourceTx | event source for ECSPI send, which can be found in SDMA mapping. |
| eventSourceRx | event source for ECSPI receive, which can be found in SDMA mapping. |
| TxChannel | SDMA channel for ECSPI send. |
| RxChannel | SDMA channel for ECSPI receive. |
| status_t ECSPI_MasterTransferSDMA | ( | ECSPI_Type * | base, |
| ecspi_sdma_handle_t * | handle, | ||
| ecspi_transfer_t * | xfer | ||
| ) |
| base | ECSPI peripheral base address. |
| handle | ECSPI SDMA handle pointer. |
| xfer | Pointer to sdma transfer structure. |
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| kStatus_ECSPI_Busy | EECSPI is not idle, is running another transfer. |
| status_t ECSPI_SlaveTransferSDMA | ( | ECSPI_Type * | base, |
| ecspi_sdma_handle_t * | handle, | ||
| ecspi_transfer_t * | xfer | ||
| ) |
| base | ECSPI peripheral base address. |
| handle | ECSPI SDMA handle pointer. |
| xfer | Pointer to sdma transfer structure. |
| kStatus_Success | Successfully start a transfer. |
| kStatus_InvalidArgument | Input argument is invalid. |
| kStatus_ECSPI_Busy | EECSPI is not idle, is running another transfer. |
| void ECSPI_MasterTransferAbortSDMA | ( | ECSPI_Type * | base, |
| ecspi_sdma_handle_t * | handle | ||
| ) |
| base | ECSPI peripheral base address. |
| handle | ECSPI SDMA handle pointer. |
| void ECSPI_SlaveTransferAbortSDMA | ( | ECSPI_Type * | base, |
| ecspi_sdma_handle_t * | handle | ||
| ) |
| base | ECSPI peripheral base address. |
| handle | ECSPI SDMA handle pointer. |