The MCUXpresso SDK provides a peripheral driver for the General Power Controller (GPC) module of MCUXpresso SDK devices.
API functions are provided to configure the system about working in dedicated power mode. There are mainly about enabling the power for memory, enabling the wakeup sources for STOP modes, and power up/down operations for various peripherals.
| void GPC_EnableIRQ |
( |
GPC_Type * |
base, |
|
|
uint32_t |
irqId |
|
) |
| |
- Parameters
-
| base | GPC peripheral base address. |
| irqId | ID number of IRQ to be enabled, available range is 32-159. |
| void GPC_DisableIRQ |
( |
GPC_Type * |
base, |
|
|
uint32_t |
irqId |
|
) |
| |
- Parameters
-
| base | GPC peripheral base address. |
| irqId | ID number of IRQ to be disabled, available range is 32-159. |
| bool GPC_GetIRQStatusFlag |
( |
GPC_Type * |
base, |
|
|
uint32_t |
irqId |
|
) |
| |
- Parameters
-
| base | GPC peripheral base address. |
| irqId | ID number of IRQ to be enabled, available range is 32-159. |
- Returns
- Indicated IRQ/Event is asserted or not.
| static void GPC_RequestPdram0PowerDown |
( |
GPC_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
This function configures the FLEXRAM PDRAM0 if it will keep power when cpu core is power down. When the PDRAM0 Power is 1, PDRAM0 will be power down once when CPU core is power down. When the PDRAM0 Power is 0, PDRAM0 will keep power on even if CPU core is power down. When CPU core is re-power up, the default setting is 1.
- Parameters
-
| base | GPC peripheral base address. |
| enable | Enable the request or not. |
| static void GPC_RequestMEGAPowerOn |
( |
GPC_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| enable | Enable the power on sequence, or the power down sequence. |