|  | MCUXpresso SDK API Reference Manual
    Rev. 0
    NXP Semiconductors | 
The MCUXpresso SDK provides a driver to access the Secure Digital Card based on the SPI driver.
This function group implements the SD card functional API in the SPI mode.
| Data Structures | |
| struct | sdspi_host_t | 
| SDSPI host state.  More... | |
| struct | sdspi_card_t | 
| SD Card Structure.  More... | |
| Enumerations | |
| enum | _sdspi_status { kStatus_SDSPI_SetFrequencyFailed = MAKE_STATUS(kStatusGroup_SDSPI, 0U), kStatus_SDSPI_ExchangeFailed = MAKE_STATUS(kStatusGroup_SDSPI, 1U), kStatus_SDSPI_WaitReadyFailed = MAKE_STATUS(kStatusGroup_SDSPI, 2U), kStatus_SDSPI_ResponseError = MAKE_STATUS(kStatusGroup_SDSPI, 3U), kStatus_SDSPI_WriteProtected = MAKE_STATUS(kStatusGroup_SDSPI, 4U), kStatus_SDSPI_GoIdleFailed = MAKE_STATUS(kStatusGroup_SDSPI, 5U), kStatus_SDSPI_SendCommandFailed = MAKE_STATUS(kStatusGroup_SDSPI, 6U), kStatus_SDSPI_ReadFailed = MAKE_STATUS(kStatusGroup_SDSPI, 7U), kStatus_SDSPI_WriteFailed = MAKE_STATUS(kStatusGroup_SDSPI, 8U), kStatus_SDSPI_SendInterfaceConditionFailed, kStatus_SDSPI_SendOperationConditionFailed, kStatus_SDSPI_ReadOcrFailed = MAKE_STATUS(kStatusGroup_SDSPI, 11U), kStatus_SDSPI_SetBlockSizeFailed = MAKE_STATUS(kStatusGroup_SDSPI, 12U), kStatus_SDSPI_SendCsdFailed = MAKE_STATUS(kStatusGroup_SDSPI, 13U), kStatus_SDSPI_SendCidFailed = MAKE_STATUS(kStatusGroup_SDSPI, 14U), kStatus_SDSPI_StopTransmissionFailed = MAKE_STATUS(kStatusGroup_SDSPI, 15U), kStatus_SDSPI_SendApplicationCommandFailed, kStatus_SDSPI_InvalidVoltage = MAKE_STATUS(kStatusGroup_SDSPI, 17U), kStatus_SDSPI_SwitchCmdFail = MAKE_STATUS(kStatusGroup_SDSPI, 18U), kStatus_SDSPI_NotSupportYet = MAKE_STATUS(kStatusGroup_SDSPI, 19U) } | 
| SDSPI API status.  More... | |
| enum | _sdspi_card_flag { kSDSPI_SupportHighCapacityFlag = (1U << 0U), kSDSPI_SupportSdhcFlag = (1U << 1U), kSDSPI_SupportSdxcFlag = (1U << 2U), kSDSPI_SupportSdscFlag = (1U << 3U) } | 
| SDSPI card flag.  More... | |
| enum | _sdspi_response_type { kSDSPI_ResponseTypeR1 = 0U, kSDSPI_ResponseTypeR1b = 1U, kSDSPI_ResponseTypeR2 = 2U, kSDSPI_ResponseTypeR3 = 3U, kSDSPI_ResponseTypeR7 = 4U } | 
| SDSPI response type.  More... | |
| enum | _sdspi_cmd { kSDSPI_CmdGoIdle = kSDMMC_GoIdleState << 8U | kSDSPI_ResponseTypeR1, kSDSPI_CmdCrc = kSDSPI_CommandCrc << 8U | kSDSPI_ResponseTypeR1, kSDSPI_CmdSendInterfaceCondition } | 
| SDSPI command type.  More... | |
| SDSPI Function | |
| status_t | SDSPI_Init (sdspi_card_t *card) | 
| Initializes the card on a specific SPI instance.  More... | |
| void | SDSPI_Deinit (sdspi_card_t *card) | 
| Deinitializes the card.  More... | |
| bool | SDSPI_CheckReadOnly (sdspi_card_t *card) | 
| Checks whether the card is write-protected.  More... | |
| status_t | SDSPI_ReadBlocks (sdspi_card_t *card, uint8_t *buffer, uint32_t startBlock, uint32_t blockCount) | 
| Reads blocks from the specific card.  More... | |
| status_t | SDSPI_WriteBlocks (sdspi_card_t *card, uint8_t *buffer, uint32_t startBlock, uint32_t blockCount) | 
| Writes blocks of data to the specific card.  More... | |
| status_t | SDSPI_SendCid (sdspi_card_t *card) | 
| Send GET-CID command In our sdspi init function, this function is removed for better code size, if id information is needed, you can call it after the init function directly.  More... | |
| status_t | SDSPI_SendPreErase (sdspi_card_t *card, uint32_t blockCount) | 
| Multiple blocks write pre-erase function.  More... | |
| status_t | SDSPI_EraseBlocks (sdspi_card_t *card, uint32_t startBlock, uint32_t blockCount) | 
| Block erase function.  More... | |
| status_t | SDSPI_SwitchToHighSpeed (sdspi_card_t *card) | 
| Switch to high speed function.  More... | |
| struct sdspi_host_t | 
| Data Fields | |
| uint32_t | busBaudRate | 
| Bus baud rate. | |
| status_t(* | setFrequency )(uint32_t frequency) | 
| Set frequency of SPI. | |
| status_t(* | exchange )(uint8_t *in, uint8_t *out, uint32_t size) | 
| Exchange data over SPI. | |
| struct sdspi_card_t | 
Define the card structure including the necessary fields to identify and describe the card.
| Data Fields | |
| sdspi_host_t * | host | 
| Host state information. | |
| uint32_t | relativeAddress | 
| Relative address of the card. | |
| uint32_t | flags | 
| Flags defined in _sdspi_card_flag.  More... | |
| uint8_t | rawCid [16U] | 
| Raw CID content. | |
| uint8_t | rawCsd [16U] | 
| Raw CSD content. | |
| uint8_t | rawScr [8U] | 
| Raw SCR content. | |
| uint32_t | ocr | 
| Raw OCR content. | |
| sd_cid_t | cid | 
| CID. | |
| sd_csd_t | csd | 
| CSD. | |
| sd_scr_t | scr | 
| SCR. | |
| uint32_t | blockCount | 
| Card total block number. | |
| uint32_t | blockSize | 
| Card block size. | |
| uint32_t sdspi_card_t::flags | 
| enum _sdspi_status | 
| enum _sdspi_card_flag | 
| enum _sdspi_response_type | 
| enum _sdspi_cmd | 
| status_t SDSPI_Init | ( | sdspi_card_t * | card | ) | 
This function initializes the card on a specific SPI instance.
| card | Card descriptor | 
| kStatus_SDSPI_SetFrequencyFailed | Set frequency failed. | 
| kStatus_SDSPI_GoIdleFailed | Go idle failed. | 
| kStatus_SDSPI_SendInterfaceConditionFailed | Send interface condition failed. | 
| kStatus_SDSPI_SendOperationConditionFailed | Send operation condition failed. | 
| kStatus_Timeout | Send command timeout. | 
| kStatus_SDSPI_NotSupportYet | Not support yet. | 
| kStatus_SDSPI_ReadOcrFailed | Read OCR failed. | 
| kStatus_SDSPI_SetBlockSizeFailed | Set block size failed. | 
| kStatus_SDSPI_SendCsdFailed | Send CSD failed. | 
| kStatus_SDSPI_SendCidFailed | Send CID failed. | 
| kStatus_Success | Operate successfully. | 
| void SDSPI_Deinit | ( | sdspi_card_t * | card | ) | 
This function deinitializes the specific card.
| card | Card descriptor | 
| bool SDSPI_CheckReadOnly | ( | sdspi_card_t * | card | ) | 
This function checks if the card is write-protected via CSD register.
| card | Card descriptor. | 
| true | Card is read only. | 
| false | Card isn't read only. | 
| status_t SDSPI_ReadBlocks | ( | sdspi_card_t * | card, | 
| uint8_t * | buffer, | ||
| uint32_t | startBlock, | ||
| uint32_t | blockCount | ||
| ) | 
This function reads blocks from specific card.
| card | Card descriptor. | 
| buffer | the buffer to hold the data read from card | 
| startBlock | the start block index | 
| blockCount | the number of blocks to read | 
| kStatus_SDSPI_SendCommandFailed | Send command failed. | 
| kStatus_SDSPI_ReadFailed | Read data failed. | 
| kStatus_SDSPI_StopTransmissionFailed | Stop transmission failed. | 
| kStatus_Success | Operate successfully. | 
| status_t SDSPI_WriteBlocks | ( | sdspi_card_t * | card, | 
| uint8_t * | buffer, | ||
| uint32_t | startBlock, | ||
| uint32_t | blockCount | ||
| ) | 
This function writes blocks to specific card
| card | Card descriptor. | 
| buffer | the buffer holding the data to be written to the card | 
| startBlock | the start block index | 
| blockCount | the number of blocks to write | 
| kStatus_SDSPI_WriteProtected | Card is write protected. | 
| kStatus_SDSPI_SendCommandFailed | Send command failed. | 
| kStatus_SDSPI_ResponseError | Response is error. | 
| kStatus_SDSPI_WriteFailed | Write data failed. | 
| kStatus_SDSPI_ExchangeFailed | Exchange data over SPI failed. | 
| kStatus_SDSPI_WaitReadyFailed | Wait card to be ready status failed. | 
| kStatus_Success | Operate successfully. | 
| status_t SDSPI_SendCid | ( | sdspi_card_t * | card | ) | 
| card | Card descriptor. | 
| kStatus_SDSPI_SendCommandFailed | Send command failed. | 
| kStatus_SDSPI_ReadFailed | Read data blocks failed. | 
| kStatus_Success | Operate successfully. | 
| status_t SDSPI_SendPreErase | ( | sdspi_card_t * | card, | 
| uint32_t | blockCount | ||
| ) | 
This function should be called before SDSPI_WriteBlocks, it is used to set the number of the write blocks to be pre-erased before writing.
| card | Card descriptor. | 
| blockCount | the block counts to be write. | 
| kStatus_SDSPI_SendCommandFailed | Send command failed. | 
| kStatus_SDSPI_SendApplicationCommandFailed | |
| kStatus_SDSPI_ResponseError | |
| kStatus_Success | Operate successfully. | 
| status_t SDSPI_EraseBlocks | ( | sdspi_card_t * | card, | 
| uint32_t | startBlock, | ||
| uint32_t | blockCount | ||
| ) | 
| card | Card descriptor. | 
| startBlock | start block address to be erase. | 
| blockCount | the block counts to be erase. | 
| kStatus_SDSPI_WaitReadyFailed | Wait ready failed. | 
| kStatus_SDSPI_SendCommandFailed | Send command failed. | 
| kStatus_Success | Operate successfully. | 
| status_t SDSPI_SwitchToHighSpeed | ( | sdspi_card_t * | card | ) | 
This function can be called after SDSPI_Init function if target board's layout support >25MHZ spi baudrate, otherwise this function is useless.Be careful with call this function, code size and stack usage will be enlarge.
| card | Card descriptor. | 
| kStatus_Fail | switch failed. | 
| kStatus_Success | Operate successfully. |