|  | MCUXpresso SDK API Reference Manual
    Rev. 0
    NXP Semiconductors | 
| Files | |
| file | fsl_i2s.h | 
| Data Structures | |
| struct | i2s_config_t | 
| I2S configuration structure.  More... | |
| struct | i2s_transfer_t | 
| Buffer to transfer from or receive audio data into.  More... | |
| struct | i2s_handle_t | 
| Members not to be accessed / modified outside of the driver.  More... | |
| Macros | |
| #define | I2S_NUM_BUFFERS (4) | 
| Number of buffers .  More... | |
| Typedefs | |
| typedef void(* | i2s_transfer_callback_t )(I2S_Type *base, i2s_handle_t *handle, status_t completionStatus, void *userData) | 
| Callback function invoked from transactional API on completion of a single buffer transfer.  More... | |
| Enumerations | |
| enum | _i2s_status { kStatus_I2S_BufferComplete, kStatus_I2S_Done = MAKE_STATUS(kStatusGroup_I2S, 1), kStatus_I2S_Busy } | 
| I2S status codes.  More... | |
| enum | i2s_flags_t { kI2S_TxErrorFlag = I2S_FIFOINTENSET_TXERR_MASK, kI2S_TxLevelFlag = I2S_FIFOINTENSET_TXLVL_MASK, kI2S_RxErrorFlag = I2S_FIFOINTENSET_RXERR_MASK, kI2S_RxLevelFlag = I2S_FIFOINTENSET_RXLVL_MASK } | 
| I2S flags.  More... | |
| enum | i2s_master_slave_t { kI2S_MasterSlaveNormalSlave = 0x0, kI2S_MasterSlaveWsSyncMaster = 0x1, kI2S_MasterSlaveExtSckMaster = 0x2, kI2S_MasterSlaveNormalMaster = 0x3 } | 
| Master / slave mode.  More... | |
| enum | i2s_mode_t { kI2S_ModeI2sClassic = 0x0, kI2S_ModeDspWs50 = 0x1, kI2S_ModeDspWsShort = 0x2, kI2S_ModeDspWsLong = 0x3 } | 
| I2S mode.  More... | |
| enum | _i2s_secondary_channel { kI2S_SecondaryChannel1 = 0U, kI2S_SecondaryChannel2 = 1U, kI2S_SecondaryChannel3 = 2U } | 
| I2S secondary channel.  More... | |
| Driver version | |
| #define | FSL_I2S_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) | 
| I2S driver version 2.1.0.  More... | |
| Initialization and deinitialization | |
| void | I2S_TxInit (I2S_Type *base, const i2s_config_t *config) | 
| Initializes the FLEXCOMM peripheral for I2S transmit functionality.  More... | |
| void | I2S_RxInit (I2S_Type *base, const i2s_config_t *config) | 
| Initializes the FLEXCOMM peripheral for I2S receive functionality.  More... | |
| void | I2S_TxGetDefaultConfig (i2s_config_t *config) | 
| Sets the I2S Tx configuration structure to default values.  More... | |
| void | I2S_RxGetDefaultConfig (i2s_config_t *config) | 
| Sets the I2S Rx configuration structure to default values.  More... | |
| void | I2S_Deinit (I2S_Type *base) | 
| De-initializes the I2S peripheral.  More... | |
| Non-blocking API | |
| void | I2S_TxTransferCreateHandle (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_callback_t callback, void *userData) | 
| Initializes handle for transfer of audio data.  More... | |
| status_t | I2S_TxTransferNonBlocking (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_t transfer) | 
| Begins or queue sending of the given data.  More... | |
| void | I2S_TxTransferAbort (I2S_Type *base, i2s_handle_t *handle) | 
| Aborts sending of data.  More... | |
| void | I2S_RxTransferCreateHandle (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_callback_t callback, void *userData) | 
| Initializes handle for reception of audio data.  More... | |
| status_t | I2S_RxTransferNonBlocking (I2S_Type *base, i2s_handle_t *handle, i2s_transfer_t transfer) | 
| Begins or queue reception of data into given buffer.  More... | |
| void | I2S_RxTransferAbort (I2S_Type *base, i2s_handle_t *handle) | 
| Aborts receiving of data.  More... | |
| status_t | I2S_TransferGetCount (I2S_Type *base, i2s_handle_t *handle, size_t *count) | 
| Returns number of bytes transferred so far.  More... | |
| status_t | I2S_TransferGetErrorCount (I2S_Type *base, i2s_handle_t *handle, size_t *count) | 
| Returns number of buffer underruns or overruns.  More... | |
| Enable / disable | |
| static void | I2S_Enable (I2S_Type *base) | 
| Enables I2S operation.  More... | |
| static void | I2S_Disable (I2S_Type *base) | 
| Disables I2S operation.  More... | |
| Interrupts | |
| static void | I2S_EnableInterrupts (I2S_Type *base, uint32_t interruptMask) | 
| Enables I2S FIFO interrupts.  More... | |
| static void | I2S_DisableInterrupts (I2S_Type *base, uint32_t interruptMask) | 
| Disables I2S FIFO interrupts.  More... | |
| static uint32_t | I2S_GetEnabledInterrupts (I2S_Type *base) | 
| Returns the set of currently enabled I2S FIFO interrupts.  More... | |
| void | I2S_TxHandleIRQ (I2S_Type *base, i2s_handle_t *handle) | 
| Invoked from interrupt handler when transmit FIFO level decreases.  More... | |
| void | I2S_RxHandleIRQ (I2S_Type *base, i2s_handle_t *handle) | 
| Invoked from interrupt handler when receive FIFO level decreases.  More... | |
| struct i2s_config_t | 
| Data Fields | |
| i2s_master_slave_t | masterSlave | 
| Master / slave configuration. | |
| i2s_mode_t | mode | 
| I2S mode. | |
| bool | rightLow | 
| Right channel data in low portion of FIFO. | |
| bool | leftJust | 
| Left justify data in FIFO. | |
| bool | sckPol | 
| SCK polarity. | |
| bool | wsPol | 
| WS polarity. | |
| uint16_t | divider | 
| Flexcomm function clock divider (1 - 4096) | |
| bool | oneChannel | 
| true mono, false stereo | |
| uint8_t | dataLength | 
| Data length (4 - 32) | |
| uint16_t | frameLength | 
| Frame width (4 - 512) | |
| uint16_t | position | 
| Data position in the frame. | |
| uint8_t | watermark | 
| FIFO trigger level. | |
| bool | txEmptyZero | 
| Transmit zero when buffer becomes empty or last item. | |
| bool | pack48 | 
| Packing format for 48-bit data (false - 24 bit values, true - alternating 32-bit and 16-bit values) | |
| struct i2s_transfer_t | 
| struct _i2s_handle | 
Transactional state of the intialized transfer or receive I2S operation.
| Data Fields | |
| uint32_t | state | 
| State of transfer. | |
| i2s_transfer_callback_t | completionCallback | 
| Callback function pointer. | |
| void * | userData | 
| Application data passed to callback. | |
| bool | oneChannel | 
| true mono, false stereo | |
| uint8_t | dataLength | 
| Data length (4 - 32) | |
| bool | pack48 | 
| Packing format for 48-bit data (false - 24 bit values, true - alternating 32-bit and 16-bit values) | |
| bool | useFifo48H | 
| When dataLength 17-24: true use FIFOWR48H, false use FIFOWR. | |
| volatile i2s_transfer_t | i2sQueue [I2S_NUM_BUFFERS] | 
| Transfer queue storing transfer buffers. | |
| volatile uint8_t | queueUser | 
| Queue index where user's next transfer will be stored. | |
| volatile uint8_t | queueDriver | 
| Queue index of buffer actually used by the driver. | |
| volatile uint32_t | errorCount | 
| Number of buffer underruns/overruns. | |
| volatile uint32_t | transferCount | 
| Number of bytes transferred. | |
| volatile uint8_t | watermark | 
| FIFO trigger level. | |
| #define FSL_I2S_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) | 
| #define I2S_NUM_BUFFERS (4) | 
| typedef void(* i2s_transfer_callback_t)(I2S_Type *base, i2s_handle_t *handle, status_t completionStatus, void *userData) | 
| base | I2S base pointer. | 
| handle | pointer to I2S transaction. | 
| completionStatus | status of the transaction. | 
| userData | optional pointer to user arguments data. | 
| enum _i2s_status | 
| enum i2s_flags_t | 
| enum i2s_master_slave_t | 
| enum i2s_mode_t | 
| void I2S_TxInit | ( | I2S_Type * | base, | 
| const i2s_config_t * | config | ||
| ) | 
Ungates the FLEXCOMM clock and configures the module for I2S transmission using a configuration structure. The configuration structure can be custom filled or set with default values by I2S_TxGetDefaultConfig().
| base | I2S base pointer. | 
| config | pointer to I2S configuration structure. | 
| void I2S_RxInit | ( | I2S_Type * | base, | 
| const i2s_config_t * | config | ||
| ) | 
Ungates the FLEXCOMM clock and configures the module for I2S receive using a configuration structure. The configuration structure can be custom filled or set with default values by I2S_RxGetDefaultConfig().
| base | I2S base pointer. | 
| config | pointer to I2S configuration structure. | 
| void I2S_TxGetDefaultConfig | ( | i2s_config_t * | config | ) | 
This API initializes the configuration structure for use in I2S_TxInit(). The initialized structure can remain unchanged in I2S_TxInit(), or it can be modified before calling I2S_TxInit(). Example:
Default values:
| config | pointer to I2S configuration structure. | 
| void I2S_RxGetDefaultConfig | ( | i2s_config_t * | config | ) | 
This API initializes the configuration structure for use in I2S_RxInit(). The initialized structure can remain unchanged in I2S_RxInit(), or it can be modified before calling I2S_RxInit(). Example:
Default values:
| config | pointer to I2S configuration structure. | 
| void I2S_Deinit | ( | I2S_Type * | base | ) | 
This API gates the FLEXCOMM clock. The I2S module can't operate unless I2S_TxInit or I2S_RxInit is called to enable the clock.
| base | I2S base pointer. | 
| void I2S_TxTransferCreateHandle | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle, | ||
| i2s_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| callback | function to be called back when transfer is done or fails. | 
| userData | pointer to data passed to callback. | 
| status_t I2S_TxTransferNonBlocking | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle, | ||
| i2s_transfer_t | transfer | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| transfer | data buffer. | 
| kStatus_Success | |
| kStatus_I2S_Busy | if all queue slots are occupied with unsent buffers. | 
| void I2S_TxTransferAbort | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| void I2S_RxTransferCreateHandle | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle, | ||
| i2s_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| callback | function to be called back when transfer is done or fails. | 
| userData | pointer to data passed to callback. | 
| status_t I2S_RxTransferNonBlocking | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle, | ||
| i2s_transfer_t | transfer | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| transfer | data buffer. | 
| kStatus_Success | |
| kStatus_I2S_Busy | if all queue slots are occupied with buffers which are not full. | 
| void I2S_RxTransferAbort | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| status_t I2S_TransferGetCount | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | I2S base pointer. | |
| handle | pointer to handle structure. | |
| [out] | count | number of bytes transferred so far by the non-blocking transaction. | 
| kStatus_Success | |
| kStatus_NoTransferInProgress | there is no non-blocking transaction currently in progress. | 
| status_t I2S_TransferGetErrorCount | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | I2S base pointer. | |
| handle | pointer to handle structure. | |
| [out] | count | number of transmit errors encountered so far by the non-blocking transaction. | 
| kStatus_Success | |
| kStatus_NoTransferInProgress | there is no non-blocking transaction currently in progress. | 
| 
 | inlinestatic | 
| base | I2S base pointer. | 
| 
 | inlinestatic | 
| base | I2S base pointer. | 
| 
 | inlinestatic | 
| base | I2S base pointer. | 
| interruptMask | bit mask of interrupts to enable. See i2s_flags_t for the set of constants that should be OR'd together to form the bit mask. | 
| 
 | inlinestatic | 
| base | I2S base pointer. | 
| interruptMask | bit mask of interrupts to enable. See i2s_flags_t for the set of constants that should be OR'd together to form the bit mask. | 
| 
 | inlinestatic | 
| base | I2S base pointer. | 
| void I2S_TxHandleIRQ | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| void I2S_RxHandleIRQ | ( | I2S_Type * | base, | 
| i2s_handle_t * | handle | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. |