| Enumerator | 
|---|
| kSerialManager_UsbVirtualControllerKhci0 | KHCI 0U.  | 
| kSerialManager_UsbVirtualControllerKhci1 | KHCI 1U, Currently, there are no platforms which have two KHCI IPs, this is reserved to be used in the future.  | 
| kSerialManager_UsbVirtualControllerEhci0 | EHCI 0U.  | 
| kSerialManager_UsbVirtualControllerEhci1 | EHCI 1U, Currently, there are no platforms which have two EHCI IPs, this is reserved to be used in the future.  | 
| kSerialManager_UsbVirtualControllerLpcIp3511Fs0 | LPC USB IP3511 FS controller 0.  | 
| kSerialManager_UsbVirtualControllerLpcIp3511Fs1 | LPC USB IP3511 FS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.  | 
| kSerialManager_UsbVirtualControllerLpcIp3511Hs0 | LPC USB IP3511 HS controller 0.  | 
| kSerialManager_UsbVirtualControllerLpcIp3511Hs1 | LPC USB IP3511 HS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.  | 
| kSerialManager_UsbVirtualControllerOhci0 | OHCI 0U.  | 
| kSerialManager_UsbVirtualControllerOhci1 | OHCI 1U, Currently, there are no platforms which have two OHCI IPs, this is reserved to be used in the future.  | 
| kSerialManager_UsbVirtualControllerIp3516Hs0 | IP3516HS 0U.  | 
| kSerialManager_UsbVirtualControllerIp3516Hs1 | IP3516HS 1U, Currently, there are no platforms which have two IP3516HS IPs, this is reserved to be used in the future.  |