|  | MCUXpresso SDK API Reference Manual
    Rev. 0
    NXP Semiconductors | 
| Files | |
| file | fsl_usart_freertos.h | 
| Data Structures | |
| struct | rtos_usart_config | 
| FLEX USART configuration structure.  More... | |
| struct | usart_rtos_handle_t | 
| FLEX USART FreeRTOS handle.  More... | |
| Driver version | |
| #define | FSL_USART_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) | 
| USART freertos driver version 2.0.1.  More... | |
| USART RTOS Operation | |
| int | USART_RTOS_Init (usart_rtos_handle_t *handle, usart_handle_t *t_handle, const struct rtos_usart_config *cfg) | 
| Initializes a USART instance for operation in RTOS.  More... | |
| int | USART_RTOS_Deinit (usart_rtos_handle_t *handle) | 
| Deinitializes a USART instance for operation.  More... | |
| USART transactional Operation | |
| int | USART_RTOS_Send (usart_rtos_handle_t *handle, const uint8_t *buffer, uint32_t length) | 
| Sends data in the background.  More... | |
| int | USART_RTOS_Receive (usart_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received) | 
| Receives data.  More... | |
| struct rtos_usart_config | 
| Data Fields | |
| USART_Type * | base | 
| USART base address. | |
| uint32_t | srcclk | 
| USART source clock in Hz. | |
| uint32_t | baudrate | 
| Desired communication speed. | |
| usart_parity_mode_t | parity | 
| Parity setting. | |
| usart_stop_bit_count_t | stopbits | 
| Number of stop bits to use. | |
| uint8_t * | buffer | 
| Buffer for background reception. | |
| uint32_t | buffer_size | 
| Size of buffer for background reception. | |
| struct usart_rtos_handle_t | 
| Data Fields | |
| USART_Type * | base | 
| USART base address. | |
| usart_transfer_t | txTransfer | 
| TX transfer structure. | |
| usart_transfer_t | rxTransfer | 
| RX transfer structure. | |
| SemaphoreHandle_t | rxSemaphore | 
| RX semaphore for resource sharing. | |
| SemaphoreHandle_t | txSemaphore | 
| TX semaphore for resource sharing. | |
| EventGroupHandle_t | rxEvent | 
| RX completion event. | |
| EventGroupHandle_t | txEvent | 
| TX completion event. | |
| void * | t_state | 
| Transactional state of the underlying driver. | |
| #define FSL_USART_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 1, 0)) | 
| int USART_RTOS_Init | ( | usart_rtos_handle_t * | handle, | 
| usart_handle_t * | t_handle, | ||
| const struct rtos_usart_config * | cfg | ||
| ) | 
| handle | The RTOS USART handle, the pointer to allocated space for RTOS context. | 
| t_handle | The pointer to allocated space where to store transactional layer internal state. | 
| cfg | The pointer to the parameters required to configure the USART after initialization. | 
| int USART_RTOS_Deinit | ( | usart_rtos_handle_t * | handle | ) | 
This function deinitializes the USART module, sets all register values to reset value, and releases the resources.
| handle | The RTOS USART handle. | 
| int USART_RTOS_Send | ( | usart_rtos_handle_t * | handle, | 
| const uint8_t * | buffer, | ||
| uint32_t | length | ||
| ) | 
This function sends data. It is a synchronous API. If the hardware buffer is full, the task is in the blocked state.
| handle | The RTOS USART handle. | 
| buffer | The pointer to buffer to send. | 
| length | The number of bytes to send. | 
| int USART_RTOS_Receive | ( | usart_rtos_handle_t * | handle, | 
| uint8_t * | buffer, | ||
| uint32_t | length, | ||
| size_t * | received | ||
| ) | 
This function receives data from USART. It is a synchronous API. If data is immediately available, it is returned immediately and the number of bytes received.
| handle | The RTOS USART handle. | 
| buffer | The pointer to buffer where to write received data. | 
| length | The number of bytes to receive. | 
| received | The pointer to a variable of size_t where the number of received data is filled. |