MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

Files

file  fsl_clock.h
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0
 Configure whether driver controls clock. More...
 
#define MU_CLOCKS
 Clock ip name array for MU. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define FLEXSPI_CLOCKS
 Clock ip name array for FLEXSPI. More...
 
#define RGPIO_CLOCKS
 Clock ip name array for RGPIO. More...
 
#define FTM_CLOCKS
 Clock ip name array for FTM. More...
 
#define GPT_CLOCKS
 Clock ip name array for GPT. More...
 
#define FLEXCAN_CLOCKS
 Clock ip name array for FLEXCAN. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define LPADC_CLOCKS
 Clock ip name array for LPADC. More...
 
#define INTMUX_CLOCKS
 Clock ip name array for INTMUX. More...
 
#define SAI_CLOCKS
 Clock ip name array for SAI. More...
 
#define SEMA42_CLOCKS
 Clock ip name array for SAI. More...
 
#define TPM_CLOCKS
 Clock ip name array for TPM. More...
 
#define LPIT_CLOCKS
 Clock ip name array for LPIT. More...
 
#define LPI2C_CLOCKS
 Clock ip name array for LPI2C. More...
 
#define LPSPI_CLOCKS
 Clock ip name array for LPSPI. More...
 
#define EDMA_CLOCKS
 Clock ip name array for EDMA. More...
 
#define ESAI_CLOCKS
 Clock ip name array for LPIT. More...
 
#define ISI_CLOCKS
 Clock ip name array for ISI. More...
 
#define MIPI_CSI2RX_CLOCKS
 Clock ip name array for MIPI CSI2 RX. More...
 
#define MIPI_DSI_HOST_CLOCKS
 Clock ip name array for MIPI DSI host. More...
 
#define ENET_CLOCKS
 Clock ip name array for ENET. More...
 
#define DPU_CLOCKS
 Clock ip name array for DPU. More...
 
#define CI_PI_CLOCKS
 Clock ip name array for CI_PI. More...
 
#define CAAM_CLOCKS
 Clock ip name array for CAAM. More...
 
#define LDB_CLOCKS
 Clock ip name array for LVDS display bridge(LDB). More...
 
#define LPCG_TUPLE(rsrc, base)   ((uint32_t)((((base) >> 12U) << 10U) | rsrc))
 LPCG TUPLE macors to map corresponding ip clock name, SCFW API resource index and LPCG Register base address. More...
 
#define LPCG_TUPLE_REG_BASE(tuple)   ((volatile uint32_t *)((((uint32_t)(tuple) >> 10U) & 0xFFFFFU) << 12U))
 Get the LPCG REG base address. More...
 
#define LPCG_TUPLE_RSRC(tuple)   ((sc_rsrc_t)((uint32_t)(tuple)&0x3FFU))
 Get the resource index. More...
 
#define NV   (0U)
 LPCG Cell not available. More...
 

Enumerations

enum  clock_ip_src_t {
  kCLOCK_IpSrcNone = 0U,
  kCLOCK_IpSrcDummy = 1U
}
 Clock source for peripherals that support various clock selections. More...
 
enum  clock_name_t {
  kCLOCK_CoreSysClk,
  kCLOCK_CONECTIVITY_AhbClk
}
 Clock name used to get clock frequency. More...
 
enum  clock_ip_name_t
 Peripheral clock name difinition used for clock gate, clock source and clock divider setting. More...
 

Functions

void CLOCK_Init (sc_ipc_t ipc)
 Initialize Clock module. More...
 
void CLOCK_Deinit (void)
 Deinitialize Clock module.
 
bool CLOCK_EnableClockExt (clock_ip_name_t name, uint32_t gate)
 Enable the clock for specific IP, with gate setting. More...
 
static bool CLOCK_EnableClock (clock_ip_name_t name)
 Enable the clock for specific IP. More...
 
bool CLOCK_DisableClock (clock_ip_name_t name)
 Disable the clock for specific IP. More...
 
uint32_t CLOCK_SetIpFreq (clock_ip_name_t name, uint32_t freq)
 Set the clock frequency for specific IP module. More...
 
uint32_t CLOCK_GetIpFreq (clock_ip_name_t name)
 Get the clock frequency for a specific IP module. More...
 
uint32_t CLOCK_GetFreq (clock_name_t name)
 Gets the clock frequency for a specific clock name. More...
 
uint32_t CLOCK_GetCoreSysClkFreq (void)
 Get the core clock or system clock frequency. More...
 
void CLOCK_ConfigLPCG (clock_ip_name_t name, uint32_t swGate, uint32_t hwGate)
 Config the LPCG cell for specific IP. More...
 
void CLOCK_SetLpcgGate (volatile uint32_t *regBase, uint32_t swGate, uint32_t hwGate, uint32_t bitsMask)
 Set LPCG gate for specific LPCG. More...
 
void SDK_DelayAtLeastUs (uint32_t delay_us)
 Use DWT to delay at least for some time. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 CLOCK driver version 2.2.0. More...
 

Macro Definition Documentation

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
#define MU_CLOCKS
Value:
{ \
kCLOCK_M4_0_Mu0B, kCLOCK_M4_0_Mu0B, kCLOCK_M4_0_Mu0B, kCLOCK_M4_0_Mu0B, kCLOCK_M4_0_Mu0A0, kCLOCK_M4_0_Mu0A1, \
kCLOCK_M4_0_Mu0A2, kCLOCK_M4_0_Mu0A3, kCLOCK_M4_0_Mu1A, kCLOCK_LSIO_Mu0A, kCLOCK_LSIO_Mu1A, \
kCLOCK_LSIO_Mu2A, kCLOCK_LSIO_Mu3A, kCLOCK_LSIO_Mu4A, kCLOCK_LSIO_Mu5A, kCLOCK_LSIO_Mu6A, \
kCLOCK_LSIO_Mu7A, kCLOCK_LSIO_Mu8A, kCLOCK_LSIO_Mu9A, kCLOCK_LSIO_Mu10A, kCLOCK_LSIO_Mu11A, \
kCLOCK_LSIO_Mu12A, kCLOCK_LSIO_Mu13A, kCLOCK_LSIO_Mu5B, kCLOCK_LSIO_Mu6B, kCLOCK_LSIO_Mu7B, \
kCLOCK_LSIO_Mu8B, kCLOCK_LSIO_Mu9B, kCLOCK_LSIO_Mu10B, kCLOCK_LSIO_Mu11B, kCLOCK_LSIO_Mu12B, \
kCLOCK_LSIO_Mu13B, \
}
#define GPIO_CLOCKS
Value:
{ \
kCLOCK_IpInvalid, kCLOCK_IpInvalid, kCLOCK_IpInvalid, kCLOCK_HSIO_Gpio, kCLOCK_LSIO_Gpio0, kCLOCK_LSIO_Gpio1, \
kCLOCK_LSIO_Gpio2, kCLOCK_LSIO_Gpio3, kCLOCK_LSIO_Gpio4, kCLOCK_LSIO_Gpio5, kCLOCK_LSIO_Gpio6, \
kCLOCK_LSIO_Gpio7, kCLOCK_IpInvalid, \
}
#define FLEXSPI_CLOCKS
Value:
{ \
kCLOCK_LSIO_Flexspi0, kCLOCK_LSIO_Flexspi1, \
}
#define RGPIO_CLOCKS
Value:
{ \
kCLOCK_M4_0_Rgpio, \
}
#define FTM_CLOCKS
Value:
{ \
kCLOCK_DMA_Ftm0, kCLOCK_DMA_Ftm1, \
}
#define GPT_CLOCKS
Value:
{ \
kCLOCK_AUDIO_Gpt0, kCLOCK_AUDIO_Gpt1, kCLOCK_AUDIO_Gpt2, kCLOCK_AUDIO_Gpt3, kCLOCK_AUDIO_Gpt4, \
kCLOCK_AUDIO_Gpt5, kCLOCK_LSIO_Gpt0, kCLOCK_LSIO_Gpt1, kCLOCK_LSIO_Gpt2, kCLOCK_LSIO_Gpt3, \
kCLOCK_LSIO_Gpt4, \
}
#define FLEXCAN_CLOCKS
Value:
{ \
kCLOCK_DMA_Can0, kCLOCK_DMA_Can1, kCLOCK_DMA_Can2, \
}
#define LPUART_CLOCKS
Value:
{ \
kCLOCK_DMA_Lpuart0, kCLOCK_DMA_Lpuart1, kCLOCK_DMA_Lpuart2, kCLOCK_DMA_Lpuart3, kCLOCK_M4_0_Lpuart, \
kCLOCK_SCU_Lpuart, \
}
#define LPADC_CLOCKS
Value:
{ \
kCLOCK_ADMA_Lpadc0, \
}
#define INTMUX_CLOCKS
Value:
{ \
kCLOCK_M4_0_Intmux, \
}
#define SAI_CLOCKS
Value:
{ \
kCLOCK_AUDIO_Sai0, kCLOCK_AUDIO_Sai1, kCLOCK_AUDIO_Sai2, kCLOCK_AUDIO_Sai3, kCLOCK_AUDIO_Sai4, \
kCLOCK_AUDIO_Sai5, \
}
#define SEMA42_CLOCKS
Value:
{ \
kCLOCK_M4_0_Sema42, kCLOCK_SCU_Sema42, \
}
#define TPM_CLOCKS
Value:
{ \
kCLOCK_M4_0_Tpm, kCLOCK_SCU_Tpm, \
}
#define LPIT_CLOCKS
Value:
{ \
kCLOCK_M4_0_Lpit, kCLOCK_SCU_Lpit, \
}
#define LPI2C_CLOCKS
Value:
{ \
kCLOCK_DMA_Lpi2c0, kCLOCK_DMA_Lpi2c1, kCLOCK_DMA_Lpi2c2, kCLOCK_DMA_Lpi2c3, kCLOCK_CiPiLpi2c, \
kCLOCK_M4_0_Lpi2c, kCLOCK_DiMiPiDsiLvds0Lpi2c0, kCLOCK_DiMiPiDsiLvds0Lpi2c1, kCLOCK_DiMiPiDsiLvds1Lpi2c0, \
kCLOCK_DiMiPiDsiLvds1Lpi2c1, kCLOCK_MipiCsiLpi2c, kCLOCK_SCU_Lpi2c, \
}
#define LPSPI_CLOCKS
Value:
{ \
kCLOCK_DMA_Lpspi0, kCLOCK_DMA_Lpspi1, kCLOCK_DMA_Lpspi2, kCLOCK_DMA_Lpspi3, \
}
#define EDMA_CLOCKS
Value:
{ \
kCLOCK_DMA_Dma0, \
}
#define ESAI_CLOCKS
Value:
{ \
kCLOCK_AUDIO_Esai0, kCLOCK_AUDIO_Esai1, \
}
#define ISI_CLOCKS
Value:
{ \
kCLOCK_IMAGING_Isi0, kCLOCK_IMAGING_Isi1, kCLOCK_IMAGING_Isi2, kCLOCK_IMAGING_Isi3, kCLOCK_IMAGING_Isi4, \
kCLOCK_IMAGING_Isi5, kCLOCK_IMAGING_Isi6, kCLOCK_IMAGING_Isi7, \
}
#define MIPI_CSI2RX_CLOCKS
Value:
{ \
kCLOCK_MipiCsi2Rx0, \
}
#define MIPI_DSI_HOST_CLOCKS
Value:
{ \
kCLOCK_MipiDsiHost0, kCLOCK_MipiDsiHost1 \
}
#define ENET_CLOCKS
Value:
{ \
kCLOCK_CONNECTIVITY_Enet0, kCLOCK_CONNECTIVITY_Enet1 \
}
#define DPU_CLOCKS
Value:
{ \
kCLOCK_Dpu0, \
}
#define CI_PI_CLOCKS
Value:
{ \
kCLOCK_CiPi0, \
}
#define CAAM_CLOCKS
Value:
{ \
kCLOCK_CAAM_JR1, kCLOCK_CAAM_JR2, kCLOCK_CAAM_JR3, \
}
#define LDB_CLOCKS
Value:
{ \
kCLOCK_Ldb0, kCLOCK_Ldb1 \
}
#define LPCG_TUPLE (   rsrc,
  base 
)    ((uint32_t)((((base) >> 12U) << 10U) | rsrc))

The LPCG base should be 4KB aligned, if not it will be truncated.

#define LPCG_TUPLE_REG_BASE (   tuple)    ((volatile uint32_t *)((((uint32_t)(tuple) >> 10U) & 0xFFFFFU) << 12U))
#define LPCG_TUPLE_RSRC (   tuple)    ((sc_rsrc_t)((uint32_t)(tuple)&0x3FFU))
#define NV   (0U)

Enumeration Type Documentation

Enumerator
kCLOCK_IpSrcNone 

Clock is off.

kCLOCK_IpSrcDummy 

Clock option 1.

Enumerator
kCLOCK_CoreSysClk 

Core/system clock for M4.

kCLOCK_CONECTIVITY_AhbClk 

AHB clock in Connectivity subsystem.

It is defined as the corresponding register address.

Function Documentation

void CLOCK_Init ( sc_ipc_t  ipc)
Parameters
ipcIPC handle for communication with SCU, see sc_ipc_t.
bool CLOCK_EnableClockExt ( clock_ip_name_t  name,
uint32_t  gate 
)
Parameters
nameWhich clock to enable, see clock_ip_name_t.
gate0: clock always on, 1: HW auto clock gating.
Returns
true if success, false if failure.
static bool CLOCK_EnableClock ( clock_ip_name_t  name)
inlinestatic
Parameters
nameWhich clock to enable, see clock_ip_name_t.
Returns
true for success, false for failure.
bool CLOCK_DisableClock ( clock_ip_name_t  name)
Parameters
nameWhich clock to disable, see clock_ip_name_t.
Returns
true for success, false for failure.
uint32_t CLOCK_SetIpFreq ( clock_ip_name_t  name,
uint32_t  freq 
)

This function sets the IP module clock frequency.

Parameters
nameWhich peripheral to check, see clock_ip_name_t.
freqTarget clock frequency value in hertz.
Returns
the Real clock frequency value in hertz, or 0 if failed
uint32_t CLOCK_GetIpFreq ( clock_ip_name_t  name)

This function gets the IP module clock frequency.

Parameters
nameWhich peripheral to get, see clock_ip_name_t.
Returns
Clock frequency value in hertz, or 0 if failed
uint32_t CLOCK_GetFreq ( clock_name_t  name)

This function checks the current clock configurations and then calculates the clock frequency for a specific clock name defined in clock_name_t.

Parameters
clockNameClock names defined in clock_name_t
Returns
Clock frequency value in hertz
uint32_t CLOCK_GetCoreSysClkFreq ( void  )
Returns
Clock frequency in Hz.
void CLOCK_ConfigLPCG ( clock_ip_name_t  name,
uint32_t  swGate,
uint32_t  hwGate 
)
Parameters
nameWhich clock to enable, see clock_ip_name_t.
swGateSoftware clock gating. 0: clock is gated; 1: clock is enabled
swGateHardware auto gating. 0: disable the HW clock gate control; 1: HW clock gating is enabled
void CLOCK_SetLpcgGate ( volatile uint32_t *  regBase,
uint32_t  swGate,
uint32_t  hwGate,
uint32_t  bitsMask 
)
Parameters
regBaseLPCG register base address.
swGateSoftware clock gating. 0: clock is gated; 1: clock is enabled
swGateHardware auto gating. 0: disable the HW clock gate control; 1: HW clock gating is enabled
bitsMaskThe available bits in LPCG register. Each bit indicate the corresponding bit is available or not.
void SDK_DelayAtLeastUs ( uint32_t  delay_us)

Please note that, this API will calculate the microsecond period with the maximum supported CPU frequency, so this API will only delay for at least the given microseconds, if precise delay count was needed, please implement a new timer count to achieve this function.

Parameters
delay_usDelay time in unit of microsecond.