MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CAU3 TDES driver

Overview

This section describes the programming interface of the CAU3 TDES driver.

Functions

status_t CAU3_TDES_CheckParity (CAU3_Type *base, cau3_key_slot_t keySlot)
 Perform a 3DES key parity check. More...
 
status_t CAU3_TDES_SetKey (CAU3_Type *base, cau3_handle_t *handle, const uint8_t *key, size_t keySize)
 Load DES key into CAU3 key slot. More...
 
status_t CAU3_TDES_Encrypt (CAU3_Type *base, cau3_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext)
 Perform a 3DES encryption. More...
 
status_t CAU3_TDES_Decrypt (CAU3_Type *base, cau3_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext)
 Perform a 3DES decryption. More...
 

Function Documentation

status_t CAU3_TDES_CheckParity ( CAU3_Type *  base,
cau3_key_slot_t  keySlot 
)

Performs a 3DES key parity check on three 8-byte keys. The function is blocking.

Parameters
baseCAU3 peripheral base address
keySlotdefines the key context to be used in the parity check
Returns
status check from task completion
status_t CAU3_TDES_SetKey ( CAU3_Type *  base,
cau3_handle_t *  handle,
const uint8_t *  key,
size_t  keySize 
)

Load the key context into the private DMEM.

Parameters
baseCAU3 peripheral base address.
handleHandle used for the request.
key0-mod-4 aligned pointer to 3DES key.
keySize3DES key size in bytes. Shall equal 24.
Returns
status from set key operation
status_t CAU3_TDES_Encrypt ( CAU3_Type *  base,
cau3_handle_t *  handle,
const uint8_t *  plaintext,
uint8_t *  ciphertext 
)

Performs a 3DES "electronic code book" encryption on one 8-byte data block. The source plaintext and destination ciphertext can overlap in system memory. Supports both blocking and non-blocking task completion.

Parameters
baseCAU3 peripheral base address.
handleHandle used for this request.
plaintextis source uint8_t array of data bytes, any alignment
ciphertextis destination uint8_t array of data byte, any alignment
Returns
status check from task completion
status_t CAU3_TDES_Decrypt ( CAU3_Type *  base,
cau3_handle_t *  handle,
const uint8_t *  ciphertext,
uint8_t *  plaintext 
)

Performs a 3DES "electronic code book" decryption on one 8-byte data block. The source ciphertext and destination plaintext can overlap in sysMemory. Supports both blocking and non-blocking task completion.

Parameters
baseCAU3 peripheral base address.
handleHandle used for this request.
ciphertextis destination uint8_t array of data byte, any alignment
plaintextis source uint8_t array of data bytes, any alignment
Returns
status check from task completion