MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CAU3 PKHA driver

Overview

This section describes the programming interface of the CAU3 PKHA driver.

Data Structures

struct  cau3_pkha_ecc_point_t
 PKHA ECC point structure. More...
 

Enumerations

enum  cau3_pkha_timing_t {
  kCAU3_PKHA_NoTimingEqualized = 0U,
  kCAU3_PKHA_TimingEqualized = 1U
}
 Use of timing equalized version of a PKHA function. More...
 
enum  cau3_pkha_f2m_t {
  kCAU3_PKHA_IntegerArith = 0U,
  kCAU3_PKHA_F2mArith = 1U
}
 Integer vs binary polynomial arithmetic selection. More...
 
enum  cau3_pkha_montgomery_form_t {
  kCAU3_PKHA_NormalValue = 0U,
  kCAU3_PKHA_MontgomeryFormat = 1U
}
 Montgomery or normal PKHA input format. More...
 

Functions

status_t CAU3_PKHA_NormalToMontgomery (CAU3_Type *base, const uint8_t *N, size_t sizeN, uint8_t *A, size_t *sizeA, uint8_t *B, size_t *sizeB, uint8_t *R2, size_t *sizeR2, cau3_pkha_timing_t equalTime, cau3_pkha_f2m_t arithType)
 Converts from integer to Montgomery format. More...
 
status_t CAU3_PKHA_MontgomeryToNormal (CAU3_Type *base, const uint8_t *N, size_t sizeN, uint8_t *A, size_t *sizeA, uint8_t *B, size_t *sizeB, cau3_pkha_timing_t equalTime, cau3_pkha_f2m_t arithType)
 Converts from Montgomery format to int. More...
 
status_t CAU3_PKHA_ModAdd (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, cau3_pkha_f2m_t arithType)
 Performs modular addition - (A + B) mod N. More...
 
status_t CAU3_PKHA_ModSub1 (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize)
 Performs modular subtraction - (A - B) mod N. More...
 
status_t CAU3_PKHA_ModSub2 (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize)
 Performs modular subtraction - (B - A) mod N. More...
 
status_t CAU3_PKHA_ModMul (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, cau3_pkha_f2m_t arithType, cau3_pkha_montgomery_form_t montIn, cau3_pkha_montgomery_form_t montOut, cau3_pkha_timing_t equalTime)
 Performs modular multiplication - (A x B) mod N. More...
 
status_t CAU3_PKHA_ModExp (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, const uint8_t *E, size_t sizeE, uint8_t *result, size_t *resultSize, cau3_pkha_f2m_t arithType, cau3_pkha_montgomery_form_t montIn, cau3_pkha_timing_t equalTime)
 Performs modular exponentiation - (A^E) mod N. More...
 
status_t CAU3_PKHA_ModSqrt (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize)
 Performs Modular Square Root. More...
 
status_t CAU3_PKHA_ModRed (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, cau3_pkha_f2m_t arithType)
 Performs modular reduction - (A) mod N. More...
 
status_t CAU3_PKHA_ModInv (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, cau3_pkha_f2m_t arithType)
 Performs modular inversion - (A^-1) mod N. More...
 
status_t CAU3_PKHA_ModR2 (CAU3_Type *base, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, cau3_pkha_f2m_t arithType)
 Computes integer Montgomery factor R^2 mod N. More...
 
status_t CAU3_PKHA_ModRR (CAU3_Type *base, const uint8_t *P, size_t sizeP, size_t sizeE, uint8_t *result, size_t *resultSize)
 Performs Integer RERP mod P. More...
 
status_t CAU3_PKHA_ModGcd (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *N, size_t sizeN, uint8_t *result, size_t *resultSize, cau3_pkha_f2m_t arithType)
 Calculates the greatest common divisor - GCD (A, N). More...
 
status_t CAU3_PKHA_PrimalityTest (CAU3_Type *base, const uint8_t *A, size_t sizeA, const uint8_t *B, size_t sizeB, const uint8_t *N, size_t sizeN, bool *res)
 Executes Miller-Rabin primality test. More...
 
status_t CAU3_PKHA_ECC_PointAdd (CAU3_Type *base, const cau3_pkha_ecc_point_t *A, const cau3_pkha_ecc_point_t *B, const uint8_t *N, const uint8_t *R2modN, const uint8_t *aCurveParam, const uint8_t *bCurveParam, size_t size, cau3_pkha_f2m_t arithType, cau3_pkha_ecc_point_t *result)
 Adds elliptic curve points - A + B. More...
 
status_t CAU3_PKHA_ECC_PointDouble (CAU3_Type *base, const cau3_pkha_ecc_point_t *B, const uint8_t *N, const uint8_t *aCurveParam, const uint8_t *bCurveParam, size_t size, cau3_pkha_f2m_t arithType, cau3_pkha_ecc_point_t *result)
 Doubles elliptic curve points - B + B. More...
 
status_t CAU3_PKHA_ECC_PointMul (CAU3_Type *base, const cau3_pkha_ecc_point_t *A, const uint8_t *E, size_t sizeE, const uint8_t *N, const uint8_t *R2modN, const uint8_t *aCurveParam, const uint8_t *bCurveParam, size_t size, cau3_pkha_timing_t equalTime, cau3_pkha_f2m_t arithType, cau3_pkha_ecc_point_t *result)
 Multiplies an elliptic curve point by a scalar - E x (A0, A1). More...
 
status_t CAU3_PKHA_ECM_PointMul (CAU3_Type *base, const uint8_t *E, size_t sizeE, const uint8_t *inputCoordinate, const uint8_t *A24, const uint8_t *N, const uint8_t *R2modN, size_t size, cau3_pkha_timing_t equalTime, uint8_t *outputCoordinate)
 Computes scalar multiplication of a point on an elliptic curve in Montgomery form. More...
 
status_t CAU3_PKHA_ECT_PointMul (CAU3_Type *base, const cau3_pkha_ecc_point_t *A, const uint8_t *E, size_t sizeE, const uint8_t *N, const uint8_t *R2modN, const uint8_t *aCurveParam, const uint8_t *dCurveParam, size_t size, cau3_pkha_timing_t equalTime, cau3_pkha_ecc_point_t *result)
 Multiplies an Edwards-form elliptic curve point by a scalar - E x (A0, A1). More...
 
status_t CAU3_PKHA_ECT_PointAdd (CAU3_Type *base, const cau3_pkha_ecc_point_t *A, const cau3_pkha_ecc_point_t *B, const uint8_t *N, const uint8_t *R2modN, const uint8_t *aCurveParam, const uint8_t *dCurveParam, size_t size, cau3_pkha_ecc_point_t *result)
 Adds an Edwards-form elliptic curve points - A + B. More...
 

Data Structure Documentation

struct cau3_pkha_ecc_point_t

Data Fields

uint8_t * X
 X coordinate (affine)
 
uint8_t * Y
 Y coordinate (affine)
 

Enumeration Type Documentation

Enumerator
kCAU3_PKHA_NoTimingEqualized 

Normal version of a PKHA operation.

kCAU3_PKHA_TimingEqualized 

Timing-equalized version of a PKHA operation.

Enumerator
kCAU3_PKHA_IntegerArith 

Use integer arithmetic.

kCAU3_PKHA_F2mArith 

Use binary polynomial arithmetic.

Enumerator
kCAU3_PKHA_NormalValue 

PKHA number is normal integer.

kCAU3_PKHA_MontgomeryFormat 

PKHA number is in montgomery format.

Function Documentation

status_t CAU3_PKHA_NormalToMontgomery ( CAU3_Type *  base,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  A,
size_t *  sizeA,
uint8_t *  B,
size_t *  sizeB,
uint8_t *  R2,
size_t *  sizeR2,
cau3_pkha_timing_t  equalTime,
cau3_pkha_f2m_t  arithType 
)

This function computes R2 mod N and optionally converts A or B into Montgomery format of A or B.

Parameters
baseCAU3 peripheral base address
Nmodulus
sizeNsize of N in bytes
[in,out]AThe first input in non-Montgomery format. Output Montgomery format of the first input.
[in,out]sizeApointer to size variable. On input it holds size of input A in bytes. On output it holds size of Montgomery format of A in bytes.
[in,out]BSecond input in non-Montgomery format. Output Montgomery format of the second input.
[in,out]sizeBpointer to size variable. On input it holds size of input B in bytes. On output it holds size of Montgomery format of B in bytes.
[out]R2Output Montgomery factor R2 mod N.
[out]sizeR2pointer to size variable. On output it holds size of Montgomery factor R2 mod N in bytes.
equalTimeRun the function time equalized or no timing equalization.
arithTypeType of arithmetic to perform (integer or F2m)
Returns
Operation status.
status_t CAU3_PKHA_MontgomeryToNormal ( CAU3_Type *  base,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  A,
size_t *  sizeA,
uint8_t *  B,
size_t *  sizeB,
cau3_pkha_timing_t  equalTime,
cau3_pkha_f2m_t  arithType 
)

This function converts Montgomery format of A or B into int A or B.

Parameters
baseCAU3 peripheral base address
Nmodulus.
sizeNsize of N modulus in bytes.
[in,out]AInput first number in Montgomery format. Output is non-Montgomery format.
[in,out]sizeApointer to size variable. On input it holds size of the input A in bytes. On output it holds size of non-Montgomery A in bytes.
[in,out]BInput first number in Montgomery format. Output is non-Montgomery format.
[in,out]sizeBpointer to size variable. On input it holds size of the input B in bytes. On output it holds size of non-Montgomery B in bytes.
equalTimeRun the function time equalized or no timing equalization.
arithTypeType of arithmetic to perform (integer or F2m)
Returns
Operation status.
status_t CAU3_PKHA_ModAdd ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  B,
size_t  sizeB,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize,
cau3_pkha_f2m_t  arithType 
)

This function performs modular addition of (A + B) mod N, with either integer or binary polynomial (F2m) inputs. In the F2m form, this function is equivalent to a bitwise XOR and it is functionally the same as subtraction.

Parameters
baseCAU3 peripheral base address
Afirst addend (integer or binary polynomial)
sizeASize of A in bytes
Bsecond addend (integer or binary polynomial)
sizeBSize of B in bytes
Nmodulus.
sizeNSize of N in bytes.
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
arithTypeType of arithmetic to perform (integer or F2m)
Returns
Operation status.
status_t CAU3_PKHA_ModSub1 ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  B,
size_t  sizeB,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize 
)

This function performs modular subtraction of (A - B) mod N with integer inputs.

Parameters
baseCAU3 peripheral base address
Afirst addend (integer or binary polynomial)
sizeASize of A in bytes
Bsecond addend (integer or binary polynomial)
sizeBSize of B in bytes
Nmodulus
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
Returns
Operation status.
status_t CAU3_PKHA_ModSub2 ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  B,
size_t  sizeB,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize 
)

This function performs modular subtraction of (B - A) mod N, with integer inputs.

Parameters
baseCAU3 peripheral base address
Afirst addend (integer or binary polynomial)
sizeASize of A in bytes
Bsecond addend (integer or binary polynomial)
sizeBSize of B in bytes
Nmodulus
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
Returns
Operation status.
status_t CAU3_PKHA_ModMul ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  B,
size_t  sizeB,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize,
cau3_pkha_f2m_t  arithType,
cau3_pkha_montgomery_form_t  montIn,
cau3_pkha_montgomery_form_t  montOut,
cau3_pkha_timing_t  equalTime 
)

This function performs modular multiplication with either integer or binary polynomial (F2m) inputs. It can optionally specify whether inputs and/or outputs will be in Montgomery form or not.

Parameters
baseCAU3 peripheral base address
Afirst addend (integer or binary polynomial)
sizeASize of A in bytes
Bsecond addend (integer or binary polynomial)
sizeBSize of B in bytes
Nmodulus.
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
arithTypeType of arithmetic to perform (integer or F2m)
montInFormat of inputs
montOutFormat of output
equalTimeRun the function time equalized or no timing equalization. This argument is ignored for F2m modular multiplication.
Returns
Operation status.
status_t CAU3_PKHA_ModExp ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  N,
size_t  sizeN,
const uint8_t *  E,
size_t  sizeE,
uint8_t *  result,
size_t *  resultSize,
cau3_pkha_f2m_t  arithType,
cau3_pkha_montgomery_form_t  montIn,
cau3_pkha_timing_t  equalTime 
)

This function performs modular exponentiation with either integer or binary polynomial (F2m) inputs.

Parameters
baseCAU3 peripheral base address
Afirst addend (integer or binary polynomial)
sizeASize of A in bytes
Nmodulus
sizeNSize of N in bytes
Eexponent
sizeESize of E in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
montInFormat of A input (normal or Montgomery)
arithTypeType of arithmetic to perform (integer or F2m)
equalTimeRun the function time equalized or no timing equalization.
Returns
Operation status.
status_t CAU3_PKHA_ModSqrt ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize 
)

This function performs modular square root with integer inputs. The modular square root function computes output result B, such that ( B x B ) mod N = input A. If no such B result exists, the result will be set to 0 and the PKHA "prime" flag will be set. Input values A and B are limited to a maximum size of 128 bytes. Note that two such square root values may exist. This algorithm will find either one of them, if any exist. The second possible square root (B') can be found by calculating B' = N - B.

Parameters
baseCAU3 peripheral base address
Ainput value, for which a square root is to be calculated
sizeASize of A in bytes
Nmodulus
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
Returns
Operation status.
status_t CAU3_PKHA_ModRed ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize,
cau3_pkha_f2m_t  arithType 
)

This function performs modular reduction with either integer or binary polynomial (F2m) inputs.

Parameters
baseCAU3 peripheral base address
Afirst addend (integer or binary polynomial)
sizeASize of A in bytes
Nmodulus
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
arithTypeType of arithmetic to perform (integer or F2m)
Returns
Operation status.
status_t CAU3_PKHA_ModInv ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize,
cau3_pkha_f2m_t  arithType 
)

This function performs modular inversion with either integer or binary polynomial (F2m) inputs.

Parameters
baseCAU3 peripheral base address
Afirst addend (integer or binary polynomial)
sizeASize of A in bytes
Nmodulus
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
arithTypeType of arithmetic to perform (integer or F2m)
Returns
Operation status.
status_t CAU3_PKHA_ModR2 ( CAU3_Type *  base,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize,
cau3_pkha_f2m_t  arithType 
)

This function computes a constant to assist in converting operands into the Montgomery residue system representation.

Parameters
baseCAU3 peripheral base address
Nmodulus
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
arithTypeType of arithmetic to perform (integer or F2m)
Returns
Operation status.
status_t CAU3_PKHA_ModRR ( CAU3_Type *  base,
const uint8_t *  P,
size_t  sizeP,
size_t  sizeE,
uint8_t *  result,
size_t *  resultSize 
)

This function is used to compute a constant to assist in converting operands into the Montgomery residue system representation specifically for Chinese Remainder Theorem while performing RSA with a CRT implementation where a modulus E=P x Q, and P and Q are prime numbers. Although labeled RERP mod P, this routine (function) can also compute RERQ mod Q.

Parameters
baseCAU3 peripheral base address
Pmodulus P or Q of CRT, an odd integer
sizePSize of P in bytes
sizeENumber of bytes of E = P x Q (this size must be given, though content of E itself is not used).
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
Returns
Operation status.
status_t CAU3_PKHA_ModGcd ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  N,
size_t  sizeN,
uint8_t *  result,
size_t *  resultSize,
cau3_pkha_f2m_t  arithType 
)

This function calculates the greatest common divisor of two inputs with either integer or binary polynomial (F2m) inputs.

Parameters
baseCAU3 peripheral base address
Afirst value (must be smaller than or equal to N)
sizeASize of A in bytes
Nsecond value (must be non-zero)
sizeNSize of N in bytes
[out]resultOutput array to store result of operation
[out]resultSizeOutput size of operation in bytes
arithTypeType of arithmetic to perform (integer or F2m)
Returns
Operation status.
status_t CAU3_PKHA_PrimalityTest ( CAU3_Type *  base,
const uint8_t *  A,
size_t  sizeA,
const uint8_t *  B,
size_t  sizeB,
const uint8_t *  N,
size_t  sizeN,
bool *  res 
)

This function calculates whether or not a candidate prime number is likely to be a prime.

Parameters
baseCAU3 peripheral base address
Ainitial random seed
sizeASize of A in bytes
Bnumber of trial runs
sizeBSize of B in bytes
Ncandidate prime integer
sizeNSize of N in bytes
[out]resTrue if the value is likely prime or false otherwise
Returns
Operation status.
status_t CAU3_PKHA_ECC_PointAdd ( CAU3_Type *  base,
const cau3_pkha_ecc_point_t *  A,
const cau3_pkha_ecc_point_t *  B,
const uint8_t *  N,
const uint8_t *  R2modN,
const uint8_t *  aCurveParam,
const uint8_t *  bCurveParam,
size_t  size,
cau3_pkha_f2m_t  arithType,
cau3_pkha_ecc_point_t *  result 
)

This function performs ECC point addition over a prime field (Fp) or binary field (F2m) using affine coordinates.

Parameters
baseCAU3 peripheral base address
ALeft-hand point
BRight-hand point
NPrime modulus of the field
R2modNNULL (the function computes R2modN internally) or pointer to pre-computed R2modN (obtained from CAU3_PKHA_ModR2() function).
aCurveParamA parameter from curve equation
bCurveParamB parameter from curve equation (constant)
sizeSize in bytes of curve points and parameters
arithTypeType of arithmetic to perform (integer or F2m)
[out]resultResult point
Returns
Operation status.
status_t CAU3_PKHA_ECC_PointDouble ( CAU3_Type *  base,
const cau3_pkha_ecc_point_t *  B,
const uint8_t *  N,
const uint8_t *  aCurveParam,
const uint8_t *  bCurveParam,
size_t  size,
cau3_pkha_f2m_t  arithType,
cau3_pkha_ecc_point_t *  result 
)

This function performs ECC point doubling over a prime field (Fp) or binary field (F2m) using affine coordinates.

Parameters
baseCAU3 peripheral base address
BPoint to double
NPrime modulus of the field
aCurveParamA parameter from curve equation
bCurveParamB parameter from curve equation (constant)
sizeSize in bytes of curve points and parameters
arithTypeType of arithmetic to perform (integer or F2m)
[out]resultResult point
Returns
Operation status.
status_t CAU3_PKHA_ECC_PointMul ( CAU3_Type *  base,
const cau3_pkha_ecc_point_t *  A,
const uint8_t *  E,
size_t  sizeE,
const uint8_t *  N,
const uint8_t *  R2modN,
const uint8_t *  aCurveParam,
const uint8_t *  bCurveParam,
size_t  size,
cau3_pkha_timing_t  equalTime,
cau3_pkha_f2m_t  arithType,
cau3_pkha_ecc_point_t *  result 
)

This function performs ECC point multiplication to multiply an ECC point by a scalar integer multiplier over a prime field (Fp) or a binary field (F2m).

Parameters
baseCAU3 peripheral base address
APoint as multiplicand
EScalar multiple
sizeEThe size of E, in bytes
NModulus, a prime number for the Fp field or Irreducible polynomial for F2m field.
R2modNNULL (the function computes R2modN internally) or pointer to pre-computed R2modN (obtained from CAU3_PKHA_ModR2() function).
aCurveParamA parameter from curve equation
bCurveParamB parameter from curve equation (C parameter for operation over F2m).
sizeSize in bytes of curve points and parameters
equalTimeRun the function time equalized or no timing equalization.
arithTypeType of arithmetic to perform (integer or F2m)
[out]resultResult point
Returns
Operation status.
status_t CAU3_PKHA_ECM_PointMul ( CAU3_Type *  base,
const uint8_t *  E,
size_t  sizeE,
const uint8_t *  inputCoordinate,
const uint8_t *  A24,
const uint8_t *  N,
const uint8_t *  R2modN,
size_t  size,
cau3_pkha_timing_t  equalTime,
uint8_t *  outputCoordinate 
)

This function computes the scalar multiplication of a point on an elliptic curve in Montgomery form. The input and output are just the x coordinates of the points. The points on a curve are defined by the equation E: B*y^2 = x^3 + A*x^2 + x mod p This function computes a point multiplication on a Montgomery curve, using Montgomery values, by means of a Montgomery ladder. At the end of the ladder, P2 = P3 + P1, where P1 is the input and P3 is the result.

Parameters
baseCAU3 peripheral base address
EScalar multiplier, any integer
sizeEThe size of E, in bytes
inputCoordinatePoint as multiplicand, an input point's affine x coordinate
A24elliptic curve a24 parameter, that is, (A+2)/4
NModulus, a prime number.
R2modNNULL (the function computes R2modN internally) or pointer to pre-computed R2modN (obtained from CAU3_PKHA_ModR2() function).
sizeSize in bytes of curve points and parameters
equalTimeRun the function time equalized or no timing equalization.
[out]outputCoordinateResulting poin's x affine coordinate.
Returns
Operation status.
status_t CAU3_PKHA_ECT_PointMul ( CAU3_Type *  base,
const cau3_pkha_ecc_point_t *  A,
const uint8_t *  E,
size_t  sizeE,
const uint8_t *  N,
const uint8_t *  R2modN,
const uint8_t *  aCurveParam,
const uint8_t *  dCurveParam,
size_t  size,
cau3_pkha_timing_t  equalTime,
cau3_pkha_ecc_point_t *  result 
)

This function performs scalar multiplication of an Edwards-form elliptic curve point in affine coordinates. The points on a curve are defined by the equation E: a*X^2 + d^2 = 1 + D^2*X^2*Y^2 mod N

Parameters
baseCAU3 peripheral base address
APoint as multiplicand
EScalar multiple
sizeEThe size of E, in bytes
NModulus, a prime number for the Fp field.
R2modNNULL (the function computes R2modN internally) or pointer to pre-computed R2modN (obtained from CAU3_PKHA_ModR2() function).
aCurveParamA parameter from curve equation
dCurveParamD parameter from curve equation.
sizeSize in bytes of curve points and parameters
equalTimeRun the function time equalized or no timing equalization.
[out]resultResult point
Returns
Operation status.
status_t CAU3_PKHA_ECT_PointAdd ( CAU3_Type *  base,
const cau3_pkha_ecc_point_t *  A,
const cau3_pkha_ecc_point_t *  B,
const uint8_t *  N,
const uint8_t *  R2modN,
const uint8_t *  aCurveParam,
const uint8_t *  dCurveParam,
size_t  size,
cau3_pkha_ecc_point_t *  result 
)

This function performs Edwards-form elliptic curve point addition over a prime field (Fp) using affine coordinates. The points on a curve are defined by the equation E: a*X^2 + Y^2 = 1 + d^2*X^2*Y^2 mod N

Parameters
baseCAU3 peripheral base address
ALeft-hand point
BRight-hand point
NPrime modulus of the field
R2modNNULL (the function computes R2modN internally) or pointer to pre-computed R2modN (obtained from CAU3_PKHA_ModR2() function).
aCurveParamA parameter from curve equation
dCurveParamD parameter from curve equation
sizeSize in bytes of curve points and parameters
[out]resultResult point
Returns
Operation status.