![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | flexio_uart_dma_handle_t |
| UART DMA handle. More... | |
Typedefs | |
| typedef void(* | flexio_uart_dma_transfer_callback_t )(FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, status_t status, void *userData) |
| UART transfer callback function. More... | |
eDMA transactional | |
| status_t | FLEXIO_UART_TransferCreateHandleDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, flexio_uart_dma_transfer_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle) |
| Initializes the FLEXIO_UART handle which is used in transactional functions. More... | |
| status_t | FLEXIO_UART_TransferSendDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, flexio_uart_transfer_t *xfer) |
| Sends data using DMA. More... | |
| status_t | FLEXIO_UART_TransferReceiveDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, flexio_uart_transfer_t *xfer) |
| Receives data using DMA. More... | |
| void | FLEXIO_UART_TransferAbortSendDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle) |
| Aborts the sent data which using DMA. More... | |
| void | FLEXIO_UART_TransferAbortReceiveDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle) |
| Aborts the receive data which using DMA. More... | |
| status_t | FLEXIO_UART_TransferGetSendCountDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, size_t *count) |
| Gets the number of bytes sent out. More... | |
| status_t | FLEXIO_UART_TransferGetReceiveCountDMA (FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, size_t *count) |
| Gets the number of bytes received. More... | |
| struct _flexio_uart_dma_handle |
Data Fields | |
| flexio_uart_dma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| UART callback function parameter. More... | |
| size_t | txDataSizeAll |
| Total bytes to be sent. More... | |
| size_t | rxDataSizeAll |
| Total bytes to be received. More... | |
| dma_handle_t * | txDmaHandle |
| The DMA TX channel used. More... | |
| dma_handle_t * | rxDmaHandle |
| The DMA RX channel used. More... | |
| volatile uint8_t | txState |
| TX transfer state. More... | |
| volatile uint8_t | rxState |
| RX transfer state. | |
| flexio_uart_dma_transfer_callback_t flexio_uart_dma_handle_t::callback |
| void* flexio_uart_dma_handle_t::userData |
| size_t flexio_uart_dma_handle_t::txDataSizeAll |
| size_t flexio_uart_dma_handle_t::rxDataSizeAll |
| dma_handle_t* flexio_uart_dma_handle_t::txDmaHandle |
| dma_handle_t* flexio_uart_dma_handle_t::rxDmaHandle |
| volatile uint8_t flexio_uart_dma_handle_t::txState |
| typedef void(* flexio_uart_dma_transfer_callback_t)(FLEXIO_UART_Type *base, flexio_uart_dma_handle_t *handle, status_t status, void *userData) |
| status_t FLEXIO_UART_TransferCreateHandleDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_dma_handle_t * | handle, | ||
| flexio_uart_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | txDmaHandle, | ||
| dma_handle_t * | rxDmaHandle | ||
| ) |
| base | Pointer to FLEXIO_UART_Type structure. |
| handle | Pointer to flexio_uart_dma_handle_t structure. |
| callback | FlexIO UART callback, NULL means no callback. |
| userData | User callback function data. |
| txDmaHandle | User requested DMA handle for TX DMA transfer. |
| rxDmaHandle | User requested DMA handle for RX DMA transfer. |
| kStatus_Success | Successfully create the handle. |
| kStatus_OutOfRange | The FlexIO UART DMA type/handle table out of range. |
| status_t FLEXIO_UART_TransferSendDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_dma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) |
This function send data using DMA. This is non-blocking function, which returns right away. When all data is sent out, the send callback function is called.
| base | Pointer to FLEXIO_UART_Type structure |
| handle | Pointer to flexio_uart_dma_handle_t structure |
| xfer | FLEXIO_UART DMA transfer structure, see flexio_uart_transfer_t. |
| kStatus_Success | if succeed, others failed. |
| kStatus_FLEXIO_UART_TxBusy | Previous transfer on going. |
| status_t FLEXIO_UART_TransferReceiveDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_dma_handle_t * | handle, | ||
| flexio_uart_transfer_t * | xfer | ||
| ) |
This function receives data using DMA. This is non-blocking function, which returns right away. When all data is received, the receive callback function is called.
| base | Pointer to FLEXIO_UART_Type structure |
| handle | Pointer to flexio_uart_dma_handle_t structure |
| xfer | FLEXIO_UART DMA transfer structure, see flexio_uart_transfer_t. |
| kStatus_Success | if succeed, others failed. |
| kStatus_FLEXIO_UART_RxBusy | Previous transfer on going. |
| void FLEXIO_UART_TransferAbortSendDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_dma_handle_t * | handle | ||
| ) |
This function aborts the sent data which using DMA.
| base | Pointer to FLEXIO_UART_Type structure |
| handle | Pointer to flexio_uart_dma_handle_t structure |
| void FLEXIO_UART_TransferAbortReceiveDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_dma_handle_t * | handle | ||
| ) |
This function aborts the receive data which using DMA.
| base | Pointer to FLEXIO_UART_Type structure |
| handle | Pointer to flexio_uart_dma_handle_t structure |
| status_t FLEXIO_UART_TransferGetSendCountDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the number of bytes sent out.
| base | Pointer to FLEXIO_UART_Type structure |
| handle | Pointer to flexio_uart_dma_handle_t structure |
| count | Number of bytes sent so far by the non-blocking transaction. |
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. |
| kStatus_Success | Successfully return the count. |
| status_t FLEXIO_UART_TransferGetReceiveCountDMA | ( | FLEXIO_UART_Type * | base, |
| flexio_uart_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
This function gets the number of bytes received.
| base | Pointer to FLEXIO_UART_Type structure |
| handle | Pointer to flexio_uart_dma_handle_t structure |
| count | Number of bytes received so far by the non-blocking transaction. |
| kStatus_NoTransferInProgress | transfer has finished or no transfer in progress. |
| kStatus_Success | Successfully return the count. |