The Smart Card interface EMVSIM driver handles the EMVSIM peripheral, which covers all necessary functions to control the ICC. These functions are ICC clock setup, ICC voltage turning on/off, ICC card detection, activation/deactivation, and ICC reset sequences. The EMVSIM peripheral covers all features of interface ICC chips.
|
| void | SMARTCARD_PHY_EMVSIM_GetDefaultConfig (smartcard_interface_config_t *config) |
| | Fills in the smartcardInterfaceConfig structure with default values. More...
|
| |
| status_t | SMARTCARD_PHY_EMVSIM_Init (EMVSIM_Type *base, const smartcard_interface_config_t *config, uint32_t srcClock_Hz) |
| | Configures a Smart card interface. More...
|
| |
| void | SMARTCARD_PHY_EMVSIM_Deinit (EMVSIM_Type *base, const smartcard_interface_config_t *config) |
| | De-initializes a Smart card interface, stops the Smart card clock, and disables the VCC. More...
|
| |
| status_t | SMARTCARD_PHY_EMVSIM_Activate (EMVSIM_Type *base, smartcard_context_t *context, smartcard_reset_type_t resetType) |
| | Activates the Smart card IC. More...
|
| |
| status_t | SMARTCARD_PHY_EMVSIM_Deactivate (EMVSIM_Type *base, smartcard_context_t *context) |
| | De-activates the Smart card IC. More...
|
| |
| status_t | SMARTCARD_PHY_EMVSIM_Control (EMVSIM_Type *base, smartcard_context_t *context, smartcard_interface_control_t control, uint32_t param) |
| | Controls the Smart card interface IC. More...
|
| |
| #define SMARTCARD_INIT_DELAY_CLOCK_CYCLES_ADJUSTMENT (4200u) |
- Parameters
-
| config | The user configuration structure of type smartcard_interface_config_t. Function fill in members: clockToResetDelay = 42000, vcc = kSmartcardVoltageClassB3_3V, with default values. |
- Parameters
-
| base | The Smart card peripheral module base address. |
| config | The user configuration structure of type smartcard_interface_config_t. The user is responsible to fill out the members of this structure and to pass the pointer of this structure into this function or call SMARTCARD_PHY_EMVSIMInitUserConfigDefault to fill out structure with default values. |
| srcClock_Hz | Smart card clock generation module source clock. |
- Return values
-
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError for an error. |
- Parameters
-
| base | Smart card peripheral module base address. |
| config | Smart card configuration structure. |
- Parameters
-
| base | The EMVSIM peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
| resetType | type of reset to be performed, possible values = kSmartcardColdReset, kSmartcardWarmReset |
- Return values
-
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError for an error. |
- Parameters
-
| base | The EMVSIM peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
- Return values
-
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError for an error. |
- Parameters
-
| base | The EMVSIM peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
| control | A interface command type. |
| param | Integer value specific to control type |
- Return values
-
| kStatus_SMARTCARD_Success | or kStatus_SMARTCARD_OtherError for an error. |